![]() |
MCUSW
|
This files defines CAN MCAL configuration structures
Data Structures | |
| struct | Can_MaskType |
| Structure defining the filter mask to be used. More... | |
| struct | Can_HwFilterType |
| Structure defining the HW filter to be used. More... | |
| struct | Can_FdBaudConfigType |
| Structure defining the CAN FD data phase baud rate configuration. More... | |
| struct | Can_BaudConfigType |
| Structure defining the CAN baud rate configuration. More... | |
| struct | Can_ControllerType |
| Can Controller Configuration definition. More... | |
| struct | Can_ControllerType_PC |
| Can Controller Pre Compile Configuration definition. More... | |
| struct | Can_MailboxType |
| Can mailox configuration definition. More... | |
| struct | Can_MailboxType_PC |
| Can mailox Pre compile configuration definition. More... | |
| struct | Can_DmaPrms |
| Dummy structure will be used if DMA support is required. More... | |
| struct | Can_ConfigType |
| Can MCAL root configuration structure. More... | |
| struct | Can_RegisterReadbackType |
| Register Readback Structure. More... | |
Macros | |
| #define | CAN_VARIANT_PRE_COMPILE (STD_ON) |
| CAN Build Variant. Build variants.(i.e Pre Compile,Post Build) | |
Can Error Types | |
Error Types returned by Can functions | |
| enum | Can_MailBoxDirectionType { CAN_MAILBOX_DIRECTION_RX = 0x0U , CAN_MAILBOX_DIRECTION_TX = 0x1U } |
| Can Mailbox direction enum. More... | |
| enum | Can_HandleType { CAN_FULL = 0x0U , CAN_BASIC = 0x1U } |
| Can Handle Type enum. More... | |
| enum | Can_TxRxProcessingType { CAN_TX_RX_PROCESSING_INTERRUPT = 0x0U , CAN_TX_RX_PROCESSING_MIXED = 0x1U , CAN_TX_RX_PROCESSING_POLLING = 0x2U } |
| Can Tx/Rx processing enum. More... | |
| enum | Can_IrqStatusType { CAN_IRQ_NO_INTR_EVENT = 0U , CAN_IRQ_INTR_STUFF_EVENT = 1U , CAN_IRQ_INTR_FORM_EVENT = 2U , CAN_IRQ_INTR_ACK_EVENT = 3U , CAN_IRQ_INTR_BIT1_EVENT = 4U , CAN_IRQ_INTR_BIT0_EVENT = 5U , CAN_IRQ_INTR_CRC_EVENT = 6U , CAN_IRQ_INTR_TOO_EVENT = 7U , CAN_IRQ_STATUS_READ_FAIL = 8U } |
| CAN IRQ status enum. More... | |
| typedef uint8 | CanControllerState_Type |
| Can Controller State enum type. | |
| typedef uint32 | Can_InterruptMask_Type |
| Can Interrupt Mask type. | |
| void | Can_GetVersionInfo (Std_VersionInfoType *VersionInfo) |
| Function returns the version information of this module. | |
| void | Can_Init (const Can_ConfigType *CfgPtr) |
| This function initializes the module. | |
| Std_ReturnType | Can_SetControllerMode (uint8 Controller, Can_ControllerStateType Transition) |
| This function performs software triggered state transitions of the CAN controller State machine. | |
| Std_ReturnType | Can_Write (Can_HwHandleType Hth, const Can_PduType *PduInfo) |
| This function is called by CanIf to pass a CAN message to CanDrv for transmission. | |
| void | Can_DisableControllerInterrupts (uint8 Controller) |
| This function disables all interrupts for this CAN controller. | |
| void | Can_EnableControllerInterrupts (uint8 Controller) |
| This function enables all allowed interrupts. | |
| void | Can_MainFunction_Write (void) |
| This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING. | |
| void | Can_MainFunction_BusOff (void) |
| This function performs the polling of bus-off events that are configured statically as 'to be polled'. | |
| void | Can_MainFunction_Read (void) |
| This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING. | |
| void | Can_MainFunction_Wakeup (void) |
| This function performs the polling of wake-up events that are configured statically as 'to be polled'. | |
| void | Can_MainFunction_Mode (void) |
| This function performs the polling of CAN controller mode transitions. | |
| Std_ReturnType | Can_SetBaudrate (uint8 Controller, uint16 BaudRateConfigID) |
| This service shall set the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset. | |
| Std_ReturnType | Can_TestLoopBackModeEnable (uint8 Controller, uint8 Mode) |
| This service will enable CAN loopback mode. | |
| Std_ReturnType | Can_TestLoopBackModeDisable (uint8 Controller, uint8 Mode) |
| This service will disable CAN loopback mode. | |
| Std_ReturnType | Can_RegisterReadback (VAR(uint8,) Controller, Can_RegisterReadbackType *RegRbPtr) |
| This service will readback CAN registers. | |
| Std_ReturnType | Can_EnableIntr (VAR(uint8,) Controller, VAR(uint8,) CanErrVar) |
| This service will Enable the interrupts. | |
| Std_ReturnType | Can_DisableIntr (VAR(uint8,) Controller, VAR(uint8,) CanErrVar) |
| This service will Disable the Interrupts. | |
| Can_IrqStatusType | Can_GetIntrStatus (VAR(uint8,) Controller) |
| This service will provide the status of the interrupt. | |
| Std_ReturnType | Can_ClearIntrStatus (VAR(uint8,) Controller) |
| This service will clear the interrupt status. | |
| void | Can_IntISR_Fun (Can_ControllerInstance CanInstanceID) |
| This function is the ISR for CAN controller 0/INT 0. | |
| void | Can_DeInit (void) |
| This function de-initializes the module. | |
| Std_ReturnType | Can_GetControllerMode (uint8 Controller, Can_ControllerStateType *ControllerModePtr) |
| This service reports about the current status of the requested CAN controller. | |
| Std_ReturnType | Can_GetControllerErrorState (uint8 ControllerId, Can_ErrorStateType *ErrorStatePtr) |
| This service obtains the error state of the CAN controller. | |
CAN DEM Error codes to report | |
Pre-compile switches for enabling/disabling DEM events | |
| enum | Can_ControllerInstance { CAN_CONTROLLER_INSTANCE_MCU_MCAN0 = 0U , CAN_CONTROLLER_INSTANCE_MCU_MCAN1 = 1U } |
| Can Controller Instances enum. More... | |
| const struct Can_ConfigType_s | CanConfigSet |
| CAN Configuration struct declaration. | |
| const struct Can_ControllerStruct_PC | CanConfigSet_PC_CanController_0 |
| CAN Controller Configuration Pre Compile struct declaration. | |
| const struct Can_ControllerStruct_PC | CanConfigSet_PC_CanController_1 |
| CAN Controller Configuration Pre Compile struct declaration. | |
| const struct Can_ControllerStruct_PC * | CanConfigSet_CanController_List_PC [CAN_NUM_CONTROLLER] |
| CAN Controller Pre Compile Configuration List. | |
| const struct Can_MailboxStruct_PC * | CanConfigSet_CanHardwareObject_List_PC [CAN_NUM_MAILBOXES] |
| CAN Mailbox Pre Compile Configuration List. | |
| const uint32 | Can_MsgmemRAMBaseAddr [CAN_MAX_CONTROLLER] |
| Base Address of the can peripherals. | |
| const uint32 | Can_MCANSSBaseAddr [CAN_MAX_CONTROLLER] |
| const uint32 | Can_MCANCoreRegBaseAddr [CAN_MAX_CONTROLLER] |
| const uint32 | Can_MCANECCAggrRegBaseAddr [CAN_MAX_CONTROLLER] |
| ISR (Can_0_Int0ISR) | |
| ISR (Can_1_Int0ISR) | |
| #define | CAN_E_HARDWARE_ERROR (DemConf_DemEventParameter_CAN_E_HARDWARE_ERROR) |
| Hardware failed. | |
CAN Driver ISR category level | |
Defines for CAN Driver ISR ISR category level | |
| #define | CAN_ISR_VOID (0x00U) |
| void ISR type | |
| #define | CAN_ISR_CAT1 (0x01U) |
| Category 1 ISR type. | |
| #define | CAN_ISR_CAT2 (0x02U) |
| Category 2 ISR type. | |
Can Driver Configuration SW Version Info | |
Pre-compile switches for enabling/disabling CAN MCAL APIs | |
| #define | CAN_VERSION_INFO_API (STD_ON) |
| #define | CAN_DEV_ERROR_DETECT (STD_ON) |
| #define | CAN_SAFETY_DIAGNOSTIC (STD_OFF) |
| #define | CAN_LOOPBACK_ENABLE (STD_ON) |
| #define | CAN_REGISTER_READBACK_API (STD_ON) |
| #define | CAN_SET_BAUDRATE_API (STD_ON) |
| #define | CAN_WAKEUP_FUNCTIONALITY_API (STD_OFF) |
| #define | CAN_MULTIPLEXED_TRANSMISSION_ENABLE (STD_ON) |
| #define | CAN_INIT_CONFIG_PC CanConfigSet |
| Pre Compile config macro name. | |
| #define | CAN_TX_POLLING (STD_OFF) |
| #define | CAN_RX_POLLING (STD_OFF) |
| #define | CAN_BUSOFF_POLLING (STD_OFF) |
| #define | CAN_WAKEUP_POLLING (STD_OFF) |
| #define | CAN_NUM_CONTROLLER (2U) |
| #define | CAN_NUM_MAILBOXES (7U) |
| #define | CAN_MAX_CONTROLLER (2U) |
| #define | CAN_MAX_MAILBOXES (64U) |
| #define | CAN_ISR_TYPE (CAN_ISR_CAT2) |
| #define | CLK_CAN_FD_FREQ (80U) |
Can Controller Id names | |
Defines for symbolic names for the CanControllerIds | |
| #define | CanConf_CanController_CanController_0 (0U) |
| #define | CanConf_CanController_CanController_1 (1U) |
| #define | CAN_CONTROLLER_MCU_MCAN0 |
| #define | CAN_CONTROLLER_MCU_MCAN1 |
| #define CAN_VARIANT_PRE_COMPILE (STD_ON) |
CAN Build Variant. Build variants.(i.e Pre Compile,Post Build)
| #define CAN_ISR_VOID (0x00U) |
void ISR type
| #define CAN_ISR_CAT1 (0x01U) |
Category 1 ISR type.
| #define CAN_ISR_CAT2 (0x02U) |
Category 2 ISR type.
| #define CAN_VERSION_INFO_API (STD_ON) |
Enable/Disable Can_GetVersionInfo()
| #define CAN_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable DEV error detection
| #define CAN_SAFETY_DIAGNOSTIC (STD_OFF) |
Enable/Disable Can Safety Diagnostic
| #define CAN_LOOPBACK_ENABLE (STD_ON) |
Enable/Disable Can_TestLoopBackModeEnable()
| #define CAN_REGISTER_READBACK_API (STD_ON) |
Enable/Disable Can_ConfigRegReadBack()
| #define CAN_SET_BAUDRATE_API (STD_ON) |
Enable/Disable Can_SetBaudrate() API
| #define CAN_WAKEUP_FUNCTIONALITY_API (STD_OFF) |
Enable/Disable Can_CheckWakeup()
| #define CAN_MULTIPLEXED_TRANSMISSION_ENABLE (STD_ON) |
Enable/Disable Multiplexed Transmission
| #define CAN_INIT_CONFIG_PC CanConfigSet |
Pre Compile config macro name.
| #define CAN_TX_POLLING (STD_OFF) |
Enable/Disable Can_MainFunction_Write
| #define CAN_RX_POLLING (STD_OFF) |
Enable/Disable Can_MainFunction_Read
| #define CAN_BUSOFF_POLLING (STD_OFF) |
Enable/Disable Can_MainFunction_BusOff
| #define CAN_WAKEUP_POLLING (STD_OFF) |
Enable/Disable Can_MainFunction_Wakeup
| #define CAN_NUM_CONTROLLER (2U) |
Number of controllers defined
| #define CAN_NUM_MAILBOXES (7U) |
Number of mailboxes defined
| #define CAN_MAX_CONTROLLER (2U) |
Max number of controller instances per SOC
| #define CAN_MAX_MAILBOXES (64U) |
Max number of mailboxes per controller
| #define CAN_ISR_TYPE (CAN_ISR_CAT2) |
OSEK Category 1 ISR Type
| #define CLK_CAN_FD_FREQ (80U) |
Clock source frequency CAN FD
| #define CanConf_CanController_CanController_0 (0U) |
| #define CanConf_CanController_CanController_1 (1U) |
| #define CAN_CONTROLLER_MCU_MCAN0 |
< MCU_MCAN0 CONTROLLER INSTANCE MCU_MCAN1 CONTROLLER INSTANCE
| #define CAN_CONTROLLER_MCU_MCAN1 |
| #define CanConf_CanHardwareObject_CanHardwareObject_0 (0U) |
| #define CAN_HTRH_0 (CanConf_CanHardwareObject_CanHardwareObject_0) |
| #define CanConf_CanHardwareObject_CanHardwareObject_1 (1U) |
| #define CAN_HTRH_1 (CanConf_CanHardwareObject_CanHardwareObject_1) |
| #define CanConf_CanHardwareObject_CanHardwareObject_2 (2U) |
| #define CAN_HTRH_2 (CanConf_CanHardwareObject_CanHardwareObject_2) |
| #define CanConf_CanHardwareObject_CanHardwareObject_3 (3U) |
| #define CAN_HTRH_3 (CanConf_CanHardwareObject_CanHardwareObject_3) |
| #define CanConf_CanHardwareObject_CanHardwareObject_4 (4U) |
| #define CAN_HTRH_4 (CanConf_CanHardwareObject_CanHardwareObject_4) |
| #define CanConf_CanHardwareObject_CanHardwareObject_5 (5U) |
| #define CAN_HTRH_5 (CanConf_CanHardwareObject_CanHardwareObject_5) |
| #define CanConf_CanHardwareObject_CanHardwareObject_6 (6U) |
| #define CAN_HTRH_6 (CanConf_CanHardwareObject_CanHardwareObject_6) |
| #define CAN_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks.
| #define CAN_TIMEOUT_DURATION (10000U) |
CAN timeout - used in CAN IFCMD busy wait and Start/Stop busy wait. Specifies the maximum time for blocking function until a timeout is detected. Unit is milli seconds.
| #define CAN_E_HARDWARE_ERROR (DemConf_DemEventParameter_CAN_E_HARDWARE_ERROR) |
Hardware failed.
| typedef uint8 CanControllerState_Type |
Can Controller State enum type.
| typedef uint32 Can_InterruptMask_Type |
Can Interrupt Mask type.
| enum Can_HandleType |
| enum Can_IrqStatusType |
CAN IRQ status enum.
| void Can_GetVersionInfo | ( | Std_VersionInfoType * | VersionInfo | ) |
Function returns the version information of this module.
* Service name : Can_GetVersionInfo * Syntax : void Can_GetVersionInfo(Std_VersionInfoType* versioninfo) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : versioninfo * Pointer to where to store the version information of this * module. * Return value : None * Description : This function returns the version information of this * module *
| void Can_Init | ( | const Can_ConfigType * | CfgPtr | ) |
This function initializes the module.
* Service name : Can_Init * Syntax : void Can_Init(const Can_ConfigType* CfgPtr) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : CfgPtr * Pointer to driver configuration. * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function initializes the module. *
| Std_ReturnType Can_SetControllerMode | ( | uint8 | Controller, |
| Can_ControllerStateType | Transition ) |
This function performs software triggered state transitions of the CAN controller State machine.
* Service name: Can_SetControllerMode * Syntax: Std_ReturnType Can_SetControllerMode(uint8 Controller, * Can_ControllerStateType Transition) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex]: 0x03 * Sync/Async: Asynchronous * Reentrancy: Non Reentrant * Parameters (in): Controller * - CAN controller for which the status shall be changed * Transition * - Transition value to request new CAN controller state * Parameters (inout): None * Parameters (out): None * Return value: Std_ReturnType * - E_OK: request accepted * - E_NOT_OK: request not accepted, a development error * occurred * Description: This function performs software triggered state transitions of * the CAN controller State machine. *
| Std_ReturnType Can_Write | ( | Can_HwHandleType | Hth, |
| const Can_PduType * | PduInfo ) |
This function is called by CanIf to pass a CAN message to CanDrv for transmission.
* Service name: Can_Write * Syntax : Std_ReturnType Can_Write(Can_HwHandleType Hth, const * Can_PduType* PduInfo) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex]: 0x06 * Sync/Async : Synchronous * Reentrancy : Reentrant (thread-safe) * Parameters (in): Hth * - Information which HW-transmit handle shall be used for * transmit. Implicitly this is also the information about * the controller to use because the Hth numbers are unique * inside one hardware unit. * PduInfo * - Pointer to SDU user memory, DLC and Identifier. * Parameters (inout): None * Parameters (out) : None * Return value: Std_ReturnType * - E_OK: Write command has been accepted * - E_NOT_OK: development error occurred * - CAN_BUSY: No TX hardware buffer available or pre-emptive call * of Can_Write that can't be implemented re-entrant * Description: This function is called by CanIf to pass a CAN message to CanDrv * for transmission. *
| void Can_DisableControllerInterrupts | ( | uint8 | Controller | ) |
This function disables all interrupts for this CAN controller.
* Service name : Can_DisableControllerInterrupts * Syntax : void Can_DisableControllerInterrupts(uint8 Controller) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN controller for which interrupts shall be disabled. * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function disables all interrupts for this CAN * controller * *
| void Can_EnableControllerInterrupts | ( | uint8 | Controller | ) |
This function enables all allowed interrupts.
* Service name : Can_EnableControllerInterrupts * Syntax : void Can_EnableControllerInterrupts(uint8 Controller) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN controller for which interrupts shall be re-enabled. * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function enables all allowed interrupts * *
| void Can_MainFunction_Write | ( | void | ) |
This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.
* Service name : Can_MainFunction_Write * Syntax : void Can_MainFunction_Write(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex]: 0x01 * Description : This function performs the polling of TX confirmation when * CAN_TX_PROCESSING is set to POLLING. * *
| void Can_MainFunction_BusOff | ( | void | ) |
This function performs the polling of bus-off events that are configured statically as 'to be polled'.
* Service name : Can_MainFunction_BusOff * Syntax : void Can_MainFunction_BusOff(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex]: 0x09 * Description : This function performs the polling of bus-off events that are * configured statically as 'to be polled'. * *
| void Can_MainFunction_Read | ( | void | ) |
This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.
* Service name : Can_MainFunction_Read * Syntax : void Can_MainFunction_Read(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex]: 0x08 * Description : This function performs the polling of RX indications when * CAN_RX_PROCESSING is set to POLLING. * *
| void Can_MainFunction_Wakeup | ( | void | ) |
This function performs the polling of wake-up events that are configured statically as 'to be polled'.
* Service name : Can_MainFunction_Wakeup * Syntax : void Can_MainFunction_Wakeup(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex]: 0x0A * Description : This function performs the polling of wake-up events that are * configured statically as 'to be polled'. * *
| void Can_MainFunction_Mode | ( | void | ) |
This function performs the polling of CAN controller mode transitions.
* Service name : Can_MainFunction_Mode * Syntax : void Can_MainFunction_Mode(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex]: 0x0C * Description : This function performs the polling of CAN controller mode * transitions. * *
| Std_ReturnType Can_SetBaudrate | ( | uint8 | Controller, |
| uint16 | BaudRateConfigID ) |
This service shall set the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset.
* * Function name : Can_SetBaudrate * Syntax : FUNC(Std_ReturnType, CAN_CODE) Can_SetBaudrate(uint8 * Controller, uint16 BaudRateConfigID) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0f * Sync/Async : Synchronous * Reentrancy : Reentrant for different Controllers. * Non reentrant for the same Controller. * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This service shall set the baud rate configuration * of the CAN controller. Depending on necessary baud rate * modifications the controller might have to reset. * *
| Std_ReturnType Can_TestLoopBackModeEnable | ( | uint8 | Controller, |
| uint8 | Mode ) |
This service will enable CAN loopback mode.
* * Service name : Can_TestLoopBackModeEnable * Syntax : Std_ReturnType Can_TestLoopBackModeEnable(uint8 * Controller, uint8 mode) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN Controller to enable loopback mode * mode * - Loopback mode * -# 0 - Digital Loopback * -# 1 - Analog Loopback * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Baudrate supported by the CAN Controller * - E_NOT_OK: Baudrate not supported / invalid CAN * Description : This service will enable CAN loopback mode. *
| Std_ReturnType Can_TestLoopBackModeDisable | ( | uint8 | Controller, |
| uint8 | Mode ) |
This service will disable CAN loopback mode.
* * Service name : Can_TestLoopBackModeDisable * Syntax : Std_ReturnType Can_TestLoopBackModeDisable(uint8 * Controller, uint8 Mode) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN Controller to enable loopback mode * mode * Loopback mode * -# 0 - Digital Loopback * -# 1 - Analog Loopback * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Loopback mode enabled in the CAN Controller * - E_NOT_OK: Loopback mode enable failed * Description : This service will disable CAN loopback mode. *
| Std_ReturnType Can_RegisterReadback | ( | VAR(uint8,) | Controller, |
| Can_RegisterReadbackType * | RegRbPtr ) |
This service will readback CAN registers.
* * Service name : Can_RegisterReadback * Syntax : Std_ReturnType Can_RegisterReadback(uint8 Controller) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - CAN Controller to readback registers configuration. * Parameters (inout): RegRbPtr - Pointer to where to store the readback * values. If this pointer is NULL_PTR, then the API * will return E_NOT_OK. * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Register readback successful. * - E_NOT_OK: Register readback failed. * Description : This service will readback CAN registers. *
This service will Enable the interrupts.
* * Service name : Can_EnableIntr * Syntax : Std_ReturnType Can_EnableIntr( * VAR(uint8, AUTOMATIC)Controller, * VAR(uint8, AUTOMATIC)CanErrVar); * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - Controller for which interrupt errors has * to be enabled. * - CanErrVar - CAN Error Type. * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Enabling Interrupts is success. * - E_NOT_OK: Enabling Interrupts failed. * Description : This service will Enable the interrupts. *
This service will Disable the Interrupts.
* * Service name : Can_DisableIntr * Syntax : Std_ReturnType Can_DisableIntr( * VAR(uint8, AUTOMATIC)Controller, * VAR(uint8, AUTOMATIC)CanErrVar) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - Controller for which interrupt errors has to * be Disabled. * - CanErrVar - CAN Error Type. * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Disabling Interrupts is success. * - E_NOT_OK: Disabling Interrupts failed. * Description : This service will Disable the Interrupts. *
| Can_IrqStatusType Can_GetIntrStatus | ( | VAR(uint8,) | Controller | ) |
This service will provide the status of the interrupt.
* * Service name : Can_GetIntrStatus * Syntax : Can_IrqStatusType Can_GetIntrStatus( * VAR(uint8, AUTOMATIC)Controller) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - Controller for which it reads the interrupt error * status. * Parameters (inout): None * Parameters (out) : None * Return value : Can_IrqStatusType * - CAN_IRQ_NO_INTR_EVENT: No Interrupt Event occured. * - CAN_IRQ_INTR_STUFF_EVENT: STUFF Error Event occured. * - CAN_IRQ_INTR_FORM_EVENT: FORM Error Event occured. * - CAN_IRQ_INTR_ACK_EVENT: ACK Error Event occured. * - CAN_IRQ_INTR_BIT1_EVENT: BIT1 Error Event occured. * - CAN_IRQ_INTR_BIT0_EVENT: BIT0` Error Event occured. * - CAN_IRQ_INTR_CRC_EVENT: CRC Error Event occured. * - CAN_IRQ_INTR_TOO_EVENT: TOO Error Event occured. * - CAN_IRQ_STATUS_READ_FAIL: Interrupt status read fail. * Description : This service will provide the status of the interrupt. *
| Std_ReturnType Can_ClearIntrStatus | ( | VAR(uint8,) | Controller | ) |
This service will clear the interrupt status.
* * Service name : Can_ClearIntrStatus * Syntax : Std_ReturnType Can_ClearIntrStatus( * VAR(uint8, AUTOMATIC)Controller) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Controller * - Controller for which it clears the interrupt * error status. * Parameters (inout): None * Parameters (out) : None * Return value : Std_ReturnType * - E_OK: Clearing Interrupt Status is Success. * - E_NOT_OK: Clearing Interrupt Status Failed. * Description : This service will clear the interrupt status. *
| void Can_IntISR_Fun | ( | Can_ControllerInstance | CanInstanceID | ) |
This function is the ISR for CAN controller 0/INT 0.
* * Function name : Can_IntISR_Fun * Syntax : void Can_IntISR_Fun(Can_ControllerInstance CanInstanceID) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : N/A * Sync/Async : Synchronous * Reentrancy : Non-Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function is the ISR for CAN controller 0/INT 0 <br> * This function should be invoked either by OS Interrupt * frame handler <br> * CAN Interrupt frame handler for Category 1 ISR *
| void Can_DeInit | ( | void | ) |
This function de-initializes the module.
* Service name : Can_DeInit * Syntax : void Can_DeInit(void) * Mode : Supervisor Mode (Privileged Mode) * Sync/Async : Synchronous * Reentrancy : Non-Reentrant * Parameters (in) : None * Parameters (inout): None * Parameters (out) : None * Return value : None * Description : This function de-initializes the module. *
| Std_ReturnType Can_GetControllerMode | ( | uint8 | Controller, |
| Can_ControllerStateType * | ControllerModePtr ) |
This service reports about the current status of the requested CAN controller.
* Service name: Can_GetControllerMode * Syntax: Std_ReturnType Can_GetControllerMode(uint8 Controller, * Can_ControllerStateType* ControllerModePtr) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex]: 0x12 * Sync/Async: Synchronous * Reentrancy: Non Reentrant * Parameters (in): Controller * - CAN controller for which the status shall be changed * Parameters (out): ControllerModePtr * - Pointer to a memory location, * where the current mode of the CAN controller will be stored. * Parameters (inout): None * Return value: Std_ReturnType * - E_OK: request accepted * - E_NOT_OK: request not accepted. * Description: This service reports about the current status of the requested * CAN controller. *
| Std_ReturnType Can_GetControllerErrorState | ( | uint8 | ControllerId, |
| Can_ErrorStateType * | ErrorStatePtr ) |
This service obtains the error state of the CAN controller.
* Service name: Can_GetControllerErrorState * Syntax: Std_ReturnType Can_GetControllerErrorState(uint8 Controller, * Can_ErrorStateType* ErrorStatePtr) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex]: 0x11 * Sync/Async: Synchronous * Reentrancy: Non Reentrant * Parameters (in): Controller * - CAN controller for which the status shall be changed * Parameters (out): ErrorStatePtr * - Pointer to a memory location, * where the error state of the CAN controller will be stored. * Parameters (inout): None * Return value: Std_ReturnType * - E_OK: request accepted * - E_NOT_OK: request not accepted * Description: This service obtains the error state of the CAN controller. *
| ISR | ( | Can_0_Int0ISR | ) |
| ISR | ( | Can_1_Int0ISR | ) |
| uint32 Can_MaskType::MaskValue |
Filter mask value.
| Can_IdType Can_HwFilterType::IDValue |
ID value extended will have MSB set
| uint32 Can_HwFilterType::Mask |
Mask for the RX filtering
| uint16 Can_FdBaudConfigType::Baud |
In Kbps
| uint8 Can_FdBaudConfigType::PropSeg |
Prop Segment value
| uint8 Can_FdBaudConfigType::Pseg1 |
Phase Segment 1
| uint8 Can_FdBaudConfigType::Pseg2 |
Phase Segment 2
| uint8 Can_FdBaudConfigType::Sjw |
Sync jump width
| uint16 Can_FdBaudConfigType::TimingValues |
Sum of all timing parameters *
| uint16 Can_FdBaudConfigType::BrpValue |
Controller BRP value for Baud
| uint16 Can_FdBaudConfigType::TrcvCompDelay |
Specifies the Transceiver Delay Compensation Offset in ns
| boolean Can_FdBaudConfigType::BrsSwitch |
Specifies if the bit rate switching shall be used for transmissions.
| uint16 Can_BaudConfigType::Baud |
In Kbps
| uint8 Can_BaudConfigType::PropSeg |
Prop Segment value
| uint8 Can_BaudConfigType::Pseg1 |
Phase Segment 1
| uint8 Can_BaudConfigType::Pseg2 |
Phase Segment 2
| uint8 Can_BaudConfigType::Sjw |
Sync jump width
| uint16 Can_BaudConfigType::TimingValues |
Sum of all timing parameters
| uint16 Can_BaudConfigType::BrpValue |
Controller BRP value for Baud
| Can_FdBaudConfigType Can_BaudConfigType::BaudFdRateConfig |
List of available Data phase Baud rates for CAN FD
| Can_BaudConfigType* Can_ControllerType::DefaultBaud |
pointer to default Baud structure
| Can_BaudConfigType** Can_ControllerType::BaudRateConfigList |
List of available Baud rates
| uint8 Can_ControllerType_PC::ControllerId |
Id as provided by GUI
| boolean Can_ControllerType_PC::CntrActive |
Contoller is used=1 or not_used=0
| uint32 Can_ControllerType_PC::CntrAddr |
Pointer to CanReg structure
| Can_TxRxProcessingType Can_ControllerType_PC::RxProcessingType |
Type can be Interrupt, Polling or Mixed
| Can_TxRxProcessingType Can_ControllerType_PC::TxProcessingType |
Type can be Interrupt, Polling or Mixed
| boolean Can_ControllerType_PC::BusOffProcessingInterrupt |
TRUE = Interrupt FALSE = Polling
| Can_ControllerInstance Can_ControllerType_PC::CanControllerInst |
Can Controller Instance
| boolean Can_ControllerType_PC::CanFDModeEnabled |
Controller is in CAN FD Mode or not
| uint8 Can_MailboxType::CanHandleType |
CanHandleType 0=Full, *1=Basic
| uint32 Can_MailboxType::MBIdType |
CanIdType 0=standard 1=Extended 2= Mixed
| Can_HwHandleType Can_MailboxType::HwHandle |
Mailbox - Hw object in the controller
| uint32 Can_MailboxType::CanHwObjectCount |
Number of hardware objects used to implement one HOH
| Can_MailBoxDirectionType Can_MailboxType::MBDir |
CanObjectType - Direction of Mailbox
| const Can_ControllerType_PC* Can_MailboxType::Controller |
Reference to CAN Controller to which the HOH is associated to.
| Can_HwFilterType** Can_MailboxType::HwFilterList |
List of HW Filter
| uint32 Can_MailboxType::HwFilterCnt |
HW Filter Count
| uint8 Can_MailboxType::CanFdPaddingValue |
If PduInfo->SduLength does not match possible DLC values CanDrv will use the next higher valid DLC for transmission with initialization of unused bytes to the value of the corresponding CanFdPaddingValue.
| boolean Can_MailboxType::CanHardwareObjectUsesPolling |
TRUE = Polling, FALSE = Interrupt
| uint16 Can_MailboxType_PC::CanObjectId |
CanObjectId - Holds handle Id
| uint32 Can_DmaPrms::Reserved |
Reserved for Future use, currently unused parameter
| Can_ControllerType** Can_ConfigType::CanControllerList |
List of enabled Controllers
| uint8 Can_ConfigType::CanMaxControllerCount |
MaxCount of Controller in Controller List
| Can_MailboxType** Can_ConfigType::MailBoxList |
MB array for all controllers
| uint32 Can_ConfigType::MaxMbCnt |
MaxMbCount in MB list in all controller
| uint32 Can_ConfigType::MaxBaudConfigID[CAN_MAX_CONTROLLER] |
Max Baud Config Index in BaudRateConfigList in all controller
| Can_DmaPrms* Can_ConfigType::DmaPrms |
Reserved for Future use, currently unused parameter
| uint32 Can_RegisterReadbackType::CanReadBackRegPID |
MCANSS PID Register
| uint32 Can_RegisterReadbackType::CanReadBackRegSTAT |
MCANSS STAT Register
| uint32 Can_RegisterReadbackType::CanReadBackRegCREL |
Auto Bus On Time Register
| uint32 Can_RegisterReadbackType::CanReadBackRegENDN |
Endianess MCAN_TEST value Constant "0x8765 4321"
| uint32 Can_RegisterReadbackType::CanReadBackRegCTRL |
MCAN CTRL Register
| uint32 Can_RegisterReadbackType::CanReadBackRegRWD |
MCAN RWD Register
| uint32 Can_RegisterReadbackType::CanReadBackRegCCCR |
MCAN CCCR Register
| uint32 Can_RegisterReadbackType::CanReadBackRegTDCR |
MCAN TDCR Register
| uint32 Can_RegisterReadbackType::CanReadBackRegGFC |
MCAN GFC Register
| uint32 Can_RegisterReadbackType::CanReadBackRegSIDFC |
MCAN SIDFC Register
| uint32 Can_RegisterReadbackType::CanReadBackRegXIDFC |
MCAN XIDFC Register
| uint32 Can_RegisterReadbackType::CanReadBackRegRXF0C |
MCAN RXF0C Register
| uint32 Can_RegisterReadbackType::CanReadBackRegRXBC |
MCAN RXBC Register
| uint32 Can_RegisterReadbackType::CanReadBackRegRXF1C |
MCAN RXF1C Register
| uint32 Can_RegisterReadbackType::CanReadBackRegTXBC |
MCAN TXBC Register
| uint32 Can_RegisterReadbackType::CanReadBackRegTXESC |
MCAN TXESC Register
| uint32 Can_RegisterReadbackType::CanReadBackRegTXEFC |
MCAN TXEFC Register
| uint32 Can_RegisterReadbackType::CanReadBackRegRXESC |
MCAN RXESC Register
| uint32 Can_RegisterReadbackType::CanReadBackRegXIDAM |
MCAN XIDAM Register
|
extern |
CAN Configuration struct declaration.
|
extern |
CAN Controller Configuration Pre Compile struct declaration.
|
extern |
CAN Controller Configuration Pre Compile struct declaration.
|
extern |
CAN Controller Pre Compile Configuration List.
|
extern |
CAN Mailbox Pre Compile Configuration List.
|
extern |
Base Address of the can peripherals.
|
extern |
|
extern |
|
extern |