102#include "EthTrcv_Types.h"
122#define ETHTRCV_SW_MAJOR_VERSION (11U)
124#define ETHTRCV_SW_MINOR_VERSION (0U)
126#define ETHTRCV_SW_PATCH_VERSION (3U)
139#define ETHTRCV_AR_RELEASE_MAJOR_VERSION (4U)
141#define ETHTRCV_AR_RELEASE_MINOR_VERSION (3U)
143#define ETHTRCV_AR_RELEASE_REVISION_VERSION (1U)
151#define ETHTRCV_VENDOR_ID (44U)
153#define ETHTRCV_MODULE_ID (73U)
155#define ETHTRCV_INSTANCE_ID (0U)
171#define ETHTRCV_INIT_ID ((uint8) 0x01U)
174#define ETHTRCV_CONTROLLER_INIT_ID ((uint8) 0x02U)
177#define ETHTRCV_SETTRCVMODE_ID ((uint8) 0x03U)
180#define ETHTRCV_GETTRCVMODE_ID ((uint8) 0x04U)
183#define ETHTRCV_SRTAUTONEGOTIA_ID ((uint8) 0x05U)
186#define ETHTRCV_GETLNKSTATE_ID ((uint8) 0x06U)
189#define ETHTRCV_GETBAUD_ID ((uint8) 0x07U)
192#define ETHTRCV_GETDPLXMODE_ID ((uint8) 0x08U)
195#define ETHTRCV_READMIIIND_ID ((uint8) 0x09U)
198#define ETHTRCV_WRITEMIIIND_ID ((uint8) 0x0AU)
201#define ETHTRCV_VERSION_ID ((uint8) 0x0BU)
204#define ETHTRCV_MAINFCT_WRITE_ID ((uint8) 0x0CU)
207#define ETHTRCV_GETTRCVWKUPMODE_ID ((uint8) 0x0DU)
210#define ETHTRCV_SETTRCVWKUPMODE_ID ((uint8) 0x0EU)
213#define ETHTRCV_CHKWKUP_ID ((uint8) 0x0FU)
216#define ETHTRCV_SETPHYTESTMODE_ID ((uint8) 0x10U)
219#define ETHTRCV_SETPHYLOOPBACKMODE_ID ((uint8) 0x11U)
222#define ETHTRCV_GETPHYSIGNALQUALITY_ID ((uint8) 0x12U)
225#define ETHTRCV_SETPHYTXMODE_ID ((uint8) 0x13U)
228#define ETHTRCV_GETCABLEDIAGNOSTICSRESULT_ID ((uint8) 0x014U)
231#define ETHTRCV_GETPHYIDENTIFIER_ID ((uint8) 0x015U)
246#ifndef ETHTRCV_E_INV_TRCV_IDX
248#define ETHTRCV_E_INV_TRCV_IDX ((uint8) 0x01U)
251#ifndef ETHTRCV_E_UNINIT
253#define ETHTRCV_E_UNINIT ((uint8) 0x02U)
256#ifndef ETHTRCV_E_PARAM_POINTER
258#define ETHTRCV_E_PARAM_POINTER ((uint8) 0x03U)
261#ifndef ETHTRCV_E_INIT_FAILED
263#define ETHTRCV_E_INIT_FAILED ((uint8) 0x04U)
266#ifndef ETHTRCV_E_NOT_SUPPORTED
268#define ETHTRCV_E_NOT_SUPPORTED ((uint8) 0x05U)
303FUNC(
void, ETHTRCV_CODE)
304EthTrcv_Init(P2CONST(EthTrcv_ConfigType, AUTOMATIC, ETHTRCV_PBCFG) CfgPtr);
329FUNC(Std_ReturnType, ETHTRCV_CODE)
333#if (STD_ON == ETHTRCV_SETTRANSCEIVERMODE_API)
360FUNC(Std_ReturnType, ETHTRCV_CODE)
362 EthTrcv_ModeType CtrlMode);
365#if (STD_ON == ETHTRCV_GETTRANSCEIVERMODE_API)
389FUNC(Std_ReturnType, ETHTRCV_CODE)
391 EthTrcv_ModeType *TrcvModePtr);
394#if (ETHTRCV_WAKEUPSUPPORT_API != ETHTRCV_WAKEUP_NOT_SUPPORTED)
426FUNC(Std_ReturnType, ETHTRCV_CODE)
427EthTrcv_SetTransceiverWakeupMode(uint8 TrcvIdx,
428 EthTrcv_WakeupModeType TrcvWakeupMode);
431#if (ETHTRCV_WAKEUPSUPPORT_API != ETHTRCV_WAKEUP_NOT_SUPPORTED)
458FUNC(Std_ReturnType, ETHTRCV_CODE)
459EthTrcv_GetTransceiverWakeupMode(uint8 TrcvIdx,
460 EthTrcv_WakeupModeType *TrcvWakeupModePtr);
463#if (ETHTRCV_WAKEUPSUPPORT_API != ETHTRCV_WAKEUP_NOT_SUPPORTED)
489FUNC(Std_ReturnType, ETHTRCV_CODE)
490EthTrcv_CheckWakeup(uint8 TrcvIdx);
496#if (STD_ON == ETHTRCV_STARTAUTONEGOTIATION_API)
521FUNC(Std_ReturnType, ETHTRCV_CODE)
525#if (STD_ON == ETHTRCV_GETLINKSTATE_API)
551FUNC(Std_ReturnType, ETHTRCV_CODE)
553 EthTrcv_LinkStateType *LinkStatePtr);
561#if (STD_ON == ETHTRCV_GETBAUDRATE_API)
588FUNC(Std_ReturnType, ETHTRCV_CODE)
590 EthTrcv_BaudRateType *BaudRatePtr);
593#if (STD_ON == ETHTRCV_GETDUPLEXMODE_API)
619FUNC(Std_ReturnType, ETHTRCV_CODE)
621 EthTrcv_DuplexModeType *DuplexModePtr);
624#if (STD_ON == ETHTRCV_SETPHYTESTMODE_API)
647FUNC(Std_ReturnType, ETHTRCV_CODE)
649 EthTrcv_PhyTestModeType Mode);
652#if (STD_ON == ETHTRCV_SETPHYLOOPBACKMODE_API)
676FUNC(Std_ReturnType, ETHTRCV_CODE)
678 EthTrcv_PhyLoopbackModeType Mode);
681#if (STD_ON == ETHTRCV_GETPHYSIGNALQUALITY_API)
706FUNC(Std_ReturnType, ETHTRCV_CODE)
708 uint32* SignalQualityPtr);
711#if (STD_ON == ETHTRCV_SETPHYTXMODE_API)
735FUNC(Std_ReturnType, ETHTRCV_CODE)
737 EthTrcv_PhyTxModeType Mode);
740#if (STD_ON == ETHTRCV_GETCABLEDIAGNOSTICSRESULT_API)
765FUNC(Std_ReturnType, ETHTRCV_CODE)
767 EthTrcv_CableDiagResultType * ResultPtr);
770#if (STD_ON == ETHTRCV_GETPHYIDENTIFIER_API)
803FUNC(Std_ReturnType, ETHTRCV_CODE)
805 uint32* OrgUniqueIdPtr,
807 uint8* RevisionNrPtr);
810#if (STD_ON == ETHTRCV_VERSION_INFO_API)
832FUNC(
void, ETHTRCV_CODE)
872FUNC(
void, ETHTRCV_CODE)
907FUNC(
void, ETHTRCV_CODE)
931FUNC(
void, ETHTRCV_CODE)
Std_ReturnType EthTrcv_GetLinkState(uint8 TrcvIdx, EthTrcv_LinkStateType *LinkStatePtr)
This function obtains the link state of the indexed transceiver.
Std_ReturnType EthTrcv_SetPhyTxMode(uint8 TrcvIdx, EthTrcv_PhyTxModeType Mode)
This function Activates a given transmission mode.
Std_ReturnType EthTrcv_GetTransceiverMode(uint8 TrcvIdx, EthTrcv_ModeType *TrcvModePtr)
This function obtains the state of the indexed transceiver.
void EthTrcv_Init(const EthTrcv_ConfigType *CfgPtr)
This function initializes the Ethernet Transceiver controller. All the required initialization for th...
Std_ReturnType EthTrcv_GetDuplexMode(uint8 TrcvIdx, EthTrcv_DuplexModeType *DuplexModePtr)
This function obtains the duplex mode of the indexed transceiver.
void EthTrcv_ReadMiiIndication(uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegIdx, uint16 RegVal)
This function is called when information has been read out via MII interface. Triggered by previous E...
Std_ReturnType EthTrcv_GetPhyIdentifier(uint8 TrcvIdx, uint32 *OrgUniqueIdPtr, uint8 *ModelNrPtr, uint8 *RevisionNrPtr)
This function Obtains the PHY identifier of the Ethernet Transceiver according to IEEE 802....
void EthTrcv_GetVersionInfo(Std_VersionInfoType *VersionInfoPtr)
Function returns the version information of this module.
void EthTrcv_MainFunction(void)
This function is used for polling state changes and wakeup reasons. It calls EthIf_TrcvModeIndication...
Std_ReturnType EthTrcv_GetCableDiagnosticsResult(uint8 TrcvIdx, EthTrcv_CableDiagResultType *ResultPtr)
This function Retrieves the cable diagnostics result of a given transceiver.
Std_ReturnType EthTrcv_SetPhyTestMode(uint8 TrcvIdx, EthTrcv_PhyTestModeType Mode)
This function Activates a given test mode.
Std_ReturnType EthTrcv_GetBaudRate(uint8 TrcvIdx, EthTrcv_BaudRateType *BaudRatePtr)
This function obtains the baud rate of the indexed transceiver.
Std_ReturnType EthTrcv_GetPhySignalQuality(uint8 TrcvIdx, uint32 *SignalQualityPtr)
This function Obtains the current signal quality of the link of the indexed transceiver.
Std_ReturnType EthTrcv_SetTransceiverMode(uint8 TrcvIdx, EthTrcv_ModeType CtrlMode)
This function enables / disables the indexed transceiver.
Std_ReturnType EthTrcv_TransceiverInit(uint8 TrcvIdx)
This function initializes the Ethernet Transceiver controller. All the required initialization for th...
void EthTrcv_WriteMiiIndication(uint8 CtrlIdx, uint8 TrcvIdx, uint8 RegId)
This function is called when information has been written via MII interface. Triggered by previous Et...
Std_ReturnType EthTrcv_StartAutoNegotiation(uint8 TrcvIdx)
This function restarts the negotiation of the transmission parameters used by the indexed.
Std_ReturnType EthTrcv_SetPhyLoopbackMode(uint8 TrcvIdx, EthTrcv_PhyLoopbackModeType Mode)
This function Activates a given loopback mode.