107#include "Std_Types.h"
129#define DIO_SW_MAJOR_VERSION (10U)
131#define DIO_SW_MINOR_VERSION (1U)
133#define DIO_SW_PATCH_VERSION (3U)
143#define DIO_AR_RELEASE_MAJOR_VERSION (4U)
145#define DIO_AR_RELEASE_MINOR_VERSION (3U)
147#define DIO_AR_RELEASE_REVISION_VERSION (1U)
155#define DIO_VENDOR_ID ((uint16) 44U)
157#define DIO_MODULE_ID ((uint16) 120U)
169#ifndef DIO_E_PARAM_INVALID_CHANNEL_ID
171#define DIO_E_PARAM_INVALID_CHANNEL_ID (0x0AU)
176#ifndef DIO_E_PARAM_INVALID_PORT_ID
178#define DIO_E_PARAM_INVALID_PORT_ID (0x14U)
183#ifndef DIO_E_PARAM_INVALID_GROUP
185#define DIO_E_PARAM_INVALID_GROUP (0x1FU)
190#ifndef DIO_E_PARAM_POINTER
192#define DIO_E_PARAM_POINTER (0x20U)
205#define DIO_SID_READ_CHANNEL (0U)
207#define DIO_SID_WRITE_CHANNEL (1U)
209#define DIO_SID_READ_PORT (2U)
211#define DIO_SID_WRITE_PORT (3U)
213#define DIO_SID_READ_CHL_GROUP (4U)
215#define DIO_SID_WRITE_CHL_GROUP (5U)
217#define DIO_SID_FLIP_CHANNEL (17U)
219#define DIO_SID_GET_VERSION_INFO (18U)
227#define DIO_PORT_WIDTH (32U)
230#define DIO_MCAL_2139_FIXED (0U)
301#if (STD_ON == DIO_REGISTER_READBACK_API)
457#if (STD_ON == DIO_VERSION_INFO_API)
478 P2VAR(Std_VersionInfoType, AUTOMATIC, DIO_APPL_DATA) versioninfo);
481#if (STD_ON == DIO_FLIP_CHANNEL_API)
511#if (STD_ON == DIO_REGISTER_READBACK_API)
This file contains generated pre compile configuration file for DIO MCAL driver.
Dio_LevelType Dio_FlipChannel(Dio_ChannelType ChannelId)
Service to flip (change from 1 to 0 or from 0 to 1) the level of a channel and return the level of th...
uint32 Dio_PortType
type definition for identifying ports
Definition Dio.h:253
uint32 Dio_PortLevelType
type definition for setting port level values
Definition Dio.h:264
void Dio_WritePort(Dio_PortType PortId, Dio_PortLevelType Level)
Service to set a value of the port.
void Dio_GetVersionInfo(Std_VersionInfoType *versioninfo)
Service to get the version information of this module.
void Dio_WriteChannelGroup(const Dio_ChannelGroupType *ChannelGroupIdPtr, Dio_PortLevelType Level)
Service to set a subset of the adjoining bits of a port to a specified level.
uint8 Dio_LevelType
type definition for setting DIO channnel level values (allowed values: STD_HIGH and STD_LOW)
Definition Dio.h:289
Dio_DirectionType
Definition Dio.h:295
Dio_PortLevelType Dio_ReadPort(Dio_PortType PortId)
Returns the level of all channels of that port.
Dio_LevelType Dio_ReadChannel(Dio_ChannelType ChannelId)
Returns the value of the specified DIO channel.
uint32 Dio_ChannelType
type definition for identifying DIO channels (meaning single port pins)
Definition Dio.h:247
void Dio_WriteChannel(Dio_ChannelType ChannelId, Dio_LevelType Level)
Service to set a level of a channel.
Std_ReturnType Dio_RegisterReadback(Dio_ChannelType ChannelId, Dio_RegisterReadbackType *DioRegRbPtr)
This function reads the important registers of the hardware unit and returns the value in the structu...
Dio_PortLevelType Dio_ReadChannelGroup(const Dio_ChannelGroupType *ChannelGroupIdPtr)
This Service reads a subset of the adjoining bits of a port.
uint8 offset
Definition Dio.h:277
Dio_PortType port
Definition Dio.h:273
uint32 pid
Definition Dio.h:307
Dio_PortLevelType mask
Definition Dio.h:275
Dio_DirectionType Dio_Direction
Definition Dio.h:309
@ DIO_DIR_OUTPUT
Definition Dio.h:297
@ DIO_DIR_INPUT
Definition Dio.h:296
Type definition for identifying channel groups (meaning a set of pins in one port)
Definition Dio.h:272