MCUSW
Loading...
Searching...
No Matches
Pwm User Guide

Introduction

This document details AUTOSAR BSW PWM module implementation

  • Supported AUTOSAR Release : 4.3.1
  • Supported Configuration Variants : Pre-Compile & Post-Build
  • Vendor ID : PWM_VENDOR_ID (44)
  • Module ID : PWM_MODULE_ID (121)

The PWM module initializes, configures and controls the internal hardware to realize PWM driver as detailed in AUTOSAR BSW PWM Driver Specification. The PWM functionality is realized through the ePWM IP available on the device. Following section highlights key aspects of this implementation, which would be of interest to an integrator.

Note: This module is not applicable for MPU device AM62X.


Pwm Driver Architecture/Design

Please refer the PWM design, which is part of CSP.


Functional Description

Clock Source to timers

Programming of clock source for the PWM module, is beyond the scope of this document. The driver expects that the user of this module has programmed required clock source. The example application demonstrates configuring clock sources for the timer and ePWM, respectively.

Note: Each PWM instance has 2 outputs and same output is available in both channels.

Back To Top


Pwm Channel ID , Instance mapping and ISR mapping

The Pwm module is implemented using the ePWM IP instances on the device.

ePWM

All ePWM instances are supported by this driver implementation (all instances present in MAIN domain). The following table lists the mapping between instance of ePWM and PwmChannelId of the configurator.

‍Note:
In AM275x SOC, PWM interrupts are not routed to R5F Core and hence PWM driver do not support the notifications feature. The below table is for other than AM275x SoC.

PwmChannelId ePWM Instance ePWM channel/signal Associated ISR (if notification is enabled)
0 EPWM0 EPWM0A, EPWM0B Pwm_Ch0Notify
1 EPWM1 EPWM1A, EPWM1B Pwm_Ch1Notify
2 EPWM2 EPWM2A, EPWM2B Pwm_Ch2Notify

Back To Top


Configuration

The Pwm Driver implementation supports multiple configuration variants (refer section Introduction), the driver expects generated Pwm_Cfg.h to be present as (File Structure). Please refer (Build) to specify path to generated configuration. The associated timer configuration generated files Pwm_Cfg.c and Pwm_PBcfg.c to be present as show (File Structure)

Note: For detailed descriptions of all configurable parameters, refer to the design document provided in the CSP package. The document is located at: "$(MCAL_INSTALL_PATH)/mcusw/csp"

The following section details on the un-supported features and additional features added.


Variance / Deviation from the specification

Note: AEP will not support EHRPWM feature because of hardware limitation.

APIs related to power state

APIs related to setting or getting power state of the device is not supported, as the hardware itself doesn’t support this feature.

Back To Top


PwmMcuClockReference

To configure the clock source for Pwm (Timer/ePWM hardware), one would have to access/configure common registers. It’s recommended that clock sources for the Pwm (Timer/ePWM hardware) are done in SBL / Start up code. Please refer to example application.


PWM_FIXED_PERIOD_SHIFTED

The PWM_FIXED_PERIOD_SHIFTED, Pwm Channel Class type is not supported in this implementation.


PwmTimeoutDuration

The timeout value parameter PwmTimeoutDuration to be configured in the configurator plugin should be purely based on R5F core frequency. Driver internally uses MCAL_SW_DELAY() is a SW delay of 9 CPU cycles per iteration.


Implementation Specific Configurations

This driver implementation introduces below listed configurable options

Back To Top


PwmDeviceVariant

Name PwmDeviceVariant
Description Used to specific family of devices, the variant of the device being used will belong one or more family of devices. Please refer (Supported Devices) to determine the family of device. Based on the family, the number of instances of Timer module supported could vary.
Container Name PwmDriverConfiguration
Type Enumeration
Range AM62X, AM62AX etc… (new family of devices could be added in future)
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


PwmTypeofInterruptFunction

Name PwmTypeofInterruptFunction
Description Specifies category of ISR.
Container Name PwmDriverConfiguration
Type Enumeration
Range PWM_ISR_CAT1 & PWM_ISR_CAT2
Value Configuration Class VARIANT-PRE-COMPILE
Note This implementation has been validated with PWM_ISR_CAT1 only

Back To Top


PwmDefaultOSCounterId

Name PwmDefaultOSCounterId
Description Specifies the OS counter to be used by the driver. All wait operations (wait for hardware timer module reset to complete) are time bound. This implementation uses OS calls (GetCounterValue () & GetElapsedValue ()) to get current and elapsed time to establish time bound operation. In cases where a constant value is returned / OS call is not operational, the time bound operation cannot be realized.
Container Name PwmDriverConfiguration
Type Boolean
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


PwmEnableRegisterReadbackApi

Name PwmEnableRegisterReadbackApi
Description Adds / Removes service API Pwm_RegisterReadback ()
Safety feature : Some of the critical registers (corruption of which
could potentially break functionality of the Pwm/Timer)
The expected usage: Periodically this service API is invoked and
checked for data-consistency. i.e. the values of members of structure
Pwm_RegisterReadbackType is not expected to change.
Also refer (@ref ug_pwm_functional_i_cfg_s_api_imp)
Container Name PwmConfigurationOfOptApiServices
Type Boolean
Value Configuration Class VARIANT-PRE-COMPILE

Back To Top


PwmClkPrescaler

Name PwmClkPrescaler
Description Used configure divider for the input clock This parameter could be used to divide this clock before it’s used to count.
Container Name PwmChannelConfigSet
Type uint8
Range 0 to 7
Value Configuration Class VARIANT-PRE-COMPILE & VARIANT-POST-BUILD

Back To Top


PwmPolarity

Name PwmPolarity
Description This parameter stores the initial polarity configured for a channel
Container Name PwmChannelConfigSet
Type Enummeration
Range PWM_HIGH, PWM_LOW
Value Configuration Class VARIANT-PRE-COMPILE & VARIANT-POST-BUILD

Back To Top


PwmIdleState

Name PwmIdleState
Description This parameter stores the initial polarity configured for a channel
Container Name PwmChannelConfigSet
Type Enummeration
Range PWM_HIGH , PWM_LOW
Value Configuration Class VARIANT-PRE-COMPILE & VARIANT-POST-BUILD

Back To Top


PwmIndex

Name PwmIndex
Description Specifies the InstanceId of this module instance.
Container Name PwmGeneral
Type uint8
Range 0, 1
Value Configuration Class VARIANT-PRE-COMPILE & VARIANT-POST-BUILD

Back To Top


ePWM Specific:


PwmHSClkPrescaler

Name PwmHSClkPrescaler
Description Used configure divider for the input clock This parameter allows the selection of High Speed pre-scalar value. The High Speed prescaler stage is clocked with the pwm clock and acts as a clock divider for the time-base clock.
Container Name PwmChannelConfigSet
Type uint8
Range 0 to 7
Value Configuration Class VARIANT-PRE-COMPILE & VARIANT-POST-BUILD

Back To Top


PwmEnableHighRes

Name PwmEnableHighRes
Description This parameter will be a switch to enable or disable high resolution (HRPWM) capability of EPWM module.
Container Name PwmChannelConfigSet
Type Boolean
Value Configuration Class VARIANT-PRE-COMPILE & VARIANT-POST-BUILD

Back To Top


PwmOutputChSelect

Name PwmOutputChSelect
Description PWM Output Channel select EPWMxA or EPWMxB or Both. Both Outputs available with same duty cycle, period and polarity.
Container Name PwmChannelConfigSet
Type Enummeration
Range EPWM_OUTPUT_CH_A , EPWM_OUTPUT_CH_B, EPWM_OUTPUT_CH_BOTH_A_AND_B
Value Configuration Class VARIANT-PRE-COMPILE & VARIANT-POST-BUILD

Back To Top


Non Standard Service APIs


Pwm_RegisterReadback

To protect HW from un-intended re-configuration (corrupted / fault hardware), some of the critical registers are read periodically and checked. By an entity outside the driver, the values of these registers are not expected to change. This is an optional service API, which can be turned OFF (refer section PwmEnableRegisterReadbackApi)

Service Name Pwm_RegisterReadback
Syntax void Pwm_RegisterReadback (Pwm_ChannelType PwmChannel, Pwm_RegisterReadbackType * RegRbPtr)
Service ID[hex] 0x0F
Sync/Async Synchronous
Reentrancy Reentrant (but not for the same timer channel)
Parameters (in) PwmChannel : Numeric identifier of the PWM channel
Parameters (inout) RegRbPtr : Pointer of type Pwm_RegisterReadbackType
Parameters (out) None
Return Value E_OK: Register read back has been done E_NOT_OK: Register read back failed (if channel is not initialized or RegRbPtr is NULL_PTR
Description Reads the important registers of the hardware unit and returns the value in the structure.

Back To Top


Interrupt Configuration

The Driver doesn’t register any interrupts handler (ISR), it’s expected that consumer of this driver registers the required interrupt handler.

For every Pwm channel with notification enabled, an ISR requires to be registered. The Interrupt number associated with instance of the Timer or ePWM is detailed in TRM (also, please refer the demo application). Please refer PwmApp_InterruptConfig () in Pwm demo application.

Some of the Timer and ePWM interrupts are not routed/mapped to this core, these interrupts would require additional programming to route these to this core. Please refer PwmApp_InterruptConfig () in Pwm demo application.

Refer section (Pwm Channel ID , Instance mapping and ISR mapping), for association between channel ID and ISR

Back To Top


Power-up

The driver doesn't configure the functional clock and power for the timer modules. Its expected that SBL power-up the required modules. Please refer SBL documentation.

Back To Top


Build and Running the Example Application

Please follow steps detailed in section (Build) to build library or example.

  1. ePWM based application name - pwm_app_epwm

Please note that a clean build for building these applications. Building both together will cause build errors. Build only one at a time.

Back To Top


Steps to run example application

Please refer (Running Examples)

Back To Top


Memory Mapping

Various objects of this implementation (e.g. variables, functions, constants) are defined under different sections. The linker command file at (Examples Linker File (Select memory location to hold example binary)) defines separate section for these objects. When the driver is integrated, its expected that these sections are created and placed in appropriate memory locations. (Locations of these objects depend on the system design and performance needs)

Section PWM_CODE PWM_VAR_INIT PWM_VAR_NOINIT PWM_CONST PWM_CONFIG
PWM_START_SEC_VAR_INIT_UNSPECIFIED (.data) USED
PWM_DATA_INIT_32_SECTION USED
PWM_TEXT_SECTION USED
PWM_DATA_NO_INIT_UNSPECIFIED_SECTION USED
PWM_CONST_32_SECTION USED
PWM_ISR_TEXT_SECTION USED
PWM_CONFIG_SECTION USED

Back To Top


Cache

This driver implementation has been validated with cache enabled. For optimal performance it’s recommended to place (Memory Mapping) sections in cache enabled memory area.

Back To Top


Prescaler/Dividers for ePWM based implementation

Setting Prescalers: Period value(Num of ticks) which determines the period is calculated using below formula:

  • PRD = (TBCLK/PWM_FREQ) / 2.
  • TBCLK – Time base clock relative to the system clock.
  • PWM_FREQ – Required output frequency.
  • /2 – Because UpDown counter is selected.(Please refer DAR for more details). The TRM gives details on this formula.
  • TBCLK is derived from below formula.
  • TBCLK = SYS_CLK / (HSPCLKDIV x CLKDIV)
  • SYS_CLK – System Clock to the PWM which is 125Mhz.
  • CLKDIV – Time-base Clock Prescale Bits. These bits determine part of the time-base clock prescale value.

Actual Division Value = / ( 1 << CLKDIV) i.e

Actual Division Value CLKDIV Value
0x0 / 1
0x1 / 2
0x2 / 4
0x3 / 8
0x4 / 16
0x5 / 32
0x6 / 64
0x7 / 128
  • HSPCLKDIV – High-Speed Time-base Clock Prescale Bits. These bits determine part of the time-base clock prescale value.

Actual Division Value = / (HSPCLKDIV * 2) i.e

Actual Division Value HSPCLKDIV
0x0 / 1
0x1 / 2
0x2 / 4
0x3 / 6
0x4 / 8
0x5 / 10
0x6 / 12
0x7 / 14

There is a chance that period value calculated is fractional, and therefore required frequency cannot be achieved. The clock dividers need to be selected correctly to avoid such errors. Please refer to the excel sheet provided to derive the correct CLKDIV and HSPCLKDIV values. Using this excel, you can test prescaler combinations with required frequency and ensure that the "Difference" is 0. The Period value should be less than or equal to 65535 (16bit HW register size for period).

Find the excel sheet here: <../../mcusw/mcal_drv/docs/Pwm_Frequency_Prescalers.xlsx>

User/Application need to note that these prescalers are configured in Pwm_Init time and cannot be changed run time. User has to consider same prescaler values, configure new period and need to see whether new period can be achieved or not using above excel.

In case if user is not able to set new period with the same prescalers combination then he need to call Pwm_DeInit and call Pwm_Init with the new prescalers combination which helps in achieving required period.

Back To Top


Dependencies on SW Modules


DET

This implementation depends on the DET in order to report development errors and can be turned OFF. Refer section (Development Error Reporting) for detailed error codes.

Back To Top


SchM

This implementation requires 1 level of exclusive access to guard critical sections. Invokes SchM_Enter_Pwm_PWM_EXCLUSIVE_AREA_0 (), SchM_Exit_Pwm_PWM_EXCLUSIVE_AREA_0 () to enter critical section and exit.

In the example implementation (File Structure SchM_Pwm.c) , all the interrupts on CPU are disabled. However, disabling of the enabled Timer/Pwm interrupt should suffice.

Back To Top


File Structure

Detailed Directory Structure
  1. Driver implemented by : Pwm.h, Pwm_Irq.h, Pwm.c, Pwm_Gptimer.c, Pwm_Priv.c ,Pwm_Irq.c, Pwm_Ehrpwm.c and Pwm_Priv.h

Note: For MPU devices, PWM generation using timers is not supported; hence, the "Pwm_Gptimer.c" file is not applicable.

Example Application :

  • There will be two separate example applications for PWM module: PwmApp_Gpt and PwmApp_Epwm. Please refer to below directory structures. Each application will have its own configuration as well, since each IP uses different Cfg files.
  • Config files for PwmApp_Gpt are located along with other applications' demo configs at /workarea/mcusw/mcal_drv/mcal/example_configs/Pwm_Demo_Cfg.
  • Config files for PwmApp_Epwm are located within the example folder at /workarea/mcusw/mcal_drv/mcal/example/Pwm/PwmApp_Epwm/Pwm_Demo_Cfg.
  • Pwm_Cfg.h: Contains statuc configuration of this module.
  • Pwm_Cfg.c: Shail implement the generated configuration for pre-compile variant.
  • Pwm_PBcfg.c: Shall implement the generated configuration for post-build variant
  • PwmApp_Startup.c and PwmApp_Startup.h: Shall implement the start-up code sequence and register interrupts.
  • PwmApp.c and PwmApp.h: Shall implement the example application that demonstrates the use of the driver

Back To Top


Error Handling


Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface (Pwm.h File Structure) lists the SID

Back To Top


Error codes

Type of Error Related Error code Value (Hex)
API Pwm_Init service called with wrong parameter PWM_E_PARAM_CONFIG 0x10
API service used without module initialization PWM_E_UNINIT 0x11
API service used with an invalid channel Identifier PWM_E_PARAM_CHANNEL 0x12
Usage of unauthorized PWM service on PWM channel configured a fixed period PWM_E_PERIOD_UNCHANGEABLE 0x13
API Pwm_Init service called while the PWM driver has already been initialised PWM_E_ALREADY_INITIALIZED 0x14
API Pwm_GetVersionInfo is called with a NULL parameter. PWM_E_PARAM_POINTER 0x15

Back To Top


API Description

The AUTOSAR BSW PWM Driver specification details the APIs required for Pwm Driver. Please refer to PWM Design Document for detailed API description. APIs related to setting/ getting the power state are not implemented, please refer to (Variance / Deviation from the specification). Also refer to (Non Standard Service APIs) for non-standard APIs which are included in this implemented.

Refer API Documentation for details

Back To Top


Example Application

PwmApp_Epwm

The example application demonstrate use of ePWM based Pwm module, the list below identifies key steps performed the example. The configuration file is present at (File Structure)

  • AM62PX: The EPWM Pin 24 (D20) on J3 connector in MCU domain can be probed to check the output EPWM signals.
  • AM62AX: The EPWM Pin 24 (D16) on J3 connector in MCU domain can be probed to check the output EPWM signals.
  • AM62DX: The EPWM Pin 3 (EXP_EHRPWM0_A) on Audio Expansion Connector #2 board (AEC #2) can be probed to check the output EPWM signals.
  • AM275x: The EPWM Pin 3 (EPWM1_A) on Audio Expansion Connector #2 board (AEC #2) can be probed to check the output EPWM signals. These pins will change based on the EVM used.
  • Initializes “Result Status Flag”
  • PwmApp_Startup ()
    • Initialize board for pin mux
    • Initialize the control mmr registers for epwm io muxing
    • Builds interrupt list and registers ISR for the enabled Pwm channel
    • Sets up clock sources for the ePWM modules
  • PwmApp_mainTest ()
    • Initialize and start PWM module (duty cycle 60%)
    • Set duty cycle to 80% (if API is enabled)
    • Set output to idle state (if API is enabled)
    • Enable the channel again using Set period and duty (if API is enabled)
    • Enables Notification and check the notifications received in 30 secs (if notification is enabled). Count the notifications received to make sure matched expected count.
    • Disable notification (if notification is enabled)
    • De-initialize and Stop Pwm
  • Checks for error status, stack corruption and prints result

Back To Top


Example Log

AM62AX - PwmApp_Epwm

        PWM_APP_EPWM: Sample Application - STARTS !!!
        PWM_APP_EPWM: EPWM being used with Channel # 0!!!
        
        PWM_APP_EPWM: PWM MCAL Version Info
        ---------------------
        PWM_APP_EPWM: Vendor ID           : 44
        PWM_APP_EPWM: Module ID           : 121
        PWM_APP_EPWM: SW Major Version    : 10
        PWM_APP_EPWM: SW Minor Version    : 1
        PWM_APP_EPWM: SW Patch Version    : 0
        
        PWM_APP_EPWM: Variant - Pre Compile being used !!!
        
        PWM_APP_EPWM: PWM Channel Initialized 
        PWM_APP_EPWM: PWM Duty cycle: 60 Percent, 2000Hz 
        PWM_APP_EPWM: PWM CHANNEL 0 configuration Register Readback values  
        PWM_APP_EPWM: EPWM_TBCTL                : 0x8032
        PWM_APP_EPWM: EPWM_TBPHS                : 0x0
        PWM_APP_EPWM: EPWM_TBCNT                : 0xc459
        PWM_APP_EPWM: EPWM_AQCTLA               : 0xf2
        PWM_APP_EPWM: EPWM_AQCTLB               : 0xf02
        PWM_APP_EPWM: EPWM_DBCTL                : 0x0
        PWM_APP_EPWM: EPWM_TZSEL                : 0x0
        PWM_APP_EPWM: EPWM_TZCTL                : 0x0
        PWM_APP_EPWM: EPWM_PCCTL                : 0x0
        PWM_APP_EPWM: EPWM_TBSTS                : 0x1
        PWM_APP_EPWM: EPWM_TBPRD                : 0xf424
        PWM_APP_EPWM: EPWM_AQSFRC               : 0xd2
        PWM_APP_EPWM: EPWM_AQSCFRC              : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: Probe EPWM in MCU domain Test Pin D16(pin 24) on J3 connector on EVM in AM62AX EVM
        PWM_APP_EPWM: This example waits for 30 seconds please probe
        
        PWM_APP_EPWM: Changing the Duty cycle from to 60 to 80 percent 
        PWM_APP_EPWM: This example waits for 30 seconds Please probe
        
        PWM_APP_EPWM: Changing the Duty cycle to 100 Percent 
        PWM_APP_EPWM: This example waits for 10 seconds Please probe
        
        PWM_APP_EPWM: Setting Output to Idle state 
        PWM_APP_EPWM: This example waits for 10 seconds Please probe
        
        PWM_APP_EPWM: Changing Frequency from 1kHz to 10KHz and Duty Cycle to 50%
        PWM_APP_EPWM: period is set to 12500
        PWM_APP_EPWM: This example validating through ISR count
        PWM_APP_EPWM: Pwm Isr Count: 300042 
        PWM_APP_EPWM: App Run time: 30005809 micro secs 
        
        PWM_APP_EPWM: Disabling Notifications for PWM channel 
        PWM_APP_EPWM: Changing Frequency from 10kHz to 4.25MHz and Duty Cycle to 40.5%
        PWM_APP_EPWM: period is set to 29
        PWM_APP_EPWM: This app again waits for 30 seconds please probe
        PWM_APP_EPWM: Pwm Stack Usage 2844 bytes
        PWM_APP_EPWM: All tests have passed!!!

AM62DX - PwmApp_Epwm

        PWM_APP_EPWM: Sample Application - STARTS !!!
        PWM_APP_EPWM: EPWM being used with Channel # 0!!!

        PWM_APP_EPWM: PWM MCAL Version Info
        ---------------------
        PWM_APP_EPWM: Vendor ID           : 44
        PWM_APP_EPWM: Module ID           : 121
        PWM_APP_EPWM: SW Major Version    : 10
        PWM_APP_EPWM: SW Minor Version    : 0
        PWM_APP_EPWM: SW Patch Version    : 0

        PWM_APP_EPWM: Variant - Pre Compile being used !!!

        PWM_APP_EPWM: PWM Channel Initialized
        PWM_APP_EPWM: PWM Duty cycle: 60 Percent, 2000Hz
        PWM_APP_EPWM: PWM CHANNEL 0 configuration Register Readback values
        PWM_APP_EPWM: EPWM_TBCTL                : 0x8032
        PWM_APP_EPWM: EPWM_TBPHS                : 0x0
        PWM_APP_EPWM: EPWM_TBCNT                : 0x3014
        PWM_APP_EPWM: EPWM_AQCTLA               : 0xf2
        PWM_APP_EPWM: EPWM_AQCTLB               : 0xf02
        PWM_APP_EPWM: EPWM_DBCTL                : 0x0
        PWM_APP_EPWM: EPWM_TZSEL                : 0x0
        PWM_APP_EPWM: EPWM_TZCTL                : 0x0
        PWM_APP_EPWM: EPWM_PCCTL                : 0x0
        PWM_APP_EPWM: EPWM_TBSTS                : 0x1
        PWM_APP_EPWM: EPWM_TBPRD                : 0xf424
        PWM_APP_EPWM: EPWM_AQSFRC               : 0xd2
        PWM_APP_EPWM: EPWM_AQSCFRC              : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: This example waits for 30 seconds please probe

        PWM_APP_EPWM: Changing the Duty cycle from to 60 to 80 percent
        PWM_APP_EPWM: This example waits for 30 seconds Please probe

        PWM_APP_EPWM: Changing the Duty cycle to 100 Percent
        PWM_APP_EPWM: This example waits for 10 seconds Please probe

        PWM_APP_EPWM: Setting Output to Idle state
        PWM_APP_EPWM: This example waits for 10 seconds Please probe

        PWM_APP_EPWM: Changing Frequency from 1kHz to 10KHz and Duty Cycle to 50%
        PWM_APP_EPWM: period is set to 12500
        PWM_APP_EPWM: This example validating through ISR count
        PWM_APP_EPWM: Pwm Isr Count: 300000
        PWM_APP_EPWM: App Run time: 30001774 micro secs

        PWM_APP_EPWM: Disabling Notifications for PWM channel
        PWM_APP_EPWM: Changing Frequency from 10kHz to 4.25MHz and Duty Cycle to 40.5%
        PWM_APP_EPWM: period is set to 29
        PWM_APP_EPWM: This app again waits for 30 seconds please probe
        PWM_APP_EPWM: Pwm Stack Usage 2844 bytes
        PWM_APP_EPWM: All tests have passed!!!

AM275X - PwmApp_Epwm

        MCU Initialized!
        Module clock frequency set. Module = 86 , Freq = 250000000 !!!

        PWM_APP_EPWM: Sample Application - STARTS !!!
        PWM_APP_EPWM: EPWM being used with Channel # 0!!!
        
        PWM_APP_EPWM: PWM MCAL Version Info
        ---------------------
        PWM_APP_EPWM: Vendor ID           : 44
        PWM_APP_EPWM: Module ID           : 121
        PWM_APP_EPWM: SW Major Version    : 10
        PWM_APP_EPWM: SW Minor Version    : 0
        PWM_APP_EPWM: SW Patch Version    : 0
        
        PWM_APP_EPWM: Variant - Pre Compile being used !!!
        
        PWM_APP_EPWM: PWM Channel Initialized 
        PWM_APP_EPWM: PWM Duty cycle: 60 Percent, 2000Hz 
        PWM_APP_EPWM: PWM CHANNEL 0 configuration Register Readback values  
        PWM_APP_EPWM: EPWM_TBCTL                : 0x8032
        PWM_APP_EPWM: EPWM_TBPHS                : 0x0
        PWM_APP_EPWM: EPWM_TBCNT                : 0xf0ef
        PWM_APP_EPWM: EPWM_AQCTLA               : 0xf2
        PWM_APP_EPWM: EPWM_AQCTLB               : 0xf02
        PWM_APP_EPWM: EPWM_DBCTL                : 0x0
        PWM_APP_EPWM: EPWM_TZSEL                : 0x0
        PWM_APP_EPWM: EPWM_TZCTL                : 0x0
        PWM_APP_EPWM: EPWM_PCCTL                : 0x0
        PWM_APP_EPWM: EPWM_TBSTS                : 0x0
        PWM_APP_EPWM: EPWM_TBPRD                : 0xf424
        PWM_APP_EPWM: EPWM_AQSFRC               : 0xd2
        PWM_APP_EPWM: EPWM_AQSCFRC              : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: EPWM_Aqsfrc               : 0x0
        PWM_APP_EPWM: This example waits for 30 seconds please probe
        
        PWM_APP_EPWM: Changing the Duty cycle from to 60 to 80 percent 
        PWM_APP_EPWM: This example waits for 30 seconds Please probe
        
        PWM_APP_EPWM: Changing the Duty cycle to 100 Percent 
        PWM_APP_EPWM: This example waits for 10 seconds Please probe
        
        PWM_APP_EPWM: Setting Output to Idle state 
        PWM_APP_EPWM: This example waits for 10 seconds Please probe
        
        PWM_APP_EPWM: Changing Frequency from 1kHz to 10KHz and Duty Cycle to 50%
        PWM_APP_EPWM: period is set to 12500
        
        PWM_APP_EPWM: Changing Frequency from 10kHz to 4.25MHz and Duty Cycle to 40.5%
        PWM_APP_EPWM: period is set to 29
        PWM_APP_EPWM: This app again waits for 30 seconds please probe
        PWM_APP_EPWM: Pwm Stack Usage 2868 bytes
        PWM_APP_EPWM: All tests have passed!!!

Back To Top


References

Back To Top