![]() |
MCUSW
|
This files defines SPI MCAL configuration structures
Data Structures | |
| struct | Spi_ChannelConfigType |
| SPI Channel configuration structure. More... | |
| struct | Spi_McspiExternalDeviceConfigType |
| SPI Job configuration structure specific to McSPI peripheral. More... | |
| struct | Spi_ExternalDeviceConfigType |
| SPI external device specific configuration structure . More... | |
| struct | Spi_JobConfigType |
| SPI Job configuration structure. More... | |
| struct | Spi_SeqConfigType |
| SPI Sequence configuration structure. More... | |
| struct | Spi_HwUnitConfigType |
| SPI Hardware unit configuration structure. More... | |
| struct | Spi_ConfigType |
| SPI config structure. More... | |
| struct | Spi_ChannelConfigType_PC |
| SPI channel config structure parameters Pre-Compile only. More... | |
| struct | Spi_JobConfigType_PC |
| SPI job config structure parameters Pre-Compile only. More... | |
| struct | Spi_SeqConfigType_PC |
| SPI sequence config structure parameters Pre-Compile only. More... | |
| struct | Spi_RegisterReadbackType |
| SPI register readback structure. More... | |
Macros | |
| #define | SPI_VARIANT_POST_BUILD (STD_ON) |
| SPI Build Variant. Build variants.(i.e Pre Compile,Post Build or Link time) | |
SPI Config Ids | |
The Config Ids used for different SPI Configuration builds | |
| enum | Spi_StatusType { SPI_UNINIT = 0U , SPI_IDLE = 1U , SPI_BUSY = 2U } |
| This type defines a range of specific status for SPI Handler/Driver. More... | |
| enum | Spi_JobResultType { SPI_JOB_OK = 0U , SPI_JOB_PENDING = 1U , SPI_JOB_FAILED = 2U , SPI_JOB_QUEUED = 3U } |
| This type defines a range of specific Jobs status for SPI Handler/Driver. More... | |
| enum | Spi_SeqResultType { SPI_SEQ_OK = 0U , SPI_SEQ_PENDING = 1U , SPI_SEQ_FAILED = 2U , SPI_SEQ_CANCELLED = 3U } |
| This type defines a range of specific Sequences status for SPI Handler/Driver. More... | |
| enum | Spi_HwUnitResultType { SPI_HW_UNIT_OK = 0U , SPI_HW_UNIT_PENDING = 1U , SPI_HW_UNIT_FAILED = 2U } |
| This type defines a range of specific HW unit status for SPI Handler/Driver. More... | |
| enum | Spi_AsyncModeType { SPI_POLLING_MODE = 0U , SPI_INTERRUPT_MODE = 1U } |
| Specifies the asynchronous mechanism mode for SPI busses handled asynchronously in LEVEL 2. More... | |
| enum | Spi_TransferType { SPI_MSB = 0U , SPI_LSB = 1U } |
| Word transfer order - MSB first or LSB first. More... | |
| enum | Spi_LevelType { SPI_LOW = STD_LOW , SPI_HIGH } |
| Type for SPI Chip Select Polarity and Clock Idle Level. More... | |
| enum | Spi_CsPinType { SPI_CS0 = 0U , SPI_CS1 , SPI_CS2 , SPI_CS3 } |
| SPI Chip Select Pin. More... | |
| enum | Spi_ClkMode { SPI_CLK_MODE_0 = 0x00U , SPI_CLK_MODE_1 = 0x01U , SPI_CLK_MODE_2 = 0x02U , SPI_CLK_MODE_3 = 0x03U } |
| SPI Clock Mode - sets the clock polarity and phase. Note: These values are a direct register mapping. So don't change value. More... | |
| enum | Spi_TxRxMode { SPI_TX_RX_MODE_BOTH = 0x00U , SPI_TX_RX_MODE_TX_ONLY = 0x02U } |
| SPI TX/RX Mode. More... | |
| enum | Spi_JobPriorityType { SPI_JOB_PRIORITY_0 = 0U , SPI_JOB_PRIORITY_1 , SPI_JOB_PRIORITY_2 , SPI_JOB_PRIORITY_3 } |
| SPI Job Priority. More... | |
| enum | Spi_CsModeType { SPI_SINGLE = 0U , SPI_CONTINUOUS = 1U } |
| SPI Chip Select Mode. More... | |
| enum | Spi_DataDelayType { SPI_DATADELAY_0 = 0U , SPI_DATADELAY_1 = 1U , SPI_DATADELAY_2 = 2U , SPI_DATADELAY_3 = 3U } |
| Spi_DataDelayType defines the number of interface clock cycles between CS toggling and first or last edge of MCSPI clock. More... | |
| enum | Spi_DataLineReceiveType { DATA_LINE_0_RECEPTION = 0U , DATA_LINE_1_RECEPTION = 1U } |
| Spi_DataLineReceiveType defines the lines selected for reception. More... | |
| enum | Spi_DataLineTransmitType { DATA_LINE_NO_TRANSMISSION = 0x3U , DATA_LINE_0_TRANSMISSION = 0x2U , DATA_LINE_1_TRANSMISSION = 0x1U , DATA_LINE_BOTH_TRANSMISSION = 0x0U } |
| Spi_DataLineTransmitType defines the lines selected for transmission. More... | |
| enum | Mcspi_IrqStatusType { SPI_NO_EVENT = 0U , SPI_EVENT_PENDING = 1U , SPI_STATUS_READ_FAIL = 2U } |
| Irq status and std return type. More... | |
| typedef void(* | Spi_CacheWbInv) (uint8 *BufPtr, uint16 LenByte) |
| Cache write-back invalidate function. | |
| typedef void(* | Spi_CacheWb) (uint8 *BufPtr, uint16 LenByte) |
| Cache write-back function. | |
| typedef void(* | Spi_CacheInv) (uint8 *BufPtr, uint16 LenByte) |
| Cache invalidate function. | |
| void | Spi_Init (const Spi_ConfigType *CfgPtr) |
| Service for SPI initialization. | |
| Std_ReturnType | Spi_DeInit (void) |
| Service for SPI de-initialization. | |
| Spi_StatusType | Spi_GetStatus (void) |
| Service returns the SPI Handler/Driver software module status. | |
| Spi_JobResultType | Spi_GetJobResult (Spi_JobType Job) |
| This service returns the last transmission result of the specified Job. | |
| Spi_SeqResultType | Spi_GetSequenceResult (Spi_SequenceType Sequence) |
| This service returns the last transmission result of the specified Sequence. | |
| void | Spi_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| This service returns the version information of this module. | |
| Spi_StatusType | Spi_GetHWUnitStatus (Spi_HWUnitType HWUnit) |
| This service returns the status of the specified SPI Hardware microcontroller peripheral. | |
| Std_ReturnType | Spi_WriteIB (Spi_ChannelType Channel, const Spi_DataBufferType *DataBufferPtr) |
| Service for writing one or more data to an IB SPI Handler/Driver Channel specified by parameter. | |
| Std_ReturnType | Spi_ReadIB (Spi_ChannelType Channel, Spi_DataBufferType *DataBufferPointer) |
| Service for reading synchronously one or more data from an IB SPI Handler/Driver Channel specified by parameter. | |
| Std_ReturnType | Spi_SetupEB (Spi_ChannelType Channel, const Spi_DataBufferType *SrcDataBufferPtr, Spi_DataBufferType *DesDataBufferPtr, Spi_NumberOfDataType Length) |
| Service to setup the buffers and the length of data for the EB SPI Handler/Driver Channel specified. | |
| Std_ReturnType | Spi_AsyncTransmit (Spi_SequenceType Sequence) |
| Service to transmit data on the SPI bus. | |
| void | Spi_Cancel (Spi_SequenceType Sequence) |
| Service cancels the specified on-going sequence transmission. | |
| Std_ReturnType | Spi_SyncTransmit (Spi_SequenceType Sequence) |
| Service to transmit data on the SPI bus. | |
| Std_ReturnType | Spi_SetAsyncMode (Spi_AsyncModeType Mode) |
| Service to set the asynchronous mechanism mode for SPI busses handled asynchronously. | |
| void | Spi_MainFunction_Handling (void) |
| This function polls the SPI interrupts linked to HW Units allocated to the transmission of SPI sequences to enable the evolution of transmission state machine. | |
| Std_ReturnType | Spi_GetDmaHandle (struct Udma_DrvObj *udmaObjPtr) |
| Service for getting DMA handle in SPI. | |
| Std_ReturnType | Spi_RegisterReadback (Spi_HWUnitType HWUnit, Spi_RegisterReadbackType *RegRbPtr) |
| This function reads the important registers of the hardware unit and returns the value in the structure. | |
| Std_ReturnType | Spi_dataOverflowUnderflowIntrEnable (Spi_HWUnitType HWUnit, uint32 intFlags) |
| This function Enable Under/Overflow Interupts of the hardware unit and returns the status. | |
| Std_ReturnType | Spi_dataOverflowUnderflowIntrDisable (Spi_HWUnitType HWUnit, uint32 intFlags) |
| This function Disable Under/Overflow Interupts of the hardware unit and returns the status. | |
| Mcspi_IrqStatusType | Spi_dataOverflowUnderflowIntrGetStatus (Spi_HWUnitType HWUnit, uint32 intFlags) |
| This function status Under/Overflow Interupts of the hardware unit and returns the status. | |
| Std_ReturnType | Spi_dataOverflowUnderflowIntrStatusClear (Spi_HWUnitType HWUnit, uint32 intFlags) |
| This function status clear Under/Overflow Interupts of the hardware unit and returns the status. | |
SPI HW unit Info | |
| enum | Spi_HwUnitType { CSIB0 = 0U , CSIB1 , CSIB2 , CSIB3 , CSIB4 , CSIB5 , CSIB6 , CSIB7 , CSIB8 , CSIB9 , CSIB10 } |
| This type defines a range of HW SPI Hardware microcontroller peripheral allocated to this Job. More... | |
| const uint32 | Spi_HwUnitBaseAddr [SPI_HW_UNIT_CNT] |
| const struct Spi_ConfigType_s | SpiDriver |
| SPI Configuration struct declaration. | |
| void | SpiApp_wbInvCache (uint8 *buf, uint16 len) |
| Cache write-back invalidate function. | |
| void | SpiApp_wbCache (uint8 *buf, uint16 len) |
| Cache write-back function. | |
| void | SpiApp_invCache (uint8 *buf, uint16 len) |
| Cache invalidate function. | |
| void | Spi_IrqUnitMcuMcspi0TxRx (void) |
| SPI Hwunit ISR. | |
| void | Spi_IrqUnitMcuMcspi1TxRx (void) |
| SPI MCU_MCSPI1 ISR. | |
| void | Spi_IrqUnitMcuMcspi2TxRx (void) |
| SPI MCU_MCSPI2 ISR. | |
| void | Spi_IrqUnitMcspi0TxRx (void) |
| SPI MCSPI0 ISR. | |
| void | Spi_IrqUnitMcspi1TxRx (void) |
| SPI MCSPI1 ISR. | |
| void | Spi_IrqUnitMcspi2TxRx (void) |
| SPI MCSPI2 ISR. | |
| void | Spi_IrqUnitMcspi3TxRx (void) |
| SPI MCSPI3 ISR. | |
| void | Spi_IrqUnitMcspi4TxRx (void) |
| SPI MCSPI4 ISR. | |
| #define | SPI_UNIT_MCU_MCSPI0 ((Spi_HWUnitType) CSIB0) |
| MCU MCSPI0 instance. | |
| #define | SPI_UNIT_MCU_MCSPI1 ((Spi_HWUnitType) CSIB1) |
| MCU MCSPI1 instance. | |
| #define | SPI_UNIT_MCU_MCSPI2 ((Spi_HWUnitType) CSIB2) |
| MCU MCSPI2 instance. | |
| #define | SPI_UNIT_MCSPI0 ((Spi_HWUnitType) CSIB3) |
| MCSPI0 instance. | |
| #define | SPI_UNIT_MCSPI1 ((Spi_HWUnitType) CSIB4) |
| MCSPI1 instance. | |
| #define | SPI_UNIT_MCSPI2 ((Spi_HWUnitType) CSIB5) |
| MCSPI2 instance. | |
| #define | SPI_UNIT_MCSPI3 ((Spi_HWUnitType) CSIB6) |
| MCSPI3 instance. | |
| #define | SPI_UNIT_MCSPI4 ((Spi_HWUnitType) CSIB7) |
| MCSPI4 instance. | |
| #define | SPI_UNIT_MCSPI5 ((Spi_HWUnitType) CSIB8) |
| MCSPI5 instance. | |
| #define | SPI_UNIT_MCSPI6 ((Spi_HWUnitType) CSIB9) |
| MCSPI6 instance. | |
| #define | SPI_UNIT_MCSPI7 ((Spi_HWUnitType) CSIB10) |
| MCSPI7 instance. | |
| #define | SPI_HW_UNIT_CNT (11U) |
| Total HW units - used for array allocation. This should be +1 of the max unit number. | |
SPI Driver ISR category level | |
Definitions for SPI Driver ISR ISR category level. | |
| #define | SPI_ISR_VOID (0x00U) |
| void ISR type | |
| #define | SPI_ISR_CAT1 (0x01U) |
| Category 1 ISR type. | |
| #define | SPI_ISR_CAT2 (0x02U) |
| Category 2 ISR type. | |
| #define | SPI_CHANNELBUFFERS (SPI_IB_EB) |
| Pre Compile config macro name. | |
| #define | SPI_IB_MAX_LENGTH (64U) |
| Internal Buffer length in bytes - applicable only for SPI_IB. | |
| #define | SPI_DEV_ERROR_DETECT (STD_ON) |
| Enable/disable SPI dev detect error. | |
| #define | SPI_JOB_LOG (STD_OFF) |
| Enable/disable SPI job log. | |
| #define | SPI_MAX_JOB_LOG (100U) |
| Maximum job log entries when logging is ON. | |
| #define | SPI_MAX_HW_DMA_UNIT (0U) |
| Enable/disable SPI DMA Support. | |
| #define | SPI_DMA_ENABLE (STD_OFF) |
| Enable/disable SPI DMA Support. | |
| #define | SPI_LEVEL_0 (0U) |
| Basic Synchronous functions. | |
| #define | SPI_LEVEL_1 (1U) |
| Basic Asynchronous functions. | |
| #define | SPI_LEVEL_2 (2U) |
| Synchronous and Asynchronous functions. | |
| #define | SPI_SUPPORT_CONCURRENT_SYNC_TRANSMIT (STD_OFF) |
| Concurrent sync transmit support - by defualt this is off. | |
| #define | SPI_SCALEABILITY (SPI_LEVEL_2) |
| Scalability level. | |
| #define | SPI_VERSION_INFO_API (STD_ON) |
| Enable/disable SPI get version info API. | |
| #define | SPI_HW_STATUS_API (STD_ON) |
| Enable/disable SPI HW Status API. | |
| #define | SPI_CANCEL_API (STD_ON) |
| Enable/disable SPI cancel API. | |
| #define | SPI_MAX_CHANNELS_PER_JOB (1U) |
| Maximum channels allowed per job. | |
| #define | SPI_MAX_JOBS_PER_SEQ (1U) |
| Maximum jobs allowed per sequence. | |
| #define | SPI_MAX_CHANNELS (1U) |
| Maximum channels across all jobs/sequence/hwunit. | |
| #define | SPI_MAX_JOBS (1U) |
| Maximum jobs across all sequence/hwunit. | |
| #define | SPI_MAX_SEQ (1U) |
| Maximum sequence across all hwunit. | |
| #define | SPI_MAX_HW_UNIT (8U) |
| Maximum HW unit - This should match the sum for the below units ISR which are ON. | |
| #define | SPI_MAX_EXT_DEV (11U) |
| Maximum external device cfg. | |
| #define | SPI_UNIT_MCU_MCSPI0_ACTIVE (STD_ON) |
| Enable/disable SPI MCU MCSPI0 unit ISR. | |
| #define | SPI_UNIT_MCU_MCSPI1_ACTIVE (STD_ON) |
| Enable/disable SPI MCU MCSPI1 unit ISR. | |
| #define | SPI_UNIT_MCU_MCSPI2_ACTIVE (STD_ON) |
| Enable/disable SPI MCU MCSPI2 unit ISR. | |
| #define | SPI_UNIT_MCSPI0_ACTIVE (STD_ON) |
| Enable/disable SPI MCSPI0 unit ISR. | |
| #define | SPI_UNIT_MCSPI1_ACTIVE (STD_ON) |
| Enable/disable SPI MCSPI1 unit ISR. | |
| #define | SPI_UNIT_MCSPI2_ACTIVE (STD_ON) |
| Enable/disable SPI MCSPI2 unit ISR. | |
| #define | SPI_UNIT_MCSPI3_ACTIVE (STD_ON) |
| Enable/disable SPI MCSPI3 unit ISR. | |
| #define | SPI_UNIT_MCSPI4_ACTIVE (STD_ON) |
| Enable/disable SPI MCSPI4 unit ISR. | |
| #define | SPI_UNIT_MCSPI5_ACTIVE (STD_OFF) |
| Enable/disable SPI MCSPI5 unit ISR. | |
| #define | SPI_UNIT_MCSPI6_ACTIVE (STD_OFF) |
| Enable/disable SPI MCSPI6 unit ISR. | |
| #define | SPI_UNIT_MCSPI7_ACTIVE (STD_OFF) |
| Enable/disable SPI MCSPI7 unit ISR. | |
| #define | SPI_ISR_TYPE (SPI_ISR_CAT1) |
| ISR type. | |
| #define | SPI_OS_COUNTER_ID ((CounterType)OsCounter_0) |
| OS counter ID - used for timeout in case of error. | |
| #define | SPI_TIMEOUT_DURATION (32000U) |
| SPI timeout - used in McSPI IP reset Each tick is 31.25us (for 32K Counter). Wait for 100ms which comes to below value. | |
| #define | SPI_REGISTER_READBACK_API (STD_ON) |
| Enable/disable SPI register read back API. | |
| #define | SPI_SAFETY_API (STD_ON) |
| Enable/disable SPI safety API. | |
| #define | SpiConf_SpiChannel_SpiChannel_0 (0U) |
| Symbolic Name Channel Id - 0 SpiChannel_0. | |
| #define | SpiConf_SpiExternalDevice_CS0 (SPI_CS0) |
| Symbolic Name Chip Select - 0. | |
| #define | SpiConf_SpiJob_SpiJob_0 (0U) |
| Symbolic Name Job Id - 0 SpiJob_0. | |
| #define | SpiConf_SpiSequence_SpiSequence_0 (0U) |
| Symbolic Name Sequence Id - 0 SpiSequence_0. | |
| #define | SpiConf_SpiExternalDevice_HwUnitId0 (CSIB0) |
| Symbolic Name HW Unit - 0. | |
| #define | SpiConf_SpiExternalDevice_HwUnitId1 (CSIB1) |
| Symbolic Name HW Unit - 0. | |
| #define | SpiConf_SpiExternalDevice_HwUnitId2 (CSIB2) |
| Symbolic Name HW Unit - 0. | |
| #define | SpiConf_SpiExternalDevice_HwUnitId3 (CSIB3) |
| Symbolic Name HW Unit - 0. | |
| #define | SpiConf_SpiExternalDevice_HwUnitId4 (CSIB4) |
| Symbolic Name HW Unit - 0. | |
| #define | SpiConf_SpiExternalDevice_HwUnitId5 (CSIB5) |
| Symbolic Name HW Unit - 0. | |
| #define | SpiConf_SpiExternalDevice_HwUnitId6 (CSIB6) |
| Symbolic Name HW Unit - 0. | |
| #define | SpiConf_SpiExternalDevice_HwUnitId7 (CSIB7) |
| Symbolic Name HW Unit - 0. | |
SPI DEM Error codes to report | |
Pre-compile switches for enabling/disabling DEM events | |
| #define | SPI_E_HARDWARE_ERROR (DemConf_DemEventParameter_SPI_E_HARDWARE_ERROR) |
| Hardware failed. | |
| #define SPI_VARIANT_POST_BUILD (STD_ON) |
SPI Build Variant. Build variants.(i.e Pre Compile,Post Build or Link time)
| #define SPI_ISR_VOID (0x00U) |
void ISR type
| #define SPI_ISR_CAT1 (0x01U) |
Category 1 ISR type.
| #define SPI_ISR_CAT2 (0x02U) |
Category 2 ISR type.
| #define SPI_CHANNELBUFFERS (SPI_IB_EB) |
Pre Compile config macro name.
Buffer mode - Internal or External or Both
| #define SPI_IB_MAX_LENGTH (64U) |
Internal Buffer length in bytes - applicable only for SPI_IB.
| #define SPI_DEV_ERROR_DETECT (STD_ON) |
Enable/disable SPI dev detect error.
| #define SPI_JOB_LOG (STD_OFF) |
Enable/disable SPI job log.
| #define SPI_MAX_JOB_LOG (100U) |
Maximum job log entries when logging is ON.
| #define SPI_MAX_HW_DMA_UNIT (0U) |
Enable/disable SPI DMA Support.
| #define SPI_DMA_ENABLE (STD_OFF) |
Enable/disable SPI DMA Support.
| #define SPI_LEVEL_0 (0U) |
Basic Synchronous functions.
| #define SPI_LEVEL_1 (1U) |
Basic Asynchronous functions.
| #define SPI_LEVEL_2 (2U) |
Synchronous and Asynchronous functions.
| #define SPI_SUPPORT_CONCURRENT_SYNC_TRANSMIT (STD_OFF) |
Concurrent sync transmit support - by defualt this is off.
| #define SPI_SCALEABILITY (SPI_LEVEL_2) |
Scalability level.
| #define SPI_VERSION_INFO_API (STD_ON) |
Enable/disable SPI get version info API.
| #define SPI_HW_STATUS_API (STD_ON) |
Enable/disable SPI HW Status API.
| #define SPI_CANCEL_API (STD_ON) |
Enable/disable SPI cancel API.
| #define SPI_MAX_CHANNELS_PER_JOB (1U) |
Maximum channels allowed per job.
| #define SPI_MAX_JOBS_PER_SEQ (1U) |
Maximum jobs allowed per sequence.
| #define SPI_MAX_CHANNELS (1U) |
Maximum channels across all jobs/sequence/hwunit.
| #define SPI_MAX_JOBS (1U) |
Maximum jobs across all sequence/hwunit.
| #define SPI_MAX_SEQ (1U) |
Maximum sequence across all hwunit.
| #define SPI_MAX_HW_UNIT (8U) |
Maximum HW unit - This should match the sum for the below units ISR which are ON.
| #define SPI_MAX_EXT_DEV (11U) |
Maximum external device cfg.
| #define SPI_UNIT_MCU_MCSPI0_ACTIVE (STD_ON) |
Enable/disable SPI MCU MCSPI0 unit ISR.
| #define SPI_UNIT_MCU_MCSPI1_ACTIVE (STD_ON) |
Enable/disable SPI MCU MCSPI1 unit ISR.
| #define SPI_UNIT_MCU_MCSPI2_ACTIVE (STD_ON) |
Enable/disable SPI MCU MCSPI2 unit ISR.
| #define SPI_UNIT_MCSPI0_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI0 unit ISR.
| #define SPI_UNIT_MCSPI1_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI1 unit ISR.
| #define SPI_UNIT_MCSPI2_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI2 unit ISR.
| #define SPI_UNIT_MCSPI3_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI3 unit ISR.
| #define SPI_UNIT_MCSPI4_ACTIVE (STD_ON) |
Enable/disable SPI MCSPI4 unit ISR.
| #define SPI_UNIT_MCSPI5_ACTIVE (STD_OFF) |
Enable/disable SPI MCSPI5 unit ISR.
| #define SPI_UNIT_MCSPI6_ACTIVE (STD_OFF) |
Enable/disable SPI MCSPI6 unit ISR.
| #define SPI_UNIT_MCSPI7_ACTIVE (STD_OFF) |
Enable/disable SPI MCSPI7 unit ISR.
| #define SPI_ISR_TYPE (SPI_ISR_CAT1) |
ISR type.
| #define SPI_OS_COUNTER_ID ((CounterType)OsCounter_0) |
OS counter ID - used for timeout in case of error.
| #define SPI_TIMEOUT_DURATION (32000U) |
SPI timeout - used in McSPI IP reset Each tick is 31.25us (for 32K Counter). Wait for 100ms which comes to below value.
| #define SPI_REGISTER_READBACK_API (STD_ON) |
Enable/disable SPI register read back API.
| #define SPI_SAFETY_API (STD_ON) |
Enable/disable SPI safety API.
| #define SpiConf_SpiChannel_SpiChannel_0 (0U) |
Symbolic Name Channel Id - 0 SpiChannel_0.
| #define SpiConf_SpiExternalDevice_CS0 (SPI_CS0) |
Symbolic Name Chip Select - 0.
| #define SpiConf_SpiJob_SpiJob_0 (0U) |
Symbolic Name Job Id - 0 SpiJob_0.
| #define SpiConf_SpiSequence_SpiSequence_0 (0U) |
Symbolic Name Sequence Id - 0 SpiSequence_0.
| #define SpiConf_SpiExternalDevice_HwUnitId0 (CSIB0) |
Symbolic Name HW Unit - 0.
| #define SpiConf_SpiExternalDevice_HwUnitId1 (CSIB1) |
Symbolic Name HW Unit - 0.
| #define SpiConf_SpiExternalDevice_HwUnitId2 (CSIB2) |
Symbolic Name HW Unit - 0.
| #define SpiConf_SpiExternalDevice_HwUnitId3 (CSIB3) |
Symbolic Name HW Unit - 0.
| #define SpiConf_SpiExternalDevice_HwUnitId4 (CSIB4) |
Symbolic Name HW Unit - 0.
| #define SpiConf_SpiExternalDevice_HwUnitId5 (CSIB5) |
Symbolic Name HW Unit - 0.
| #define SpiConf_SpiExternalDevice_HwUnitId6 (CSIB6) |
Symbolic Name HW Unit - 0.
| #define SpiConf_SpiExternalDevice_HwUnitId7 (CSIB7) |
Symbolic Name HW Unit - 0.
| #define SPI_E_HARDWARE_ERROR (DemConf_DemEventParameter_SPI_E_HARDWARE_ERROR) |
Hardware failed.
| #define SPI_UNIT_MCU_MCSPI0 ((Spi_HWUnitType) CSIB0) |
MCU MCSPI0 instance.
| #define SPI_UNIT_MCU_MCSPI1 ((Spi_HWUnitType) CSIB1) |
MCU MCSPI1 instance.
| #define SPI_UNIT_MCU_MCSPI2 ((Spi_HWUnitType) CSIB2) |
MCU MCSPI2 instance.
| #define SPI_UNIT_MCSPI0 ((Spi_HWUnitType) CSIB3) |
MCSPI0 instance.
| #define SPI_UNIT_MCSPI1 ((Spi_HWUnitType) CSIB4) |
MCSPI1 instance.
| #define SPI_UNIT_MCSPI2 ((Spi_HWUnitType) CSIB5) |
MCSPI2 instance.
| #define SPI_UNIT_MCSPI3 ((Spi_HWUnitType) CSIB6) |
MCSPI3 instance.
| #define SPI_UNIT_MCSPI4 ((Spi_HWUnitType) CSIB7) |
MCSPI4 instance.
| #define SPI_UNIT_MCSPI5 ((Spi_HWUnitType) CSIB8) |
MCSPI5 instance.
| #define SPI_UNIT_MCSPI6 ((Spi_HWUnitType) CSIB9) |
MCSPI6 instance.
| #define SPI_UNIT_MCSPI7 ((Spi_HWUnitType) CSIB10) |
MCSPI7 instance.
| #define SPI_HW_UNIT_CNT (11U) |
Total HW units - used for array allocation. This should be +1 of the max unit number.
| typedef void(* Spi_CacheWbInv) (uint8 *BufPtr, uint16 LenByte) |
Cache write-back invalidate function.
Pointer to a function that performs the cache write-back invalidate operation. This function is to be called on TX buffers before they are given to the Spi controller hardware.
| typedef void(* Spi_CacheWb) (uint8 *BufPtr, uint16 LenByte) |
Cache write-back function.
Pointer to a function that performs the cache write-back operation. This function is to be called on TX buffers before they are given to the Spi controller hardware.
| typedef void(* Spi_CacheInv) (uint8 *BufPtr, uint16 LenByte) |
Cache invalidate function.
Pointer to a function that performs the cache invalidate operation. This function is to be called on RX buffers after they have been retrieved from the Spi controller hardware.
| enum Spi_StatusType |
| enum Spi_JobResultType |
This type defines a range of specific Jobs status for SPI Handler/Driver.
| enum Spi_SeqResultType |
This type defines a range of specific Sequences status for SPI Handler/Driver.
| enum Spi_HwUnitResultType |
| enum Spi_AsyncModeType |
Specifies the asynchronous mechanism mode for SPI busses handled asynchronously in LEVEL 2.
| enum Spi_TransferType |
| enum Spi_LevelType |
| enum Spi_CsPinType |
| enum Spi_ClkMode |
SPI Clock Mode - sets the clock polarity and phase. Note: These values are a direct register mapping. So don't change value.
| enum Spi_TxRxMode |
SPI TX/RX Mode.
Note:
| Enumerator | |
|---|---|
| SPI_TX_RX_MODE_BOTH | Both TX and RX are enabled |
| SPI_TX_RX_MODE_TX_ONLY | Only TX is enabled |
| enum Spi_JobPriorityType |
| enum Spi_CsModeType |
| enum Spi_DataDelayType |
Spi_DataLineTransmitType defines the lines selected for transmission.
| enum Mcspi_IrqStatusType |
| enum Spi_HwUnitType |
This type defines a range of HW SPI Hardware microcontroller peripheral allocated to this Job.
| void Spi_Init | ( | const Spi_ConfigType * | CfgPtr | ) |
Service for SPI initialization.
* Service name : Spi_Init * Syntax : void Spi_Init( const Spi_ConfigType* CfgPtr ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : CfgPtr - Pointer to configuration set * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : Service for SPI initialization *
| Std_ReturnType Spi_DeInit | ( | void | ) |
Service for SPI de-initialization.
* Service name : Spi_DeInit * Syntax : Std_ReturnType Spi_DeInit( void ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: de-initialisation command has been accepted * E_NOT_OK: de-initialisation command has not been * accepted * Description : Service for SPI de-initialization *
| Spi_StatusType Spi_GetStatus | ( | void | ) |
Service returns the SPI Handler/Driver software module status.
* Service name : Spi_GetStatus * Syntax : Spi_StatusType Spi_GetStatus( void ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x06 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : Spi_StatusType - Spi_StatusType * Description : Service for SPI de-initialization *
| Spi_JobResultType Spi_GetJobResult | ( | Spi_JobType | Job | ) |
This service returns the last transmission result of the specified Job.
* Service name : Spi_GetJobResult * Syntax : Spi_JobResultType Spi_GetJobResult( Spi_JobType Job ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Job - Job ID. An invalid job ID will return an * undefined result * Parameters (inout) : None * Parameters (out) : None * Return value : Spi_JobResultType - Spi_JobResultType * Description : Service for SPI de-initialization *
| Spi_SeqResultType Spi_GetSequenceResult | ( | Spi_SequenceType | Sequence | ) |
This service returns the last transmission result of the specified Sequence.
* Service name : Spi_GetSequenceResult * Syntax : Spi_SeqResultType Spi_GetSequenceResult( * Spi_SequenceType Sequence ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x08 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Sequence - Sequence ID. An invalid sequence ID will * return an undefined result * Parameters (inout) : None * Parameters (out) : None * Return value : Spi_SeqResultType - Spi_SeqResultType * Description : This service returns the last transmission result of * the specified Sequence *
| void Spi_GetVersionInfo | ( | Std_VersionInfoType * | versioninfo | ) |
This service returns the version information of this module.
* Service name : Spi_GetVersionInfo * Syntax : void Spi_GetVersionInfo( Std_VersionInfoType* * versioninfo ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x09 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout) : versioninfo - Pointer to where to store the version * information of this module * Parameters (out) : None * Return value : None * Description : This service returns the version information of this * module *
| Spi_StatusType Spi_GetHWUnitStatus | ( | Spi_HWUnitType | HWUnit | ) |
This service returns the status of the specified SPI Hardware microcontroller peripheral.
* Service name : Spi_GetHWUnitStatus * Syntax : Spi_StatusType Spi_GetHWUnitStatus( Spi_HWUnitType * HWUnit ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0b * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : HWUnit - SPI Hardware microcontroller peripheral * unit ID. * Parameters (inout) : None * Parameters (out) : None * Return value : Spi_StatusType - Spi_StatusType * Description : This service returns the status of the specified SPI * Hardware microcontroller peripheral *
| Std_ReturnType Spi_WriteIB | ( | Spi_ChannelType | Channel, |
| const Spi_DataBufferType * | DataBufferPtr ) |
Service for writing one or more data to an IB SPI Handler/Driver Channel specified by parameter.
* Service name : Spi_WriteIB * Syntax : Std_ReturnType Spi_WriteIB( * Spi_ChannelType Channel, * const Spi_DataBufferType* DataBufferPtr ) * * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x02 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Channel - Channel ID * DataBufferPtr - Pointer to source data buffer. * If this pointer is null, it is assumed that the data * to be transmitted is not relevant and the default * transmit value of this channel will be used instead. * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: Write command has been accepted * E_NOT_OK: Write command has not been accepted * Description : Service for writing one or more data to an IB SPI * Handler/Driver Channel specified by parameter *
| Std_ReturnType Spi_ReadIB | ( | Spi_ChannelType | Channel, |
| Spi_DataBufferType * | DataBufferPointer ) |
Service for reading synchronously one or more data from an IB SPI Handler/Driver Channel specified by parameter.
* Service name : Spi_ReadIB * Syntax : Std_ReturnType Spi_ReadIB( * Spi_ChannelType Channel, * Spi_DataBufferType* DataBufferPointer ) * * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Channel - Channel ID * Parameters (inout) : None * Parameters (out) : DataBufferPointer - Pointer to destination data buffer. * Return value : Std_ReturnType * E_OK: Read command has been accepted * E_NOT_OK: Read command has not been accepted * Description : Service for reading synchronously one or more data * from an IB SPI Handler/Driver Channel specified by * parameter *
| Std_ReturnType Spi_SetupEB | ( | Spi_ChannelType | Channel, |
| const Spi_DataBufferType * | SrcDataBufferPtr, | ||
| Spi_DataBufferType * | DesDataBufferPtr, | ||
| Spi_NumberOfDataType | Length ) |
Service to setup the buffers and the length of data for the EB SPI Handler/Driver Channel specified.
* Service name : Spi_SetupEB * Syntax : Std_ReturnType Spi_SetupEB( Spi_ChannelType Channel, * const Spi_DataBufferType* SrcDataBufferPtr, * Spi_DataBufferType* DesDataBufferPtr, * Spi_NumberOfDataType Length ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Channel - Channel ID * SrcDataBufferPtr - Pointer to source data buffer * DesDataBufferPtr - Pointer to destination data buffer * in RAM. * Length - Length (number of data elements) of the data * to be transmitted from SrcDataBufferPtr and/or * received * from DesDataBufferPtr Min.: 1 Max.: Max of data * specified at configuration for this channel * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: Setup command has been accepted * E_NOT_OK: Setup command has not been accepted * Description : Service to setup the buffers and the length of data * for the EB SPI Handler/Driver Channel specified *
| Std_ReturnType Spi_AsyncTransmit | ( | Spi_SequenceType | Sequence | ) |
Service to transmit data on the SPI bus.
* Service name : Spi_AsyncTransmit * Syntax : Std_ReturnType Spi_AsyncTransmit( Spi_SequenceType * Sequence ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x03 * Sync/Async : Asynchronous * Reentrancy : Reentrant * Parameters (in) : Sequence - Sequence ID * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: Transmission command has been accepted * E_NOT_OK: Transmission command has not been accepted * Description : Service to transmit data on the SPI bus *
| void Spi_Cancel | ( | Spi_SequenceType | Sequence | ) |
Service cancels the specified on-going sequence transmission.
* Service name : Spi_Cancel * Syntax : void Spi_Cancel( Spi_SequenceType Sequence ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0c * Sync/Async : Asynchronous * Reentrancy : Reentrant * Parameters (in) : Sequence - Sequence ID * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : Service cancels the specified on-going sequence * transmission *
| Std_ReturnType Spi_SyncTransmit | ( | Spi_SequenceType | Sequence | ) |
Service to transmit data on the SPI bus.
* Service name : Spi_SyncTransmit * Syntax : Std_ReturnType Spi_SyncTransmit( Spi_SequenceType * Sequence) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Sequence - Sequence ID * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: Transmission command has been completed * E_NOT_OK: Transmission command has not been completed * Description : Service to transmit data on the SPI bus *
| Std_ReturnType Spi_SetAsyncMode | ( | Spi_AsyncModeType | Mode | ) |
Service to set the asynchronous mechanism mode for SPI busses handled asynchronously.
* Service name : Spi_SetAsyncMode * Syntax : Std_ReturnType Spi_SetAsyncMode( Spi_AsyncModeType * Mode ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0D * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : Mode - New mode required. * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType * E_OK: Setting command has been done * E_NOT_OK: Setting command has not been accepted * Description : Service to set the asynchronous mechanism mode for * SPI busses handled asynchronously. *
| void Spi_MainFunction_Handling | ( | void | ) |
This function polls the SPI interrupts linked to HW Units allocated to the transmission of SPI sequences to enable the evolution of transmission state machine.
* Service name : Spi_MainFunction_Handling * Syntax : void Spi_MainFunction_Handling( void ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x10 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : This function polls the SPI interrupts linked to * HW Units allocated to the transmission of SPI * sequences to enable the evolution of transmission * state machine. *
| Std_ReturnType Spi_GetDmaHandle | ( | struct Udma_DrvObj * | udmaObjPtr | ) |
Service for getting DMA handle in SPI.
* Service name : Spi_SetDmaHandle * Syntax : Std_ReturnType Spi_SetDmaHandle(Udma_DrvHandle dmaDrvHandle); * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x20 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : dmaDrvHandle - dma driver handle * Parameters (inout) : None * Parameters (out) : None * Return value : Spi_StatusType - Spi_StatusType * Description : Service for getting DMA handle in SPI *
| Std_ReturnType Spi_RegisterReadback | ( | Spi_HWUnitType | HWUnit, |
| Spi_RegisterReadbackType * | RegRbPtr ) |
This function reads the important registers of the hardware unit and returns the value in the structure.
This API should be called after Spi_Init is called. Otherwise this API will return E_NOT_OK.
This API could be used to readback the register contents after Spi_Init and then the readback value could be compared during SPI execution to check the correctness of the HW unit. Since this API is used for this purpose, the register returned are the ones which doesn't change after init based on job or channel config.
* Service name : Spi_RegisterReadback * Mode : Supervisor Mode (Privileged Mode) * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : HWUnit - SPI Hardware microcontroller peripheral * unit ID. If this is invalid, then the API will * return E_NOT_OK. * Parameters (inout) : RegRbPtr - Pointer to where to store the readback * values. If this pointer is NULL_PTR, then the API * will return E_NOT_OK. * Return value : Std_ReturnType * E_OK: Register read back has been done * E_NOT_OK: Register read back failed *
| Std_ReturnType Spi_dataOverflowUnderflowIntrEnable | ( | Spi_HWUnitType | HWUnit, |
| uint32 | intFlags ) |
This function Enable Under/Overflow Interupts of the hardware unit and returns the status.
* Service name : Spi_dataOverflowUnderflowIntrEnable * Mode : Supervisor Mode (Privileged Mode) * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : HWUnit - SPI Hardware microcontroller peripheral * unit ID. If this is invalid, then the API will * return E_NOT_OK. * : intFlags - Mask value of MCSPI_IRQENABLE register * Return value : Std_ReturnType * E_OK: Interupt Enabled * E_NOT_OK: Interupt Enable failed *
| Std_ReturnType Spi_dataOverflowUnderflowIntrDisable | ( | Spi_HWUnitType | HWUnit, |
| uint32 | intFlags ) |
This function Disable Under/Overflow Interupts of the hardware unit and returns the status.
* Service name : Spi_dataOverflowUnderflowIntrDisable * Mode : Supervisor Mode (Privileged Mode) * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : HWUnit - SPI Hardware microcontroller peripheral * unit ID. If this is invalid, then the API will * return E_NOT_OK. * : intFlags - Mask value of MCSPI_IRQSTATUS register * Return value : Std_ReturnType * E_OK: Interupt Disabled * E_NOT_OK: Interupt Disable failed * *
| Mcspi_IrqStatusType Spi_dataOverflowUnderflowIntrGetStatus | ( | Spi_HWUnitType | HWUnit, |
| uint32 | intFlags ) |
This function status Under/Overflow Interupts of the hardware unit and returns the status.
* Service name : Spi_dataOverflowUnderflowIntrGetStatus * Mode : Supervisor Mode (Privileged Mode) * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : HWUnit - SPI Hardware microcontroller peripheral * unit ID. If this is invalid, then the API will * return E_NOT_OK. * intFlags - Mask value of MCSPI_IRQSTATUS register * Return value : Mcspi_IrqStatusType * SPI_NO_EVENT: No underflow event * SPI_EVENT_PENDING: Underflow Event * SPI_STATUS_READ_FAIL: Status read fail *
| Std_ReturnType Spi_dataOverflowUnderflowIntrStatusClear | ( | Spi_HWUnitType | HWUnit, |
| uint32 | intFlags ) |
This function status clear Under/Overflow Interupts of the hardware unit and returns the status.
* Service name : Spi_dataOverflowUnderflowIntrStatusClear * Mode : Supervisor Mode (Privileged Mode) * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : HWUnit - SPI Hardware microcontroller peripheral * unit ID. If this is invalid, then the API will * return E_NOT_OK. * intFlags - Mask value of MCSPI_IRQSTATUS register * Return value : Std_ReturnType * E_OK: Interuptstatus cleares * E_NOT_OK: Interupt status clear failed * *
|
extern |
Cache write-back invalidate function.
|
extern |
Cache write-back function.
|
extern |
Cache invalidate function.
| void Spi_IrqUnitMcuMcspi0TxRx | ( | void | ) |
SPI Hwunit ISR.
SPI MCU_MCSPI0 ISR
| void Spi_IrqUnitMcuMcspi1TxRx | ( | void | ) |
SPI MCU_MCSPI1 ISR.
| void Spi_IrqUnitMcuMcspi2TxRx | ( | void | ) |
SPI MCU_MCSPI2 ISR.
| void Spi_IrqUnitMcspi0TxRx | ( | void | ) |
SPI MCSPI0 ISR.
| void Spi_IrqUnitMcspi1TxRx | ( | void | ) |
SPI MCSPI1 ISR.
| void Spi_IrqUnitMcspi2TxRx | ( | void | ) |
SPI MCSPI2 ISR.
| void Spi_IrqUnitMcspi3TxRx | ( | void | ) |
SPI MCSPI3 ISR.
| void Spi_IrqUnitMcspi4TxRx | ( | void | ) |
SPI MCSPI4 ISR.
| uint8 Spi_ChannelConfigType::channelBufType |
Buffer Type IB/EB
| uint8 Spi_ChannelConfigType::dataWidth |
Width of clock frame in bits. In case of McSPI, valid values are from 1 to 32 bits.
| uint32 Spi_ChannelConfigType::defaultTxData |
Default transmit value when TX buffer is NULL
| Spi_NumberOfDataType Spi_ChannelConfigType::maxBufLength |
Max data length for external or internal buffer in SPI words. In case of internal buffers, this represents the number of words to copy from application buffer to internal buffer in case of Spi_WriteIB() API or from internal buffer to application buffer in case of Spi_ReadIB(). The value of this should be less than or equal to the SPI configuration SPI_IB_MAX_LENGTH as this macro is is used for buffer allocation.
| Spi_TransferType Spi_ChannelConfigType::transferType |
Start with MSB or LSB. Only MSB is supported.
| uint16 Spi_McspiExternalDeviceConfigType::csEnable |
Chip select functionality on/off
| Spi_CsModeType Spi_McspiExternalDeviceConfigType::csMode |
Select single or continuous mode Note: Applicable only for McSPI;
| Spi_LevelType Spi_McspiExternalDeviceConfigType::csPolarity |
Chip select pin polarity high or low
| Spi_DataDelayType Spi_McspiExternalDeviceConfigType::csIdleTime |
CS idle time (Timing between clock and chip select) if single mode is chosen. Values in case of McSPI McSPI 0x00 - 0.5 clock cycles 0x01 - 1.5 clock cycles 0x02 - 2.5 clock cycles 0x03 - 3.5 clock cycles
| uint32 Spi_McspiExternalDeviceConfigType::clkDivider |
Clock divider. This is used to derive the required baudrate from the McSPI functional clock. This value should be 1 less than the actual divider value. So a value of 0 means the divider is 1.
Maximum allowed value of divider is 4095(12 bit register field)
| Spi_ClkMode Spi_McspiExternalDeviceConfigType::clkMode |
Mode 0 = {0=CPOL,0=CPHA}; Mode 1={0,1}; Mode 2={1,0} Mode 3={1,1}
| Spi_TxRxMode Spi_McspiExternalDeviceConfigType::txRxMode |
TX and RX mode
| uint16 Spi_McspiExternalDeviceConfigType::startBitEnable |
Start bit D/CX added before SPI transfer. Polarity is defined by start bit level (below).
| Spi_LevelType Spi_McspiExternalDeviceConfigType::startBitLevel |
Start-bit polarity used when startBitEnable is TRUE.
| Spi_DataLineReceiveType Spi_McspiExternalDeviceConfigType::receptionLineEnable |
Defines the data lines selected for reception.
| Spi_DataLineTransmitType Spi_McspiExternalDeviceConfigType::transmissionLineEnable |
Defines the data lines selected for transmission.
| Spi_McspiExternalDeviceConfigType Spi_ExternalDeviceConfigType::mcspi |
MCSPI HW specific external device config. Should be populated only if hwUnitId is MCSPI
| Spi_JobPriorityType Spi_JobConfigType::jobPriority |
Job priority
| Spi_HWUnitType Spi_JobConfigType::hwUnitId |
HWUnit associated with this job
| Spi_JobEndNotifyType Spi_JobConfigType::Spi_JobEndNotification |
Job end notification callback fxn pointer
| uint32 Spi_JobConfigType::channelPerJob |
Number of channels for this job. Should not be more than SPI_MAX_CHANNELS_PER_JOB
| Spi_ChannelType Spi_JobConfigType::channelList[SPI_MAX_CHANNELS_PER_JOB] |
Channel index list
| uint8 Spi_SeqConfigType::seqInterruptible |
Sequence interruptible or not (TRUE/FALSE)
| Spi_SeqEndNotifyType Spi_SeqConfigType::Spi_SequenceEndNotification |
Sequence end notification callback fxn pointer
| uint32 Spi_SeqConfigType::jobPerSeq |
Number of jobs for this sequence. Should not be more than SPI_MAX_JOBS_PER_SEQ
| Spi_JobType Spi_SeqConfigType::jobList[SPI_MAX_JOBS_PER_SEQ] |
Job index list
| Spi_HWUnitType Spi_HwUnitConfigType::hwUnitId |
SPI HW unit to use
| boolean Spi_HwUnitConfigType::enabledmaMode |
Enable SPI DMA Support per instance
| uint32 Spi_HwUnitConfigType::dmaTxChIntrNum |
DMA TX channel interrupt number
| uint32 Spi_HwUnitConfigType::dmaRxChIntrNum |
DMA RX channel interrupt number
| uint8 Spi_ConfigType::maxChannels |
Maximum number of channels. Should not be more than SPI_MAX_CHANNELS
| uint8 Spi_ConfigType::maxJobs |
Maximum number of jobs Should not be more than SPI_MAX_JOBS
| uint8 Spi_ConfigType::maxSeq |
Maximum number of sequences Should not be more than SPI_MAX_SEQ
| uint8 Spi_ConfigType::maxHwUnit |
Maximum number of HW unit Should not be more than SPI_MAX_HW_UNIT
| uint8 Spi_ConfigType::maxExtDevCfg |
Maximum number of external device configurations Should not be more than SPI_MAX_EXT_DEV
| uint32 Spi_ConfigType::udmaInstId |
UDMA Instance Id. Based on core in which the SpiDriver is running Udma Instance should be chosen
| Spi_CacheWbInv Spi_ConfigType::cacheWbInv |
Cache write-back invalidate function
| Spi_CacheWb Spi_ConfigType::cacheWb |
Cache write-back function
| Spi_CacheInv Spi_ConfigType::cacheInv |
Cache invalidate function
| Spi_ChannelConfigType Spi_ConfigType::channelCfg[SPI_MAX_CHANNELS] |
Channel configurations
| Spi_JobConfigType Spi_ConfigType::jobCfg[SPI_MAX_JOBS] |
Job configurations
| Spi_SeqConfigType Spi_ConfigType::seqCfg[SPI_MAX_SEQ] |
Sequence configurations
| Spi_HwUnitConfigType Spi_ConfigType::hwUnitCfg[SPI_MAX_HW_UNIT] |
HW Unit configurations
| Spi_ExternalDeviceConfigType Spi_ConfigType::extDevCfg[SPI_MAX_EXT_DEV] |
External HW device config
| Spi_ChannelType Spi_ChannelConfigType_PC::channelId |
Channel ID
| Spi_JobType Spi_JobConfigType_PC::jobId |
Job ID
| Spi_CsPinType Spi_JobConfigType_PC::csPin |
Chip select pin to use
| uint8 Spi_JobConfigType_PC::externalDeviceCfgId |
index into SpiConfig.extDevCfg[] indicating the devCfg associated with the job
| Spi_SequenceType Spi_SeqConfigType_PC::seqId |
Sequence ID
| uint32 Spi_RegisterReadbackType::mcspiHlRev |
IP revision identifier
| uint32 Spi_RegisterReadbackType::mcspiHlHwInfo |
Information about the IP module's hardware configuration
| uint32 Spi_RegisterReadbackType::mcspiHlSysConfig |
Clock management configuration
| uint32 Spi_RegisterReadbackType::mcspiRev |
IP revision number
| uint32 Spi_RegisterReadbackType::mcspiSysStatus |
IP status information
| uint32 Spi_RegisterReadbackType::mcspiSyst |
System config
| uint32 Spi_RegisterReadbackType::mcspiModulctrl |
module ctrl register MCSPI_MODULCTRL
| uint32 Spi_RegisterReadbackType::mcspiSysConfig |
sysconfig register MCSPI_SYSCONFIG
| uint32 Spi_RegisterReadbackType::mcspiCh0config |
| uint32 Spi_RegisterReadbackType::mcspiCh1config |
| uint32 Spi_RegisterReadbackType::mcspiCh2config |
| uint32 Spi_RegisterReadbackType::mcspiCh3config |
module Channel config Register MCSPI_CHCONF_0/1/2/3
| uint32 Spi_RegisterReadbackType::mcspiIrqenable |
Irqenable MCSPI_IRQENABLE
|
extern |
|
extern |
SPI Configuration struct declaration.