![]() |
MCUSW
|
This files defines ICU MCAL configuration structures
This files defines ICU MCAL configuration structures
Data Structures | |
| struct | Icu_DutyCycleType |
| This type defines Duty Cycle struct. More... | |
| struct | Icu_ChannelConfigType_PC |
| ICU Channel Config Structure of Pre-Compile only. More... | |
| struct | Icu_ConfigType_PC |
| ICU Config Structure of Pre-Compile only. More... | |
| struct | Icu_ChannelConfigType |
| ICU Channel Config Structure. More... | |
| struct | Icu_ConfigType |
| ICU Config Structure. More... | |
| struct | Icu_RegisterReadbackType |
| Icu register readback structure. More... | |
Macros | |
| #define | ICU_PRE_COMPILE_VARIANT (STD_ON ) |
| ICU Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time) | |
| #define | ICU_VARIANT_POST_BUILD (STD_OFF) |
| #define | ICU_PRE_COMPILE_VARIANT (STD_ON ) |
| ICU Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time) | |
| #define | ICU_VARIANT_POST_BUILD (STD_OFF) |
Macros to define Rising and Falling edge config for capture registers | |
| enum | Icu_ModeType { ICU_MODE_NORMAL , ICU_MODE_SLEEP } |
| This type defines a range of mode type. More... | |
| enum | Icu_InputStateType { ICU_ACTIVE , ICU_IDLE } |
| This type defines a input state of ICU driver. More... | |
| enum | Icu_ActivationType { ICU_RISING_EDGE , ICU_FALLING_EDGE , ICU_BOTH_EDGES } |
| This type defines Activation range. More... | |
| enum | Icu_MeasurementModeType { ICU_MODE_SIGNAL_EDGE_DETECT , ICU_MODE_SIGNAL_MEASUREMENT , ICU_MODE_TIMESTAMP , ICU_MODE_EDGE_COUNTER } |
| This type defines available measurement modes. More... | |
| enum | Icu_SignalMeasurementPropertyType { ICU_LOW_TIME , ICU_HIGH_TIME , ICU_PERIOD_TIME , ICU_DUTY_CYCLE } |
| This type defines Signal Measurement Property range. More... | |
| enum | Icu_TimestampBufferType { ICU_LINEAR_BUFFER , ICU_CIRCULAR_BUFFER } |
| This type defines TimeStamp Property range. More... | |
| typedef uint32 | Icu_ValueType |
| This type defines Value type. | |
| typedef uint32 | Icu_IndexType |
| This type defines return value Icu_GetTimeStampIndex. | |
| typedef uint32 | Icu_EdgeNumberType |
| This type defines return value of Icu-Icu_GetEdgeNumbers. | |
| typedef void(* | Icu_NotifyFuncType) (void) |
| Notification callback function pointer | |
| typedef uint8 | Icu_ChannelType |
| This type defines Channel type. | |
| typedef uint32 | Icu_ChannelPrescalerType |
| This type defines Prescaler type. | |
| void | Icu_Init (const Icu_ConfigType *ConfigPtr) |
| Service for ICU initialization. | |
| void | Icu_DeInit (void) |
| Service for ICU de-initialization. | |
| void | Icu_SetActivationCondition (Icu_ChannelType Channel, Icu_ActivationType Activation) |
| Service for setting Activation Condition. | |
| void | Icu_DisableNotification (Icu_ChannelType Channel) |
| Service for disabling notification. | |
| void | Icu_EnableNotification (Icu_ChannelType Channel) |
| Service for enabling notification. | |
| Icu_InputStateType | Icu_GetInputState (Icu_ChannelType Channel) |
| Service for getting the ICU input status. | |
| void | Icu_StartTimestamp (Icu_ChannelType Channel, Icu_ValueType *BufferPtr, uint16 BufferSize, uint16 NotifyInterval) |
| Service for starts the captuing of timer values on the edges. | |
| void | Icu_StopTimestamp (Icu_ChannelType Channel) |
| Service for stopping the timestamp measurement. | |
| Icu_IndexType | Icu_GetTimestampIndex (Icu_ChannelType Channel) |
| Service for reading the timestamp index of a givem channel. | |
| void | Icu_ResetEdgeCount (Icu_ChannelType Channel) |
| Service for resets the value of the counted edges to zero. | |
| void | Icu_EnableEdgeCount (Icu_ChannelType Channel) |
| Service enabling the counting of edges of a given channel. | |
| void | Icu_DisableEdgeCount (Icu_ChannelType Channel) |
| Service for disabling the couting of edges of the given channel. | |
| Icu_EdgeNumberType | Icu_GetEdgeNumbers (Icu_ChannelType Channel) |
| Service for reading the number of counted edges. | |
| void | Icu_EnableEdgeDetection (Icu_ChannelType Channel) |
| Service for enabling/re-enabling the detection of edges of the given channel. | |
| void | Icu_DisableEdgeDetection (Icu_ChannelType Channel) |
| Service for disabling the detection of edges of the given channel. | |
| void | Icu_StartSignalMeasurement (Icu_ChannelType Channel) |
| Service for starting the measurement of signals. | |
| void | Icu_StopSignalMeasurement (Icu_ChannelType Channel) |
| Service for stopping the measurement of signals. | |
| Icu_ValueType | Icu_GetTimeElapsed (Icu_ChannelType Channel) |
| Service for reading the elasped time for the given channel. | |
| void | Icu_GetDutyCycleValues (Icu_ChannelType Channel, Icu_DutyCycleType *DutyCycleValues) |
| Service for reading the coherent active time and period time of given channel. | |
| void | Icu_CheckWakeup (EcuM_WakeupSourceType WakeupSource) |
| This function checks if a wakeup capable ICU channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid ICU channel wakeup event. | |
| void | Icu_DisableWakeup (Icu_ChannelType Channel) |
| This function disables the wakeup capability of a single ICU channel. | |
| void | Icu_EnableWakeup (Icu_ChannelType Channel) |
| This function (re-)enables the wakeup capability of the given ICU channel. | |
| void | Icu_SetMode (Icu_ModeType Mode) |
| This function sets the ICU mode. | |
| Std_ReturnType | Icu_RegisterReadback (Icu_ChannelType IcuChannel, Icu_RegisterReadbackType *RegRbPtr) |
| Icu_IndexType | Icu_GetTimeStampIndex (Icu_ChannelType Channel) |
ICU Driver ISR category level | |
Definitions for ICU Driver ISR ISR category level. | |
| const uint32 | Icu_HwUnitBaseAddr [ICU_MAX_NUM_CHANNELS] |
| const struct Icu_ConfigType_PC_s | IcuConfigSet_PC |
| ICU Configuration structure declaration. | |
| const struct Icu_ConfigType_s | IcuConfigSet |
| void | Icu_ch1Notify (void) |
| ICU ISR. | |
| #define | IcuConf_IcuChannel_IcuChannel_0 (1U) |
| Channel ID Symbolic Names Configured channel ID(s) | |
| #define | ICU_CHANNEL1 (1U) |
| ECAP Channel 1, in MAIN DOMAIN. | |
ICU Driver ISR category level | |
Definitions for ICU Driver ISR ISR category level. | |
| const uint32 | Icu_HwUnitBaseAddr [ICU_MAX_NUM_CHANNELS] |
| const struct Icu_ConfigType_PC_s | IcuConfigSet_PC |
| ICU Configuration structure declaration. | |
| const struct Icu_ConfigType_s | IcuConfigSet |
| void | Icu_ch2Notify (void) |
| ICU ISR. | |
| #define | ICU_ISR_VOID (0x00U) |
| void ISR type | |
| #define | ICU_ISR_CAT1 (0x01U) |
| Category 1 ISR type. | |
| #define | ICU_ISR_CAT2 (0x02U) |
| Category 2 ISR type. | |
| #define | ICU_SAFETY_DIAGNOSTIC_API (STD_ON) |
| Enable/Disable Icu Safety Diagnostic. | |
| #define | ICU_DE_INIT_API (STD_ON) |
| Enable/Disable Icu DeInit API. | |
| #define | ICU_EDGE_COUNT_API (STD_ON) |
| Enable/Disable Edge Count API. | |
| #define | ICU_EDGE_DETECT_API (STD_ON) |
| Enable/Disable Edge Detect API. | |
| #define | ICU_GET_DUTY_CYCLE_VALUES_API (STD_ON) |
| Enable/Disable Get Duty Cycle Values API. | |
| #define | ICU_GET_INPUT_STATE_API (STD_ON) |
| Enable/Disable Get Input State API. | |
| #define | ICU_GET_TIME_ELAPSED_API (STD_ON) |
| Enable/Disable Get Time Elapsed API. | |
| #define | ICU_GET_VERSION_INFO_API (STD_ON) |
| Enable/Disable Get Version Info API. | |
| #define | ICU_SIGNAL_MEASUREMENT_API (STD_ON) |
| Enable/Disable Signal Measurement API. | |
| #define | ICU_TIMESTAMP_API (STD_ON) |
| Enable/Disable Timestamp API. | |
| #define | ICU_DEV_ERROR_DETECT (STD_ON) |
| Enable/Disable Development error detet. | |
| #define | ICU_WAKEUP_FUNCTIONALITY_API (STD_OFF) |
| Enable/disable ICU wakeup functionality API. | |
| #define | ICU_ENABLEWAKEUP_API (STD_OFF) |
| Enable/disable ICU wakeup functionality API. | |
| #define | ICU_DISABLEWAKEUP_API (STD_OFF) |
| Enable/disable ICU wakeup functionality API. | |
| #define | ICU_SETMODE_API (STD_OFF) |
| Enable/Disable Icu set mode API. | |
| #define | ICU_INIT_CONFIG_PC IcuConfigSet |
| Pre Compile config macro name. | |
| #define | ICU_ISR_TYPE (ICU_ISR_CAT1) |
| ISR type. | |
| #define | ICU_MAX_NUM_CHANNELS (3U) |
| #define | ICU_ISR_VOID (0x00U) |
| void ISR type | |
| #define | ICU_ISR_CAT1 (0x01U) |
| Category 1 ISR type. | |
| #define | ICU_ISR_CAT2 (0x02U) |
| Category 2 ISR type. | |
| #define | ICU_SAFETY_DIAGNOSTIC_API (STD_OFF) |
| Enable/Disable Icu Safety Diagnostic. | |
| #define | ICU_DE_INIT_API (STD_ON) |
| Enable/Disable Icu DeInit API. | |
| #define | ICU_EDGE_COUNT_API (STD_ON) |
| Enable/Disable Edge Count API. | |
| #define | ICU_EDGE_DETECT_API (STD_ON) |
| Enable/Disable Edge Detect API. | |
| #define | ICU_GET_DUTY_CYCLE_VALUES_API (STD_ON) |
| Enable/Disable Get Duty Cycle Values API. | |
| #define | ICU_GET_INPUT_STATE_API (STD_ON) |
| Enable/Disable Get Input State API. | |
| #define | ICU_GET_TIME_ELAPSED_API (STD_ON) |
| Enable/Disable Get Time Elapsed API. | |
| #define | ICU_GET_VERSION_INFO_API (STD_ON) |
| Enable/Disable Get Version Info API. | |
| #define | ICU_SIGNAL_MEASUREMENT_API (STD_ON) |
| Enable/Disable Signal Measurement API. | |
| #define | ICU_TIMESTAMP_API (STD_ON) |
| Enable/Disable Timestamp API. | |
| #define | ICU_DEV_ERROR_DETECT (STD_ON) |
| Enable/Disable Development error detet. | |
| #define | ICU_WAKEUP_FUNCTIONALITY_API (STD_OFF) |
| Enable/disable ICU wakeup functionality API. | |
| #define | ICU_ENABLEWAKEUP_API (STD_OFF) |
| Enable/disable ICU wakeup functionality API. | |
| #define | ICU_DISABLEWAKEUP_API (STD_OFF) |
| Enable/disable ICU wakeup functionality API. | |
| #define | ICU_SETMODE_API (STD_OFF) |
| Enable/Disable Icu set mode API. | |
| #define | IcuConf_IcuChannel_IcuChannel_2 (2U) |
| Channel ID Symbolic Names Configured channel ID(s) | |
| #define | ICU_INIT_CONFIG_PC IcuConfigSet |
| Pre Compile config macro name. | |
| #define | ICU_ISR_TYPE (ICU_ISR_CAT1) |
| ISR type. | |
| #define | ICU_MAX_NUM_CHANNELS (3U) |
| #define | ICU_CHANNEL2 (2U) |
| ECAP Channel 2, in MAIN R5 DOMAIN. | |
| #define ICU_PRE_COMPILE_VARIANT (STD_ON ) |
ICU Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time)
| #define ICU_VARIANT_POST_BUILD (STD_OFF) |
| #define ICU_ISR_VOID (0x00U) |
void ISR type
| #define ICU_ISR_CAT1 (0x01U) |
Category 1 ISR type.
| #define ICU_ISR_CAT2 (0x02U) |
Category 2 ISR type.
| #define ICU_SAFETY_DIAGNOSTIC_API (STD_ON) |
Enable/Disable Icu Safety Diagnostic.
| #define ICU_DE_INIT_API (STD_ON) |
Enable/Disable Icu DeInit API.
| #define ICU_EDGE_COUNT_API (STD_ON) |
Enable/Disable Edge Count API.
| #define ICU_EDGE_DETECT_API (STD_ON) |
Enable/Disable Edge Detect API.
| #define ICU_GET_DUTY_CYCLE_VALUES_API (STD_ON) |
Enable/Disable Get Duty Cycle Values API.
| #define ICU_GET_INPUT_STATE_API (STD_ON) |
Enable/Disable Get Input State API.
| #define ICU_GET_TIME_ELAPSED_API (STD_ON) |
Enable/Disable Get Time Elapsed API.
| #define ICU_GET_VERSION_INFO_API (STD_ON) |
Enable/Disable Get Version Info API.
| #define ICU_SIGNAL_MEASUREMENT_API (STD_ON) |
Enable/Disable Signal Measurement API.
| #define ICU_TIMESTAMP_API (STD_ON) |
Enable/Disable Timestamp API.
| #define ICU_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable Development error detet.
| #define ICU_WAKEUP_FUNCTIONALITY_API (STD_OFF) |
Enable/disable ICU wakeup functionality API.
| #define ICU_ENABLEWAKEUP_API (STD_OFF) |
Enable/disable ICU wakeup functionality API.
| #define ICU_DISABLEWAKEUP_API (STD_OFF) |
Enable/disable ICU wakeup functionality API.
| #define ICU_SETMODE_API (STD_OFF) |
Enable/Disable Icu set mode API.
| #define IcuConf_IcuChannel_IcuChannel_0 (1U) |
Channel ID Symbolic Names Configured channel ID(s)
Channel identifiers
| #define ICU_INIT_CONFIG_PC IcuConfigSet |
Pre Compile config macro name.
| #define ICU_ISR_TYPE (ICU_ISR_CAT1) |
ISR type.
| #define ICU_MAX_NUM_CHANNELS (3U) |
| #define ICU_CHANNEL1 (1U) |
ECAP Channel 1, in MAIN DOMAIN.
| #define ICU_PRE_COMPILE_VARIANT (STD_ON ) |
ICU Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time)
| #define ICU_VARIANT_POST_BUILD (STD_OFF) |
| #define ICU_ISR_VOID (0x00U) |
void ISR type
| #define ICU_ISR_CAT1 (0x01U) |
Category 1 ISR type.
| #define ICU_ISR_CAT2 (0x02U) |
Category 2 ISR type.
| #define ICU_SAFETY_DIAGNOSTIC_API (STD_OFF) |
Enable/Disable Icu Safety Diagnostic.
| #define ICU_DE_INIT_API (STD_ON) |
Enable/Disable Icu DeInit API.
| #define ICU_EDGE_COUNT_API (STD_ON) |
Enable/Disable Edge Count API.
| #define ICU_EDGE_DETECT_API (STD_ON) |
Enable/Disable Edge Detect API.
| #define ICU_GET_DUTY_CYCLE_VALUES_API (STD_ON) |
Enable/Disable Get Duty Cycle Values API.
| #define ICU_GET_INPUT_STATE_API (STD_ON) |
Enable/Disable Get Input State API.
| #define ICU_GET_TIME_ELAPSED_API (STD_ON) |
Enable/Disable Get Time Elapsed API.
| #define ICU_GET_VERSION_INFO_API (STD_ON) |
Enable/Disable Get Version Info API.
| #define ICU_SIGNAL_MEASUREMENT_API (STD_ON) |
Enable/Disable Signal Measurement API.
| #define ICU_TIMESTAMP_API (STD_ON) |
Enable/Disable Timestamp API.
| #define ICU_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable Development error detet.
| #define ICU_WAKEUP_FUNCTIONALITY_API (STD_OFF) |
Enable/disable ICU wakeup functionality API.
| #define ICU_ENABLEWAKEUP_API (STD_OFF) |
Enable/disable ICU wakeup functionality API.
| #define ICU_DISABLEWAKEUP_API (STD_OFF) |
Enable/disable ICU wakeup functionality API.
| #define ICU_SETMODE_API (STD_OFF) |
Enable/Disable Icu set mode API.
| #define IcuConf_IcuChannel_IcuChannel_2 (2U) |
Channel ID Symbolic Names Configured channel ID(s)
Channel identifiers
| #define ICU_INIT_CONFIG_PC IcuConfigSet |
Pre Compile config macro name.
| #define ICU_ISR_TYPE (ICU_ISR_CAT1) |
ISR type.
| #define ICU_MAX_NUM_CHANNELS (3U) |
| #define ICU_CHANNEL2 (2U) |
ECAP Channel 2, in MAIN R5 DOMAIN.
| typedef uint32 Icu_ValueType |
This type defines Value type.
| typedef uint32 Icu_IndexType |
This type defines return value Icu_GetTimeStampIndex.
| typedef uint32 Icu_EdgeNumberType |
This type defines return value of Icu-Icu_GetEdgeNumbers.
| typedef void(* Icu_NotifyFuncType) (void) |
Notification callback function pointer
| typedef uint8 Icu_ChannelType |
This type defines Channel type.
| typedef uint32 Icu_ChannelPrescalerType |
This type defines Prescaler type.
| enum Icu_ModeType |
| enum Icu_InputStateType |
| enum Icu_ActivationType |
| void Icu_Init | ( | const Icu_ConfigType * | ConfigPtr | ) |
Service for ICU initialization.
* Service name : Icu_Init * Syntax : Icu_Init(const Icu_ConfigType* ConfigPtr) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : Pointer to the configuration * Parameters (out) : None * Return value : void * Description : Initializes internal variables * and the ECAP unit of the micro controller. * The function can be called on task level. *
| void Icu_DeInit | ( | void | ) |
Service for ICU de-initialization.
* Service name : Icu_DeInit * Syntax : Icu_DeInit(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (out) : None * Return value : void * Description : DeInit ECAP module *
| void Icu_SetActivationCondition | ( | Icu_ChannelType | Channel, |
| Icu_ActivationType | Activation ) |
Service for setting Activation Condition.
* Service name : Icu_SetActivationCondition * Syntax : Icu_SetActivationCondition(Icu_ChannelType Channel, * Icu_ActivationType Activation) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (in) : Icu_ActivationType Activation * Parameters (out) : None * Return value : void * Description : This service sets the Activation edge for channel * Type of activation (if supported by hardware) * ICU_RISING_EDGE, ICU_FALLING_EDGE, ICU_BOTH_EDGES *
| void Icu_DisableNotification | ( | Icu_ChannelType | Channel | ) |
Service for disabling notification.
* Service name : Icu_DisableNotification * Syntax : Icu_DisableNotification(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x06 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the notificaiton of a channel *
| void Icu_EnableNotification | ( | Icu_ChannelType | Channel | ) |
Service for enabling notification.
* Service name : Icu_EnableNotification * Syntax : Icu_EnableNotification(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables the notificaiton of a channel *
| Icu_InputStateType Icu_GetInputState | ( | Icu_ChannelType | Channel | ) |
Service for getting the ICU input status.
* Service name : Icu_GetInputState * Syntax : Icu_GetInputState(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x08 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service returns the status of the ICU input *
| void Icu_StartTimestamp | ( | Icu_ChannelType | Channel, |
| Icu_ValueType * | BufferPtr, | ||
| uint16 | BufferSize, | ||
| uint16 | NotifyInterval ) |
Service for starts the captuing of timer values on the edges.
* Service name : Icu_StartTimestamp * Syntax : Icu_StartTimestamp(Icu_ChannelType Channel, * Icu_ValueType* BufferPtr, * uint16 BufferSize, * uint16 NotifyInterval) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x09 * Sync/Async : Asynchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (in) : uint16 BufferSize * Parameters (in) : uint16 NotifyInterval * Parameters (out) : Icu_ValueType* BufferPtr * Return value : void * Description : This service starts the capturing of timer values on the edges *
| void Icu_StopTimestamp | ( | Icu_ChannelType | Channel | ) |
Service for stopping the timestamp measurement.
* Service name : Icu_StopTimestamp * Syntax : Icu_StopTimestamp(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service stops timestamp measurement of the given channel. *
| Icu_IndexType Icu_GetTimestampIndex | ( | Icu_ChannelType | Channel | ) |
Service for reading the timestamp index of a givem channel.
* Service name : Icu_GetTimestampIndex * Syntax : Icu_GetTimestampIndex(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0B * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads the timestamp index of a given channel. *
| void Icu_ResetEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service for resets the value of the counted edges to zero.
* Service name : Icu_ResetEdgeCount * Syntax : Icu_ResetEdgeCount(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0C * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service resets the value of the counted edges to zero. *
| void Icu_EnableEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service enabling the counting of edges of a given channel.
* Service name : Icu_EnableEdgeCount * Syntax : Icu_EnableEdgeCount(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0D * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables the couting of edges of the given channel. *
| void Icu_DisableEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service for disabling the couting of edges of the given channel.
* Service name : Icu_DisableEdgeCount * Syntax : Icu_DisableEdgeCount(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0E * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the couting of edges of a given channel. *
| Icu_EdgeNumberType Icu_GetEdgeNumbers | ( | Icu_ChannelType | Channel | ) |
Service for reading the number of counted edges.
* Service name : Icu_GetEdgeNumbers * Syntax : Icu_GetEdgeNumbers(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0F * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads the number of counted edges. *
| void Icu_EnableEdgeDetection | ( | Icu_ChannelType | Channel | ) |
Service for enabling/re-enabling the detection of edges of the given channel.
* Service name : Icu_EnableEdgeDetection * Syntax : Icu_EnableEdgeDetection(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x16 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables/re-enables the detection of edges of a channel. *
| void Icu_DisableEdgeDetection | ( | Icu_ChannelType | Channel | ) |
Service for disabling the detection of edges of the given channel.
* Service name : Icu_EnableEdgeDetection * Syntax : Icu_EnableEdgeDetection(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x17 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the detection of edges of a channel. *
| void Icu_StartSignalMeasurement | ( | Icu_ChannelType | Channel | ) |
Service for starting the measurement of signals.
* Service name : Icu_StartSignalMeasurement * Syntax : Icu_StartSignalMeasurement(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x13 * Sync/Async : Asynchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service starts the measurement of signals of a given channel. *
| void Icu_StopSignalMeasurement | ( | Icu_ChannelType | Channel | ) |
Service for stopping the measurement of signals.
* Service name : Icu_StopSignalMeasurement * Syntax : Icu_StopSignalMeasurement(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x14 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service stops the measurement of signals of a given channel. *
| Icu_ValueType Icu_GetTimeElapsed | ( | Icu_ChannelType | Channel | ) |
Service for reading the elasped time for the given channel.
* Service name : Icu_GetTimeElapsed * Syntax : Icu_GetTimeElapsed(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x10 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads elasped time for a given channel. *
| void Icu_GetDutyCycleValues | ( | Icu_ChannelType | Channel, |
| Icu_DutyCycleType * | DutyCycleValues ) |
Service for reading the coherent active time and period time of given channel.
* Service name : Icu_GetTimeElapsed * Syntax : Icu_GetTimeElapsed(Icu_ChannelType Channel, * Icu_DutyCycleType* DutyCycleValues) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x11 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : Icu_DutyCycleType* DutyCycleValues * Return value : void * Description : This service reads active time and period of given channel. *
| void Icu_CheckWakeup | ( | EcuM_WakeupSourceType | WakeupSource | ) |
This function checks if a wakeup capable ICU channel is the source for a wakeup event and calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid ICU channel wakeup event.
* Service name : Icu_CheckWakeup
* Syntax : void Icu_CheckWakeup(EcuM_WakeupSourceType WakeupSource)
* Service ID[hex] : 0x19
* Sync/Async : Synchronous
* Reentrancy : Reentrant(limited according to ICU050)
* Parameters (in) : WakeupSource
* Informatin on wakeup source to be checked.
The associated ICU channel can be determined from configuration data
* Parameters (inout) : None
* Parameters (out) : None
* Return value : None
* Description : Checks if a wakeup capable ICU channel is the source for a wakeup event and
* calls the ECU state manager service EcuM_SetWakeupEvent in case of a valid ICU
* channel wakeup event.
*
| void Icu_DisableWakeup | ( | Icu_ChannelType | Channel | ) |
This function disables the wakeup capability of a single ICU channel.
* Service name : Icu_DisableWakeup * Syntax : void Icu_DisableWakeup(Icu_ChannelType Channel) * Service ID[hex] : 0x20 * Sync/Async : Synchronous * Reentrancy : Reentrant(limited according to ICU050) * Parameters (in) : Channel * Numeric identifier of the ICU channel * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : This function disables the wakeup capability of a single ICU channel. *
| void Icu_EnableWakeup | ( | Icu_ChannelType | Channel | ) |
This function (re-)enables the wakeup capability of the given ICU channel.
* Service name : Icu_EnableWakeup * Syntax : void Icu_EnableWakeup(Icu_ChannelType Channel) * Service ID[hex] : 0x21 * Sync/Async : Synchronous * Reentrancy : Reentrant(limited according to ICU050) * Parameters (in) : Channel * Numeric identifier of the ICU channel * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : This function (re-)enables the wakeup capability of the given ICU channel. *
| void Icu_SetMode | ( | Icu_ModeType | Mode | ) |
This function sets the ICU mode.
* Service name : Icu_SetMode * Syntax : void Icu_SetMode(Icu_ModeType Mode) * Service ID[hex] : 0x22 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : Mode * ICU_MODE_NORMAL: Normal operation, all used interrupts are enabled * according to the notification requests. * ICU_MODE_SLEEP: Reduced power mode. In sleep mode only those * notifications are available which are configured as wakeup capable. * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : This function sets the ICU mode. *
| Std_ReturnType Icu_RegisterReadback | ( | Icu_ChannelType | IcuChannel, |
| Icu_RegisterReadbackType * | RegRbPtr ) |
| Icu_IndexType Icu_GetTimeStampIndex | ( | Icu_ChannelType | Channel | ) |
| void Icu_ch1Notify | ( | void | ) |
ICU ISR.
ICU Channel 1 ISR
| void Icu_ch2Notify | ( | void | ) |
ICU ISR.
ICU Channel 2 ISR
| Icu_ValueType Icu_DutyCycleType::ActiveTime |
Active time of Signal
| Icu_ValueType Icu_DutyCycleType::PeriodTime |
Period time of Signal
| Icu_ChannelType Icu_ChannelConfigType_PC::channelId |
Channel ID of ICU Channel in use
| Icu_ChannelConfigType_PC Icu_ConfigType_PC::chCfg[ICU_MAX_NUM_CHANNELS] |
Channel configurations
| Icu_ActivationType Icu_ChannelConfigType::defaultStartEdge |
Default activation edge to be used by ICU module
| Icu_MeasurementModeType Icu_ChannelConfigType::measurementMode |
Measurement Mode to be used
| Icu_SignalMeasurementPropertyType Icu_ChannelConfigType::signalMeasurementProperty |
Signal Measurmenet property to be used if mode choosen
| Icu_NotifyFuncType Icu_ChannelConfigType::notificationHandler |
Notification handler for notifications
| Icu_TimestampBufferType Icu_ChannelConfigType::bufferType |
Buffer Type for Timestamp API mode
| uint32 Icu_ChannelConfigType::instanceClkMHz |
Clk src for ICU module in MHz
| uint32 Icu_ChannelConfigType::prescaler |
Prescaler value to be used for ICU module
| Icu_ChannelType Icu_ConfigType::icuMaxChannel |
Number of ICU Channel being configured
| Icu_ChannelConfigType Icu_ConfigType::chCfg[ICU_MAX_NUM_CHANNELS] |
Channel configurations
| uint32 Icu_RegisterReadbackType::ECAP_CNTPHS |
| uint32 Icu_RegisterReadbackType::ECAP_ECCTL |
| uint32 Icu_RegisterReadbackType::ECAP_ECINT_EN_FLG |
|
extern |
|
extern |
ICU Configuration structure declaration.
|
extern |
|
extern |
|
extern |
ICU Configuration structure declaration.
|
extern |