![]() |
MCUSW
|
This files defines FLS MCAL configuration structures
Data Structures | |
| struct | Fls_ConfigType |
| FLS Module Configuration Structure. More... | |
Variables | |
| Fls_JobEndNotifyType | Fls_ConfigType::Fls_JobEndNotification |
| Fls_JobErrorNotifyType | Fls_ConfigType::Fls_JobErrorNotification |
| uint32 | Fls_ConfigType::maxReadNormalMode |
| uint32 | Fls_ConfigType::maxWriteNormalMode |
| boolean | Fls_ConfigType::dacEnable |
| boolean | Fls_ConfigType::xipEnable |
| uint64 | Fls_ConfigType::ospiClkSpeed |
| boolean | Fls_ConfigType::dtrEnable |
| boolean | Fls_ConfigType::phyEnable |
| OSPI_xferLines | Fls_ConfigType::ospixferlines |
| uint32 | Fls_ConfigType::flsBaudRateDiv |
| uint32 | Fls_ConfigType::blockSize |
Macros | |
| #define | FLS_PRE_COMPILE_VARIANT (STD_ON) |
| FLS Build Variant. Build variants.(i.e Pre Compile,Post Build or Link time) | |
FLS Service Ids | |
The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error | |
| enum | OSPI_xferLines { OSPI_XFER_LINES_SINGLE = 0U , OSPI_XFER_LINES_DUAL , OSPI_XFER_LINES_QUAD , OSPI_XFER_LINES_OCTAL } |
| Number of lines used for OSPI read/write transaction. More... | |
| void | Fls_SwitchMode (boolean dacEnable, boolean xipEnable) |
| Switch Mode of the OSPI Driver Parameters (in) : boolean dacEnable - should DAC mode be enaled or disabled Parameters (in) : boolean xipEnable - should XIP mode be enaled or disabled Mode : Supervisor Mode (Privileged Mode) | |
| void | Fls_Init (const Fls_ConfigType *ConfigPtr) |
| Initializes the Flash Driver. | |
| Std_ReturnType | Fls_Erase (Fls_AddressType TargetAddress, Fls_LengthType Length) |
| Erases flash sector(s). | |
| Std_ReturnType | Fls_Write (Fls_AddressType TargetAddress, const uint8 *SourceAddressPtr, Fls_LengthType Length) |
| Writes one or more complete flash pages. | |
| Std_ReturnType | Fls_Read (Fls_AddressType SourceAddress, uint8 *TargetAddressPtr, Fls_LengthType Length) |
| Reads from flash memory.. | |
| Std_ReturnType | Fls_Compare (Fls_AddressType SourceAddress, const uint8 *TargetAddressPtr, Fls_LengthType Length) |
| Compares the contents of an area of flash memory with that of an application data buffer. | |
| Std_ReturnType | Fls_BlankCheck (Fls_AddressType Address, Fls_LengthType Length) |
| The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed. | |
| MemIf_StatusType | Fls_GetStatus (void) |
| Returns the driver state. | |
| Std_ReturnType | Fls_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| This service returns the version information of this module. | |
| MemIf_JobResultType | Fls_GetJobResult (void) |
| Returns the result of the last job. | |
| void | Fls_MainFunction (void) |
| Performs the processing of jobs. | |
| void | Fls_Cancel (void) |
| Cancels an ongoing job. | |
FLS Driver ISR category level | |
Defines for FLS Driver ISR ISR category level | |
| const struct Fls_ConfigType_s | FlsConfigSet |
| FLS Configuration struct declaration. | |
| #define | FLS_ISR_VOID (0x00U) |
| void ISR type | |
| #define | FLS_ISR_CAT1 (0x01U) |
| Category 1 ISR type. | |
| #define | FLS_ISR_CAT2 (0x02U) |
| Category 2 ISR type. | |
| #define | FLS_INIT_CONFIG_PC FlsConfigSet |
| Pre Compile config macro name. | |
| #define | FLS_NOR |
| FLS_MEMORY_TYPE. | |
| #define | FLS_OSPI |
| FLS_PROTOCOL_MODE. | |
| #define | FLS_BASE_ADDRESS (1342177280U) |
| Flash Memory start address, defines lower boundary for read/writ/erase/compare jobs. | |
| #define | FLS_BLANK_CHECK_API (STD_ON) |
| Enable/disable FLS Blank Check API. | |
| #define | FLS_COMPARE_API (STD_ON) |
| Enable/disable FLS compare API. | |
| #define | FLS_CANCEL_API (STD_ON) |
| Enable/disable FLS cancel API. | |
| #define | FLS_TIMEOUT_SUPERVISION_ENABLED (STD_ON) |
| Enable/disable FlsTimeoutSupervisionEnabled. | |
| #define | FLS_DEV_ERROR_DETECT (STD_ON) |
| Enable/disable FLS dev detect error. | |
| #define | FLS_DRIVER_INDEX (0U) |
| Index of driver, used by FEE. | |
| #define | FLS_GET_JOB_RESULT_API (STD_ON) |
| Enable/disable FLS Fls_GetJobResult function API. | |
| #define | FLS_GET_STATUS_API (STD_ON) |
| Enable/disable FLS Fls_GetStatus function API. | |
| #define | FLS_TOTAL_SIZE (1073741824U) |
| Total amount of flash memory in bytes. | |
| #define | FLS_USE_INTERRUPTS (STD_OFF) |
| Job processing triggered by hardware interrupt. | |
| #define | FLS_ISR_TYPE (FLS_ISR_CAT1) |
| ISR type. | |
| #define | FLS_VERSION_INFO_API (STD_ON) |
| Enable/disable FLS get version info API. | |
| #define | FLS_OS_COUNTER_ID ((CounterType)OsCounter_0) |
| Counter ID for counter used to count wait ticks. | |
| #define | FLS_TIMEOUT_DURATION (50000) |
| Counter ID for counter used to count wait ticks. | |
| #define | FLS_OSPI_CTRL_BASE_ADDR (1191444480UL) |
| Base Address of OSPI. | |
| #define | OSPI_REGISTER_READBACK_API (STD_ON) |
| Enable/disable OSPI register read back API. | |
| #define | OSPI_SAFETY_API (STD_ON) |
| Enable/disable OSPI safety API. | |
| #define | FLS_MAX_ERASE_TIME (1000.0) |
| Max Erase time in millisec. | |
| #define | FLS_MAX_WRITE_TIME (1000.0) |
| Max Write time in millisec. | |
| #define FLS_PRE_COMPILE_VARIANT (STD_ON) |
FLS Build Variant. Build variants.(i.e Pre Compile,Post Build or Link time)
| #define FLS_ISR_VOID (0x00U) |
void ISR type
| #define FLS_ISR_CAT1 (0x01U) |
Category 1 ISR type.
| #define FLS_ISR_CAT2 (0x02U) |
Category 2 ISR type.
| #define FLS_INIT_CONFIG_PC FlsConfigSet |
Pre Compile config macro name.
| #define FLS_NOR |
FLS_MEMORY_TYPE.
| #define FLS_OSPI |
FLS_PROTOCOL_MODE.
| #define FLS_BASE_ADDRESS (1342177280U) |
Flash Memory start address, defines lower boundary for read/writ/erase/compare jobs.
| #define FLS_BLANK_CHECK_API (STD_ON) |
Enable/disable FLS Blank Check API.
| #define FLS_COMPARE_API (STD_ON) |
Enable/disable FLS compare API.
| #define FLS_CANCEL_API (STD_ON) |
Enable/disable FLS cancel API.
| #define FLS_TIMEOUT_SUPERVISION_ENABLED (STD_ON) |
Enable/disable FlsTimeoutSupervisionEnabled.
| #define FLS_DEV_ERROR_DETECT (STD_ON) |
Enable/disable FLS dev detect error.
| #define FLS_DRIVER_INDEX (0U) |
Index of driver, used by FEE.
| #define FLS_GET_JOB_RESULT_API (STD_ON) |
Enable/disable FLS Fls_GetJobResult function API.
| #define FLS_GET_STATUS_API (STD_ON) |
Enable/disable FLS Fls_GetStatus function API.
| #define FLS_TOTAL_SIZE (1073741824U) |
Total amount of flash memory in bytes.
| #define FLS_USE_INTERRUPTS (STD_OFF) |
Job processing triggered by hardware interrupt.
| #define FLS_ISR_TYPE (FLS_ISR_CAT1) |
ISR type.
| #define FLS_VERSION_INFO_API (STD_ON) |
Enable/disable FLS get version info API.
| #define FLS_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks.
| #define FLS_TIMEOUT_DURATION (50000) |
Counter ID for counter used to count wait ticks.
| #define FLS_OSPI_CTRL_BASE_ADDR (1191444480UL) |
Base Address of OSPI.
| #define OSPI_REGISTER_READBACK_API (STD_ON) |
Enable/disable OSPI register read back API.
| #define OSPI_SAFETY_API (STD_ON) |
Enable/disable OSPI safety API.
| #define FLS_MAX_ERASE_TIME (1000.0) |
Max Erase time in millisec.
| #define FLS_MAX_WRITE_TIME (1000.0) |
Max Write time in millisec.
| enum OSPI_xferLines |
| void Fls_SwitchMode | ( | boolean | dacEnable, |
| boolean | xipEnable ) |
Switch Mode of the OSPI Driver Parameters (in) : boolean dacEnable - should DAC mode be enaled or disabled Parameters (in) : boolean xipEnable - should XIP mode be enaled or disabled Mode : Supervisor Mode (Privileged Mode)
| void Fls_Init | ( | const Fls_ConfigType * | ConfigPtr | ) |
Initializes the Flash Driver.
* Service name : Fls_Init * Syntax : void Fls_Init( const Fls_ConfigType* ConfigPtr ) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : ConfigPtr - Pointer to flash driver configuration set * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : Initializes the Flash Driver *
| Std_ReturnType Fls_Erase | ( | Fls_AddressType | TargetAddress, |
| Fls_LengthType | Length ) |
Erases flash sector(s).
* Service name : Fls_Erase * Syntax : Std_ReturnType Fls_Erase(Fls_AddressType TargetAddress * ,Fls_LengthType Length) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : TargetAddress - Target address in flash memory. * This address offset will be added to the flash memory * base address. * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: erase command has been accepted * E_NOT_OK: erase command has not been accepted * Description : Erases flash sector(s). *
| Std_ReturnType Fls_Write | ( | Fls_AddressType | TargetAddress, |
| const uint8 * | SourceAddressPtr, | ||
| Fls_LengthType | Length ) |
Writes one or more complete flash pages.
* Service name : Fls_Write * Syntax : Std_ReturnType Fls_Write(Fls_AddressType TargetAddress * ,const uint8* SourceAddressPtr, * Fls_LengthType Length) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x02 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : TargetAddress - Target address in flash memory. * This address offset will be added to the flash memory * base address. * SourceAddressPtr - Pointer to source data buffer * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: write command has been accepted * E_NOT_OK: write command has not been accepted * Description : Writes one or more complete flash pages. *
| Std_ReturnType Fls_Read | ( | Fls_AddressType | SourceAddress, |
| uint8 * | TargetAddressPtr, | ||
| Fls_LengthType | Length ) |
Reads from flash memory..
* Service name : Fls_Read * Syntax : Std_ReturnType Fls_Read((Fls_AddressType SourceAddress * ,const uint8* TargetAddressPtr, * Fls_LengthType Length) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : SourceAddress - source address in flash memory. * This address offset will be added to the flash memory * base address. * TargetAddressPtr - Pointer to source data buffer * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: read command has been accepted * E_NOT_OK: read command has not been accepted * Description : Reads from flash memory. *
| Std_ReturnType Fls_Compare | ( | Fls_AddressType | SourceAddress, |
| const uint8 * | TargetAddressPtr, | ||
| Fls_LengthType | Length ) |
Compares the contents of an area of flash memory with that of an application data buffer.
* Service name : Fls_Compare * Syntax : Std_ReturnType Fls_Compare * (Fls_AddressType SourceAddress, * const uint8* TargetAddressPtr, * Fls_LengthType Length) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x08 * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : SourceAddress - Target address in flash memory. * This address offset will be added to the flash memory * base address. * TargetAddressPtr - Pointer to source data buffer * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: compare command has been accepted * E_NOT_OK: compare command has not been accepted * Description : Compares the contents of an area of flash memory * with that of an application data buffer. *
| Std_ReturnType Fls_BlankCheck | ( | Fls_AddressType | Address, |
| Fls_LengthType | Length ) |
The function Fls_BlankCheck shall verify, whether a given memory area has been erased but not (yet) programmed.
* Service name : Fls_BlankCheck * Syntax : Std_ReturnType Fls_Compare * (Fls_AddressType TargetAddress,, * Fls_LengthType Length) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0a * Sync/Async : Asynchronous * Reentrancy : Non Reentrant * Parameters (in) : TargetAddress - Target address in flash memory. * This address offset will be added to the flash memory * base address. * SourceAddressPtr - Pointer to source data buffer * Length - Number of bytes to erase * Parameters (inout) : None * Parameters (out) : None * Return value : Std_ReturnType - * E_OK: BlankCheck command has been accepted * E_NOT_OK: BlankCheck command has not been accepted * Description : The function Fls_BlankCheck shall verify, * whether a given memory area has been * erased but not (yet) programmed. *
| MemIf_StatusType Fls_GetStatus | ( | void | ) |
Returns the driver state.
* Service name : Fls_GetStatus * Syntax : MemIf_StatusType Fls_GetStatus( void ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : MemIf_StatusType * Description : Returns the driver state. *
| Std_ReturnType Fls_GetVersionInfo | ( | Std_VersionInfoType * | versioninfo | ) |
This service returns the version information of this module.
* Service name : Fls_GetVersionInfo * Syntax : void Fls_GetVersionInfo( Std_VersionInfoType* * versioninfo ) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x10 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout) : versioninfo - Pointer to where to store the version * information of this module * Parameters (out) : None * Return value : None * Description : This service returns the version information of this * module *
| MemIf_JobResultType Fls_GetJobResult | ( | void | ) |
Returns the result of the last job.
* Service name : Fls_GetJobResult * Syntax : MemIf_JobResultType Fls_GetJobResult(void) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : MemIf_JobResultType * Description : Returns the result of the last job. *
| void Fls_MainFunction | ( | void | ) |
Performs the processing of jobs.
* Service name : Fls_MainFunction * Syntax : void Fls_MainFunction(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x06 * Description : Performs the processing of jobs. *
| void Fls_Cancel | ( | void | ) |
Cancels an ongoing job.
* Service name : Fls_Cancel * Syntax : void Fls_Cancel(void) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x03 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (inout) : None * Parameters (out) : None * Return value : None * Description : Cancels an ongoing job. *
| Fls_JobEndNotifyType Fls_ConfigType::Fls_JobEndNotification |
Mapped to the job end notification routine provided by some upper layer module, typically the Fee module.
| Fls_JobErrorNotifyType Fls_ConfigType::Fls_JobErrorNotification |
Mapped to the job error notification routine provided by some upper layer module, typically the Fee module.
| uint32 Fls_ConfigType::maxReadNormalMode |
The maximum number of bytes to read or compare in one cycle of the flash driver's job processing function in normal mode.
| uint32 Fls_ConfigType::maxWriteNormalMode |
The maximum number of bytes to write in one cycle of the flash driver's job processing function in normal mode.
| boolean Fls_ConfigType::dacEnable |
Enable Direct Access Mode of Transfer in OSPI Flash
| boolean Fls_ConfigType::xipEnable |
Enable XIP mode in OSPI Flash
| uint64 Fls_ConfigType::ospiClkSpeed |
OSPI Clock Speed
| boolean Fls_ConfigType::dtrEnable |
Enable Double transfer rate protocol for OSPI.
| boolean Fls_ConfigType::phyEnable |
Enable PHY high-speed mode for DAC mode
| OSPI_xferLines Fls_ConfigType::ospixferlines |
Select the OSPI read/write transaction Lines
| uint32 Fls_ConfigType::flsBaudRateDiv |
To select the FLS baudrate Divider value
| uint32 Fls_ConfigType::blockSize |
To select OSPI block size based on variants
|
extern |
FLS Configuration struct declaration.