110#if (STD_ON == SPI_DMA_ENABLE)
This file contains interface header for SPI MCAL driver.
uint8 Spi_HWUnitType
Specifies the identification (ID) for a SPI Hardware micro controller peripheral (unit)
Definition Spi.h:242
void Spi_IntISR_McuMcspiDmaTx(Spi_HWUnitType MaxHwUnit, Spi_HWUnitType Spi_HwUnit)
void Spi_IntISR_McuMcspiTxRx(Spi_HWUnitType Spi_HwUnit)
ADC ISR.
void Spi_IntISR_McuMcspiDmaRx(Spi_HWUnitType MaxHwUnit, Spi_HWUnitType Spi_HwUnit)