112 #define WDG_VARIANT_PRE_COMPILE (STD_ON) 117 #define WDG_INIT_CONFIG_PC WdgSettingsConfig 122 #define WDG_DEV_ERROR_DETECT (STD_ON) 125 #define WDG_GET_VERSION_INFO_API (STD_ON) 128 #define WDG_REGISTER_READBACK_API (STD_ON) 132 #define WDG_MAX_TIMEOUT ((uint16)65535) 136 #define WDG_RTI_FREQUENCY ((uint32)12500000) 139 #define WDG_DISABLE_ALLOWED (STD_OFF) 148 #define WdgConf_WdgGeneral_WdgIndex_0 (0U) 159 #define DemConf_DemEventParameter_WDG_DEM_NO_EVENT (0xFFFFU) 160 #define WDG_DEM_NO_EVENT DemConf_DemEventParameter_WDG_DEM_NO_EVENT 162 #ifndef WDG_E_MODE_FAILED 164 #define WDG_E_MODE_FAILED DemConf_DemEventParameter_WDG_E_MODE_FAILED 167 #ifndef WDG_E_DISABLE_REJECTED 169 #define WDG_E_DISABLE_REJECTED DemConf_DemEventParameter_WDG_E_DISABLE_REJECTED 172 #define WDG_NUM_INSTANCE (12U) 187 extern CONST(uint32, WDG_CONST)
const struct Wdg_ConfigType_s WdgSettingsConfig
WDG Configuration struct declaration.
const struct Wdg_ConfigType_PC_s WdgSettingsConfig_PC
WDG Configuration pre compile struct declaration.
#define WDG_NUM_INSTANCE
Definition: Wdg_Cfg.h:172
const uint32 RTIHwUnit_BaseAddr[WDG_NUM_INSTANCE]
Base Address of the watchdog instances.