104 #define GPT_ISR_VOID (0x00U) 106 #define GPT_ISR_CAT1 (0x01U) 108 #define GPT_ISR_CAT2 (0x02U) void(* Gpt_IsrRefType)(uint32 fnParameter)
Typedef for the ISR Function Array.
Definition: Gpt_Irq.h:112
uint32 Gpt_ChannelType
Type describing the Gpt channel.
Definition: Gpt.h:311
void Gpt_IntISR_Fun(Gpt_ChannelType gptChannel)
GPT Channel ISR.
This file contains interface header for GPT MCAL driver.