114 #define GPT_CH_GPTIMER1 (0U) 116 #define GPT_CH_GPTIMER2 (1U) 118 #define GPT_CH_GPTIMER3 (2U) 120 #define GPT_CH_GPTIMER4 (3U) 122 #define GPT_CH_GPTIMER5 (4U) 124 #define GPT_CH_GPTIMER6 (5U) 126 #define GPT_CH_GPTIMER7 (6U) 128 #define GPT_CH_GPTIMER8 (7U) 130 #define GPT_CH_GPTIMER9 (8U) 132 #define GPT_CH_GPTIMER10 (9U) 134 #define GPT_CH_GPTIMER11 (10U) 136 #define GPT_CH_GPTIMER12 (11U) 138 #define GPT_CH_GPTIMER13 (12U) 140 #define GPT_CH_GPTIMER14 (13U) 142 #define GPT_CH_GPTIMER15 (14U) 144 #define GPT_CH_GPTIMER16 (15U) 146 #define GPT_CH_GPTIMER17 (16U) 148 #define GPT_CH_GPTIMER18 (17U) 150 #define GPT_CH_GPTIMER19 (18U) 152 #define GPT_CH_GPTIMER20 (19U) 154 #define GPT_CH_GPTIMER21 (20U) 156 #define GPT_CH_GPTIMER22 (21U) 158 #define GPT_CH_GPTIMER23 (22U) 160 #define GPT_CH_GPTIMER24 (23U) 162 #define GPT_CH_GPTIMER25 (24U) 164 #define GPT_CH_GPTIMER26 (25U) 166 #define GPT_CH_GPTIMER27 (26U) 168 #define GPT_CH_GPTIMER28 (27U) 170 #define GPT_CH_GPTIMER29 (28U) 172 #define GPT_CH_GPTIMER30 (29U) 175 #define GPT_CH_GPTIMER_MAX (30U) 184 #define GPT_PRE_COMPILE_VARIANT (STD_OFF) 190 #define GPT_DEV_ERROR_DETECT (STD_ON) 192 #define GPT_ISR_TYPE (GPT_ISR_CAT1) 195 #define GPT_REPORT_WAKEUP_SOURCE (STD_ON) 201 #define GPT_VERSION_INFO_API (STD_ON) 206 #define GPT_DEINIT_API (STD_ON) 211 #define GPT_TIME_ELAPSED_API (STD_ON) 216 #define GPT_TIME_REMAINING_API (STD_ON) 221 #define GPT_ENABLE_DISABLE_NOTIFICATION_API (STD_ON) 226 #define GPT_WAKEUP_FUNCTIONALITY_API (STD_ON) 233 #define GPT_MAX_CHANNELS (5U) 239 #define GPT_PREDEF_TIMER_TYPE (GPT_PREDEF_TIMER_DISABLED) 243 #define GPT_PREDEF_TIMER_1US_ENABLING_GRADE (GPT_PREDEF_TIMER_1US_DISABLED) 247 #define GPT_OS_COUNTER_ID ((CounterType)OsCounter_0) 254 #define GPT_TIMEOUT_DURATION (32000U) 262 #define DemConf_DemEventParameter_GPT_DEM_NO_EVENT (0xFFFFU) 263 #define GPT_DEM_NO_EVENT DemConf_DemEventParameter_GPT_DEM_NO_EVENT 265 #ifndef GPT_E_HARDWARE_ERROR 267 #define GPT_E_HARDWARE_ERROR (DemConf_DemEventParameter_GPT_E_HARDWARE_ERROR) 273 #define GPT_REGISTER_READBACK_API (STD_ON) 279 #define GptConf_GptChannelConfiguration_TIMER1 (11U) 281 #define GptConf_GptChannelConfiguration_MCU_TIMER6 (6U) 283 #define GptConf_GptChannelConfiguration_MCU_TIMER9 (9U) 285 #define GptConf_GptChannelConfiguration_TIMER5 (15U) 287 #define GptConf_GptChannelConfiguration_TIMER19 (29U) const uint32 Gpt_TimerBaseAddr[GPT_CH_GPTIMER_MAX]
Base Address of the timer peripherals.
#define GPT_CH_GPTIMER_MAX
maximum GP timer channels available
Definition: Gpt_Cfg.h:175
void Gpt_Ch12Isr(void)
GPT Channel ISR.
const struct Gpt_ConfigType_s GptChannelConfigSet
GPT Configuration.