103 #define SPI_ISR_VOID (0x00U) 105 #define SPI_ISR_CAT1 (0x01U) 107 #define SPI_ISR_CAT2 (0x02U) 122 #if (STD_ON == SPI_DMA_ENABLE) 129 #endif//#if (STD_ON == SPI_DMA_ENABLE) void Spi_IntISR_McuMcspiDmaRx(Spi_HWUnitType MaxHwUnit, Spi_HWUnitType Spi_HwUnit)
uint8 Spi_HWUnitType
Specifies the identification (ID) for a SPI Hardware micro controller peripheral (unit) ...
Definition: Spi.h:242
void Spi_IntISR_McuMcspiTxRx(Spi_HWUnitType Spi_HwUnit)
ADC ISR.
This file contains interface header for SPI MCAL driver.
void Spi_IntISR_McuMcspiDmaTx(Spi_HWUnitType MaxHwUnit, Spi_HWUnitType Spi_HwUnit)