MCUSW
Loading...
Searching...
No Matches
Sitara MPU Build and Installation User Guide

Installation Steps


AM62X/AM62AX/AM62PX/AM62DX

No additional steps required. However, the MCAL configurator would require an additional step. Please refer (Getting access to MCAL) to receive installer for configurator and steps to obtain licese is detailed in (License for Configurator)

Directory structure post installation

AM62DX

Please note that this is an indicative image, actual soc and versions would change

Back To Top


Directory Structure

Post installation of MCUSW, the following directory would be created. Please note that this is an indicative snap-shot. Modules/Drivers could be added/modified.

Top Level Directory Structure

MCAL

MCAL Directory structure, contains MCAL modules, build files. Please note that this is an indicative snap-shot. Modules/Drivers could be added/modified.

Back To Top


MCAL Modules

MCAL Examples

Contains demo applications that demonstrate use of MCAL modules. An integrator could refer these to determine the dependencies of the module.

MCAL Examples

MCAL Examples Configuration

Contains configurations (standalone i.e. configuration for given module and its dependencies, such as Gpt (not dependent on other modules)

MCAL Example Configurations

Back To Top


Build


MCAL employs make based build mechanism. When building on Windows based machine, tool such as gmake could be used.

Setup Build Environment


Following changes are required to be performed in Rules.make to build

  1. Rules.make can be found at ($SDK_INSTALL_PATH)/mcusw/build, When building on Windows environment ensure to update variables under ifeq (Windows_NT,Windows_NT)
  2. Build MCAL Examples
    • Set BUILD_OS_TYPE = baremetal to build MCAL examples/libraries
  3. Specify the location of the compiler
    • In Rules.make, update SDK_INSTALL_PATH to specify location of the SDK installation.
    • One can override compiler path by updating variable TOOLCHAIN_PATH_R5
  4. Modify Rules.make file as per Soc
    • AM62X : By default AM62X_MCU_SDK_VERSION is set to am62x_xx_xx_xx_xx. To use with specific SDK, update AM62X_MCU_SDK_VERSION in Rules.make file. Update ENABLE_UART_BOOTMODE=no to build in No Boot Mode. By default it is yes and will build in UART boot mode.
    • AM62AX: By default AM62AX_MCU_SDK_VERSION is set to am62ax_xx_xx_xx_xx. To use with specific SDK, update AM62AX_MCU_SDK_VERSION in Rules.make file.
    • AM62PX: By default AM62PX_MCU_SDK_VERSION is set to am62px_xx_xx_xx_xx. To use with specific SDK, update AM62PX_MCU_SDK_VERSION in Rules.make file.
    • AM62DX: By default AM62DX_MCU_SDK_VERSION is set to am62dx_xx_xx_xx_xx. To use with specific SDK, update AM62DX_MCU_SDK_VERSION in Rules.make file.

Note: Please refer release note for compatible Mcu_plus_Sdk version.

Build Everything MCAL


With steps listed at (Setup Build Environment) all MCAL modules can be built

AM62X

  • Ensure BUILD_OS_TYPE = baremetal
  • Go to folder ($SDK_INSTALL_PATH)/mcusw/build
  • gmake -s all BOARD=am62x_evm SOC=am62x BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal
  • On Successful compilation, binary folder would be created in ($SDK_INSTALL_PATH)/mcusw/binary/(driver name)_app/bin/am62x_evm/

AM62AX

  • Ensure BUILD_OS_TYPE = baremetal
  • Go to folder ($SDK_INSTALL_PATH)/mcusw/build
  • gmake -s all BOARD=am62ax_evm SOC=am62ax BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal
  • On Successful compilation, binary folder would be created in ($SDK_INSTALL_PATH)/mcusw/binary/(driver name)_app/bin/am62ax_evm/

AM62DX

  • Ensure BUILD_OS_TYPE = baremetal
  • Go to folder ($SDK_INSTALL_PATH)/mcusw/build
  • gmake -s all BOARD=am62dx_evm SOC=am62dx BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal
  • On Successful compilation, binary folder would be created in ($SDK_INSTALL_PATH)/mcusw/binary/(driver name)_app/bin/am62dx_evm/

AM62PX

  • Ensure BUILD_OS_TYPE = baremetal
  • Go to folder ($SDK_INSTALL_PATH)/mcusw/build
  • gmake -s all BOARD=am62px_evm SOC=am62px BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal
  • On Successful compilation, binary folder would be created in ($SDK_INSTALL_PATH)/mcusw/binary/(driver name)_app/bin/am62px_evm/

Other useful commands


  1. To Clean all examples (all MCAL drivers and their associated examples)
    • gmake -s allclean
  2. To Build all examples (all MCAL drivers and their associated examples)
    • gmake -s all BOARD=am62x_evm SOC=am62x BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal
    • gmake -s all BOARD=am62ax_evm SOC=am62ax BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal
  3. To build specific example (associated MCAL driver will also be built)
    • gmake -s can_app BOARD=am62x_evm SOC=am62x BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal
    • gmake -s can_app BOARD=am62ax_evm SOC=am62ax BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal
    • Other examples cdd_ipc_app, dio_app, eth_app, eth_virtmac_app, gpt_app, mcspi_app, wdg_app, mcu_app
      • The above list is indicative and examples could be added/deleted
      • TO build cdd ipc linux application on AM62X use below command.
      • gmake -s cdd_ipc_app_rc_linux BOARD=am62x_evm SOC=am62x BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal CDD_IPC_LINUX_BUILD=yes
      • TO build cdd ipc linux application on AM62AX use below command.
      • gmake -s cdd_ipc_app_rc_linux BOARD=am62ax_evm SOC=am62ax BUILD_PROFILE=release CORE=mcu0_0 BUILD_OS_TYPE=baremetal CDD_IPC_LINUX_BUILD=yes
      • To determine example name, refer makefile in subdirectory of ($SDK_INSTALL_PATH)/mcusw/mcal/examples/
        • gmake -help, will list available target names

Profiles


  • Debug : Mostly used to development or debugging
    • BUILD_PROFILE=debug
  • Release : Recommended to be used for production / profiling performance
    • BUILD_PROFILE=release

Examples Linker File (Select memory location to hold example binary)


The example applications use different memory and this could be changed/re-configured.

  • linker_r5.lds defines the memory locations used by the MCAL examples.
    • The linker file is specific to a device/core and available at ($SDK_INSTALL_PATH)/mcusw/build/(device family name)/(core name)/linker_r5.lds
    • In case of AM62x, ($SDK_INSTALL_PATH)/mcusw/build/am62x/mcu0_0/linker_r5.lds
    • In case of AM62Ax, ($SDK_INSTALL_PATH)/mcusw/build/am62ax/mcu0_0/linker_r5.lds
    • In case of AM62Dx, ($SDK_INSTALL_PATH)/mcusw/build/am62dx/mcu0_0/linker_r5.lds
    • In case of AM62Px, ($SDK_INSTALL_PATH)/mcusw/build/am62px/mcu0_0/linker_r5.lds
    • Used for MCAL example application, that would be hosted on MCU 0 0

  • Memory that is used to hold, code, data impacts performance of the driver
  • When placed in internal memory (such OCMRAM) best performance is noted
  • It's recommended to place ISR code and other frequently used code/data in internal memory

Running Examples


IDE


CCS


Please refer (IDE (CCS)) for CCS and GEL setup

Load Example Binaries


AM62X/AM62AX/AM62PX/AM62DX

Using Linux boot

  1. Ensure bootmode of the EVM is configured to SD Card bootmode
  2. Use Balena Etcher application to flash the linux OS on the SD Card using the file tisdk-default-image-am62xx-evm.wic.xz downloaded from linux sdk
  3. Once the SD card is flashed, insert the SD Card to EVM and observe the UART logs to make sure the EVM is booted

Using SBL Bootflow

  1. In case of AM62X refer [AM62X EVM Setup Page] (https://software-dl.ti.com/mcu-plus-sdk/esd/AM62X/09_01_00_39/exports/docs/api_guide_am62x/EVM_SETUP_PAGE.html) for flashing using SBL bootflow
  2. In case of AM62AX refer [AM62AX EVM Setup Page] (https://software-dl.ti.com/mcu-plus-sdk/esd/AM62AX/09_01_00_39/exports/docs/api_guide_am62ax/EVM_SETUP_PAGE.html) for flashing using SBL bootflow
  3. In case of AM62DX refer [AM62DX EVM Setup Page] (http://swubn04.india.englab.ti.com/mcu_plus_sdk/sitmpurtos_nightly_mcu_plus_sdk_am62dx/latest/artifacts/output/webgen/exports/docs/api_guide_am62dx/EVM_SETUP_PAGE.html) for flashing using SBL bootflow
  4. In case of AM62PX refer [AM62PX EVM Setup Page] (https://software-dl.ti.com/mcu-plus-sdk/esd/AM62PX/09_01_00_39/exports/docs/api_guide_am62px/EVM_SETUP_PAGE.html) for flashing using SBL bootflow
AM62X: Steps to Load Example Binaries
  1. POWER-ON the EVM.
  2. Boot the hardware with required boot mode.
  3. CCS Setup & Steps to run from CCS Refer the [AM62X MCU+SDK] (https://software-dl.ti.com/mcu-plus-sdk/esd/AM62X/09_01_00_39/exports/docs/api_guide_am62x/CCS_LAUNCH_PAGE.html) user guide for generic test setup details and steps to run the examples using CCS.
  4. Do CPU Reset and Load binary (driver name)_app_mcu0_0_(release or debug).xer5f
    • AM62x MCAL Binaries will be available at ($SDK_INSTALL_PATH)/mcusw/binary/(driver name)_app/bin/am62x_evm/
    • Some of the example applications (ipc) would have more than 1 binaries. The name of the binaries specify the core that it's intended to hosted on
  5. After loading respective binary, Run example application to be tested.
  6. Console for demo application logs / messages

NOTE:

  1. MCAL is validated using SBL bootflow method except Fls and Fls is validated by stopping at U-Boot in Linux Boot.
  2. All the AM62X MCAL driver supports AM62Q as well except FLS because AM62Q has different flash chip than AM62X.
AM62AX: Steps to Load Example Binaries
  1. POWER-ON the EVM.
  2. Boot the hardware with required boot mode.
  3. CCS Setup & Steps to run from CCS Refer the [AM62AX MCU+SDK] (https://software-dl.ti.com/mcu-plus-sdk/esd/AM62AX/09_01_00_39/exports/docs/api_guide_am62ax/CCS_LAUNCH_PAGE.html) user guide for generic test setup details and steps to run the examples using CCS.
  4. Do CPU Reset and Load binary (driver name)_app_mcu0_0_(release or debug).xer5f
    • AM62Ax MCAL Binaries will be available at ($SDK_INSTALL_PATH)/mcusw/binary/(driver name)_app/bin/am62ax_evm/
    • Some of the example applications (ipc) would have more than 1 binaries. The name of the binaries specify the core that it's intended to hosted on
  5. After loading respective binary, Run example application to be tested.
  6. Console for demo application logs / messages
AM62DX: Steps to Load Example Binaries
  1. POWER-ON the EVM.
  2. Boot the hardware with required boot mode.
  3. CCS Setup & Steps to run from CCS Refer the [AM62DX MCU+SDK] (https://www.ti.com/tool/PROCESSOR-SDK-AM62D) user guide for generic test setup details and steps to run the examples using CCS.
  4. Do CPU Reset and Load binary (driver name)_app_mcu0_0_(release or debug).xer5f
    • AM62Dx MCAL Binaries will be available at ($SDK_INSTALL_PATH)/mcusw/binary/(driver name)_app/bin/am62dx_evm/
    • Some of the example applications (ipc) would have more than 1 binaries. The name of the binaries specify the core that it's intended to hosted on
  5. After loading respective binary, Run example application to be tested.
  6. Console for demo application logs / messages
AM62PX: Steps to Load Example Binaries
  1. POWER-ON the EVM.
  2. Boot the hardware with required boot mode.
  3. CCS Setup & Steps to run from CCS Refer the [AM62PX MCU+SDK] (https://software-dl.ti.com/mcu-plus-sdk/esd/AM62PX/09_01_00_39/exports/docs/api_guide_am62px/CCS_LAUNCH_PAGE.html) user guide for generic test setup details and steps to run the examples using CCS.
  4. Do CPU Reset and Load binary (driver name)_app_mcu0_0_(release or debug).xer5f
    • AM62Ax MCAL Binaries will be available at ($SDK_INSTALL_PATH)/mcusw/binary/(driver name)_app/bin/am62ax_evm/
    • Some of the example applications (ipc) would have more than 1 binaries. The name of the binaries specify the core that it's intended to hosted on
  5. After loading respective binary, Run example application to be tested.
  6. Console for demo application logs / messages

Back To Top


Compiler Flags used


MCAL Drivers - Profile : Release


Flag Description
-g Default behavior. Enables symbolic debugging. The generation of debug information do not impact optimizations. Therefore, generating debug information is enabled by default.
-c Disables linking
-qq Super Quite Mode
-pdsw225 Categorizes the diagnostic identified by num as a warning
-march direct the compiler to target a particular architecture
–endian=little Little Endian
-Wall Enable most warning categories
-Wno Disable the specified warning category.
-mv7R5 Processor Architecture Cortex-R5
-mcpu Select the target processor version.
-mfpu option to specify which floating-point hardware is available for use by the compiler
-mfloat-abi option in combination with the appropriate -mfpu option depending on what Arm processor variant is in use.
-Werror Treat detected warnings in the specified category as errors(e.g., unused variables, type mismatches)
–abi=eabi Application binary interface - ELF
-D_DEBUG_ it defines the _DEBUG macro.used to enable additional debugging features in code
–inline_recursion_limit It replaces a function call site with the body of the called function during compilation.The goal is to reduce the overhead of function calls and improve performance
-mthumb Select THUMB mode instructions (16-bit THUMB or T32 THUMB depending on which processor variant is selected) for current compilation; default for Cortex-M type architectures
-s Stop compilations after emitting compiler-generated assembly files; do not call assembler or linker.
–enum_type enumeration type (or enum type) is a value type defined by a set of named constants of an underlying integral numeric type.
-eo.oem4 Output Object file extension
-ea.sem4 Output assembly file extension
–symdebug:dwarf Generate symbolic debug in DWARF format
–embed_inline_assembly Embed inline assembly in code for optimization
–float_support=vfplib VFP coprocessor is enabled
-mv7M4 indicate which architecture and processor variant combination
–emit_warnings_as_errors Treat warning as errors
-os Interlists optimizer comments with assembly statements
–optimize_with_debug Optimize fully in the presence of debug
-mv5e indicate which architecture and processor variant combination.
-DBUILD_MCU0_0 Identifies Core in the domain
-DBUILD_MCU Identifies Domain
-Xlinker Required by TI Arm Clang
–diag_suppress Suppresses the diagnostic identified by num.
–ram_model option tells the linker to initialize variables at load time
–reread_libs option, you can force the linker to reread all libraries
-DSOC_AM62X Device Identifier
-DSOC_AM62AX Device Identifier
-DSOC_AM62PX Device Identifier
-DSOC_AM62DX Device Identifier

*Note – is actually 2 "-" dashes they simply appear as one long dash in the user Guide.

MCAL Examples - Profile : Release


Same flags that were used for driver (MCAL Drivers - Profile : Release)