![]() |
MCUSW
|
This files defines PWM MCAL configuration structures
Data Structures | |
| struct | Pwm_ChannelConfigType_PC |
| Pwm channel configuration. More... | |
| struct | Pwm_ConfigType_PC |
| Pwm configuration structure. More... | |
| struct | Pwm_ChannelConfigType |
| Pwm channel configuration. More... | |
| struct | Pwm_ConfigType |
| Pwm configuration structure. More... | |
| struct | Pwm_RegisterReadbackType |
| PWM register readback structure. More... | |
Functions | |
| void | Pwm_Ch0Notify (void) |
| EPWM Channel 0 ISR. | |
Macros | |
| #define | PWM_PRE_COMPILE_VARIANT (STD_ON ) |
| PWM Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time) | |
| #define | PWM_VARIANT_POST_BUILD (STD_OFF) |
| #define | PWM_DEINIT_API (STD_ON) |
| Enable/Disable PWM DeInit API. | |
| #define | PWM_SET_DUTY_CYCLE_API (STD_ON) |
| Enable/Disable PWM SetDutyCycle API. | |
| #define | PWM_SET_OUTPUT_TO_IDLE_API (STD_ON) |
| Enable/Disable PWM SetOutputToIdle API. | |
| #define | PWM_SET_PERIOD_AND_DUTY_API (STD_ON) |
| Enable/Disable PWM SetPeriodAndDuty API. | |
| #define | PWM_VERSION_INFO_API (STD_ON) |
| Enable/Disable PWM VersionInfo API. | |
| #define | PWM_REGISTER_READBACK_API (STD_ON) |
| Enable/Disable PWM RegisterReadback API. | |
| #define | PWM_DUTYCYCLE_UPDATED_ENDPERIOD (STD_ON) |
| Enable/Disable PWM Dutycycle update always at the end of the period. | |
| #define | PWM_PERIOD_UPDATED_ENDPERIOD (STD_ON) |
| Enable/Disable PWM Period update always at the end of the period. | |
| #define | PWM_ISR_TYPE (PWM_ISR_CAT1) |
| ISR type. | |
| #define | PWM_NUM_CHANNELS (1U) |
| Number of configured channels. | |
| #define | PWM_DEV_ERROR_DETECT (STD_ON) |
| Enable/Disable PWM dev detect error. | |
| #define | PWM_NOTIFICATION_SUPPORTED (STD_ON) |
| Enable/Disable PWM notifications. | |
| #define | PWM_OS_COUNTER_ID ((CounterType)OsCounter_0) |
| Counter ID for counter used to count wait ticks. | |
| #define | PWM_INDEX (0U) |
| Instance ID for driver module for EPWM usage. | |
| #define | PWM_INSTANCE_ID (PWM_INDEX) |
| #define | PWM_USE_EPWM |
| #define | PWM_TIMEOUT_DURATION (32000U) |
| timeout. Each tick is 31.25us (for 32K Counter). Wait for 5s which comes to below value | |
| #define | PwmConf_PwmChannel_PwmChannel_0 (0U) |
| Channel ID Symbolic Names Configured channel ID(s) | |
| #define | PWM_INIT_CONFIG_PC PwmChannelConfigSet |
| Pre Compile config macro name. | |
| #define | EHRPWM_BASE_OFFSET 0x0U |
| #define | PWM_MAX_NUM_CHANNELS (3U) |
| #define | PWM_CHANNEL0 (0U) |
| EPWM Channel 0, in MCU DOMAIN. | |
PWM Driver State Values | |
The PWM Driver State Values | |
| enum | Pwm_OutputStateType { PWM_LOW = 0U , PWM_HIGH } |
| Possible output states of a PWM channel. More... | |
| enum | Pwm_EdgeNotificationType { PWM_RISING_EDGE = 1U , PWM_FALLING_EDGE = 2U , PWM_BOTH_EDGES = 3U } |
| Possible edge notification More... | |
| enum | Pwm_ChannelClassType { PWM_FIXED_PERIOD = 0U , PWM_FIXED_PERIOD_SHIFTED , PWM_VARIABLE_PERIOD } |
| Period type for pwm channels. Fixed periods prohibit changes to the period length with Pwm_SetPeriod( ). PWM_FIXED_PERIOD_SHIFTED type is not supported due to hardware restrictions of the PWM unit. More... | |
| enum | Pwm_epwmOutputCh_t { EPWM_OUTPUT_CH_A = 0U , EPWM_OUTPUT_CH_B = 1U , EPWM_OUTPUT_CH_BOTH_A_AND_B = 2U } |
| EPWM outputs in a single epwm channel. More... | |
| typedef uint32 | Pwm_PeriodType |
| typedef of period value | |
| typedef uint32 | Pwm_ChannelType |
| PWM Channel type. | |
| typedef uint32 | Pwm_FrequencyType |
| typedef of frequency value (Frequency in Hz) | |
| typedef void(* | Pwm_NotifyFuncType) (void) |
| Notification callback function pointer | |
| void | Pwm_Init (const Pwm_ConfigType *CfgPtr) |
| Service for PWM initialization. | |
| void | Pwm_DeInit (void) |
| Service for PWM de-initialization. | |
| void | Pwm_SetDutyCycle (Pwm_ChannelType ChannelNumber, uint16 DutyCycle) |
| Service for setting Duty Cycle. | |
| void | Pwm_SetPeriodAndDuty (Pwm_ChannelType ChannelNumber, Pwm_PeriodType Period, uint16 DutyCycle) |
| Service for setting Period and Duty Cycle. | |
| void | Pwm_SetOutputToIdle (Pwm_ChannelType ChannelNumber) |
| Service to set the output of a channel immediately to idle. | |
| Pwm_OutputStateType | Pwm_GetOutputState (Pwm_ChannelType ChannelNumber) |
| void | Pwm_DisableNotification (Pwm_ChannelType ChannelNumber) |
| Service to disable the Edge Notification. | |
| void | Pwm_EnableNotification (Pwm_ChannelType ChannelNumber, Pwm_EdgeNotificationType Notification) |
| Service to enable the Edge Notification. | |
| void | Pwm_GetVersionInfo (Std_VersionInfoType *versioninfo) |
| This service returns the version information of this module. | |
| Std_ReturnType | Pwm_RegisterReadback (Pwm_ChannelType ChannelNumber, Pwm_RegisterReadbackType *RegRbPtr) |
| This function reads the important registers of the hardware unit and returns the value in the structure. | |
| #define PWM_PRE_COMPILE_VARIANT (STD_ON ) |
PWM Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time)
| #define PWM_VARIANT_POST_BUILD (STD_OFF) |
| #define PWM_DEINIT_API (STD_ON) |
Enable/Disable PWM DeInit API.
| #define PWM_SET_DUTY_CYCLE_API (STD_ON) |
Enable/Disable PWM SetDutyCycle API.
| #define PWM_SET_OUTPUT_TO_IDLE_API (STD_ON) |
Enable/Disable PWM SetOutputToIdle API.
| #define PWM_SET_PERIOD_AND_DUTY_API (STD_ON) |
Enable/Disable PWM SetPeriodAndDuty API.
| #define PWM_VERSION_INFO_API (STD_ON) |
Enable/Disable PWM VersionInfo API.
| #define PWM_REGISTER_READBACK_API (STD_ON) |
Enable/Disable PWM RegisterReadback API.
| #define PWM_DUTYCYCLE_UPDATED_ENDPERIOD (STD_ON) |
Enable/Disable PWM Dutycycle update always at the end of the period.
| #define PWM_PERIOD_UPDATED_ENDPERIOD (STD_ON) |
Enable/Disable PWM Period update always at the end of the period.
| #define PWM_ISR_TYPE (PWM_ISR_CAT1) |
ISR type.
| #define PWM_NUM_CHANNELS (1U) |
Number of configured channels.
| #define PWM_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable PWM dev detect error.
| #define PWM_NOTIFICATION_SUPPORTED (STD_ON) |
Enable/Disable PWM notifications.
| #define PWM_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks.
| #define PWM_INDEX (0U) |
Instance ID for driver module for EPWM usage.
| #define PWM_INSTANCE_ID (PWM_INDEX) |
| #define PWM_USE_EPWM |
| #define PWM_TIMEOUT_DURATION (32000U) |
timeout. Each tick is 31.25us (for 32K Counter). Wait for 5s which comes to below value
| #define PwmConf_PwmChannel_PwmChannel_0 (0U) |
Channel ID Symbolic Names Configured channel ID(s)
Channel identifiers
| #define PWM_INIT_CONFIG_PC PwmChannelConfigSet |
Pre Compile config macro name.
| #define EHRPWM_BASE_OFFSET 0x0U |
| #define PWM_MAX_NUM_CHANNELS (3U) |
| #define PWM_CHANNEL0 (0U) |
EPWM Channel 0, in MCU DOMAIN.
| typedef uint32 Pwm_PeriodType |
typedef of period value
| typedef uint32 Pwm_ChannelType |
PWM Channel type.
| typedef uint32 Pwm_FrequencyType |
typedef of frequency value (Frequency in Hz)
| typedef void(* Pwm_NotifyFuncType) (void) |
Notification callback function pointer
| enum Pwm_OutputStateType |
| enum Pwm_ChannelClassType |
Period type for pwm channels. Fixed periods prohibit changes to the period length with Pwm_SetPeriod( ). PWM_FIXED_PERIOD_SHIFTED type is not supported due to hardware restrictions of the PWM unit.
| Enumerator | |
|---|---|
| PWM_FIXED_PERIOD | Period is immutable |
| PWM_FIXED_PERIOD_SHIFTED | Period is immutable with phase shift |
| PWM_VARIABLE_PERIOD | Period is variable |
| enum Pwm_epwmOutputCh_t |
| void Pwm_Init | ( | const Pwm_ConfigType * | CfgPtr | ) |
Service for PWM initialization.
* Service name : Pwm_Init * Syntax : Pwm_Init(P2CONST(Pwm_ConfigType, * AUTOMATIC, PWM_PBCFG) ConfigPtr) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : Pointer to the configuration * Parameters (out) : None * Return value : void * Description : Initializes internal variables * and the PWM unit of the micro controller. * The function can be called on task level. *
| void Pwm_DeInit | ( | void | ) |
Service for PWM de-initialization.
* Service name : Pwm_DeInit * Syntax : Pwm_DeInit(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (out) : None * Return value : void * Description : After DeInit output states should be in idle level * (it is configurable whether reset state is restored or * if channel output states are really set to idle). * The function can be called on task level. *
| void Pwm_SetDutyCycle | ( | Pwm_ChannelType | ChannelNumber, |
| uint16 | DutyCycle ) |
Service for setting Duty Cycle.
* Service name : Pwm_SetDutyCycle * Syntax : Pwm_SetDutyCycle(Pwm_ChannelType Channel, * uint16 DutyCycle) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x02 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Pwm_ChannelType Channel * Parameters (in) : uint16 DutyCycle * Parameters (out) : None * Return value : void * Description : This service sets the duty cycle for a channel * if DutyCycle is 0%, set output to inverse of polarity * if DutyCycle is >= 100%, set output to polarity * if 0% < DutyCycle < 100%, set output accordingly * The function can be called on task level. *
| void Pwm_SetPeriodAndDuty | ( | Pwm_ChannelType | ChannelNumber, |
| Pwm_PeriodType | Period, | ||
| uint16 | DutyCycle ) |
Service for setting Period and Duty Cycle.
* Service name : Pwm_SetPeriodAndDuty * Syntax : Pwm_SetPeriodAndDuty(Pwm_ChannelType Channel, * Pwm_PeriodType Period, uint16 DutyCycle) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x03 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Pwm_ChannelType Channel * Parameters (in) : Pwm_PeriodType Period * Parameters (in) : uint16 DutyCycle * Parameters (out) : None * Return value : void * Description : This service sets period and duty cycle for a channel * if DutyCycle is 0%, set output to inverse of polarity * if DutyCycle is >= 100%, set output to polarity * if 0% < DutyCycle < 100%, set output accordingly * The function can be called on task level. *
| void Pwm_SetOutputToIdle | ( | Pwm_ChannelType | ChannelNumber | ) |
Service to set the output of a channel immediately to idle.
* Service name : Pwm_SetOutputToIdle * Syntax : Pwm_SetOutputToIdle(Pwm_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x04 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Pwm_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service sets the output of a channel * immediately to idle. The idle output level * is configured in driver configuration. * The function can be called on task level. *
| Pwm_OutputStateType Pwm_GetOutputState | ( | Pwm_ChannelType | ChannelNumber | ) |
| void Pwm_DisableNotification | ( | Pwm_ChannelType | ChannelNumber | ) |
Service to disable the Edge Notification.
* Service name : Pwm_DisableNotification * Syntax : Pwm_DisableNotification(Pwm_ChannelType ChannelNumber) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x06 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Pwm_ChannelType ChannelNumber * Parameters (out) : None * Return value : None * Description : Disables the Edge Notification * This service deactivates the Edge Notification for the * pwm channel specified by the ChannelNumber Parameter. * The function can be called on task level. *
| void Pwm_EnableNotification | ( | Pwm_ChannelType | ChannelNumber, |
| Pwm_EdgeNotificationType | Notification ) |
Service to enable the Edge Notification.
* Service name : Pwm_EnableNotification * Syntax : Pwm_EnableNotification (Pwm_ChannelType Channel, * Pwm_EdgeNotificationType Notification) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Pwm_ChannelType ChannelNumber * Parameters (in) : Pwm_EdgeNotificationType Notification * Parameters (out) : None * Return value : None * Description : Enables the Edge Notification * This service enables the notification of the chosen * edges for the Pwm channel specified by the * ChannelNumber.The function can be called on task level *
| void Pwm_GetVersionInfo | ( | Std_VersionInfoType * | versioninfo | ) |
This service returns the version information of this module.
* Service name : Pwm_GetVersionInfo * Syntax : Pwm_GetVersionInfo(P2VAR(Std_VersionInfoType, * AUTOMATIC, PWM_APPL_DATA) versioninfo) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x08 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Std_VersionInfoType - Version info. * Parameters (out) : None * Return value : void * Description : Returns the version information of this module. * The function can be called on task level. *
| Std_ReturnType Pwm_RegisterReadback | ( | Pwm_ChannelType | ChannelNumber, |
| Pwm_RegisterReadbackType * | RegRbPtr ) |
This function reads the important registers of the hardware unit and returns the value in the structure.
* Service name : Pwm_RegisterReadback(Pwm_ChannelType ChannelNumber,
* Pwm_RegisterReadbackType *RegRbPtr)
* Sync/Async : Synchronous
* Reentrancy : Reentrant
* Service ID[hex] : 0x0D
* Parameters (in) : Pwm_ChannelType ChannelNumber
* Parameters (inout) : RegRbPtr - Pointer to where to store the readback
* values. If this pointer is NULL, then the API
* will return E_NOT_OK.
* Description : This API is used to check the status of critical
registers which donot change during program execution.
* Return value : Std_ReturnType
* E_OK: Register read back has been done successfully
* E_NOT_OK: Register read back failed
*
| void Pwm_Ch0Notify | ( | void | ) |
EPWM Channel 0 ISR.
| Pwm_ChannelType Pwm_ChannelConfigType_PC::channelId |
| uint32 Pwm_ChannelConfigType_PC::outputCh |
Output Select EPWMxA or EPWMxB or both(EPWMxA and EPWMxB)
| Pwm_ChannelConfigType_PC Pwm_ConfigType_PC::chCfg[PWM_NUM_CHANNELS] |
Channel configurations
| uint32 Pwm_ChannelConfigType::instanceClkHz |
System clock frequency
| uint16 Pwm_ChannelConfigType::dutyCycle |
Initial dutycycle
| uint32 Pwm_ChannelConfigType::hwPeriod |
Number of HW Unit ticks value which sets initial period
| Pwm_OutputStateType Pwm_ChannelConfigType::polarity |
Initial polarity
| Pwm_OutputStateType Pwm_ChannelConfigType::idleState |
Initial idle state
| Pwm_ChannelClassType Pwm_ChannelConfigType::channelClass |
Fixed or Variable period
| uint32 Pwm_ChannelConfigType::prescale |
Prescaler, part of PWM HW time-base clock Range - 0 <= prescale <= 7, TBCLK = SYSCLK / (prescale) 0x0 = /1 (No prescale) 0x1 = /2 0x2 = /4 0x3 = /8 0x4 = /16 0x5 = /32 0x6 = /64 0x7 = /128
| uint32 Pwm_ChannelConfigType::hsPrescale |
High-Speed Prescaler, part for PWM HW time-base clock Range - 0 <= prescale <= 7, TBCLK = SYSCLK / (hsPrescale x prescale) 0x0 = /1 (No prescale) 0x1 = /2 0x2 = /4 0x3 = /6 0x4 = /8 0x5 = /10 0x6 = /12 0x7 = /14
| boolean Pwm_ChannelConfigType::enableHR |
Enable High Resolution Capacbility
| Pwm_NotifyFuncType Pwm_ChannelConfigType::notificationHandler |
Notification handler
| Pwm_ChannelConfigType Pwm_ConfigType::chCfg[PWM_NUM_CHANNELS] |
Channel configurations
| uint16 Pwm_RegisterReadbackType::pwmTbCtl |
Time base control register
| uint16 Pwm_RegisterReadbackType::pwmTbPhs |
Time base counter phase register
| uint16 Pwm_RegisterReadbackType::pwmTbCnt |
Time base counter register
| uint16 Pwm_RegisterReadbackType::pwmAqCtlA |
Action Qualifier Control Register for Output A
| uint16 Pwm_RegisterReadbackType::pwmAqCtlB |
Action Qualifier Control Register for Output B
| uint16 Pwm_RegisterReadbackType::pwmDbCtl |
| uint16 Pwm_RegisterReadbackType::pwmTzSel |
< Dead Band Generator Control Register
| uint16 Pwm_RegisterReadbackType::pwmTzCtl |
< Trip-zone Select Register
| uint16 Pwm_RegisterReadbackType::pwmPcCtl |
< Trip-zone Control Register
| uint16 Pwm_RegisterReadbackType::pwmTbsts |
< PWM Chopper Control Register
| uint16 Pwm_RegisterReadbackType::pwmTbprd |
< Time-Base Status Register
| uint16 Pwm_RegisterReadbackType::pwmAqsfrc |
< Time-Base Period Register
| uint16 Pwm_RegisterReadbackType::pwmAqcsfrc |
< Action Qualifier Software Force Register
| uint16 Pwm_RegisterReadbackType::pwmDbred |
| uint16 Pwm_RegisterReadbackType::pwmDbfed |
| uint16 Pwm_RegisterReadbackType::pwmEtsel |
|
extern |
|
extern |
PWM Configuration structure declaration.
|
extern |