112#define WDG_VARIANT_PRE_COMPILE (STD_ON)
117#define WDG_INIT_CONFIG_PC WdgSettingsConfig
122#define WDG_DEV_ERROR_DETECT (STD_ON)
125#define WDG_GET_VERSION_INFO_API (STD_ON)
128#define WDG_REGISTER_READBACK_API (STD_ON)
132#define WDG_MAX_TIMEOUT ((uint16)65535)
136#define WDG_RTI_FREQUENCY ((uint32)12500000)
139#define WDG_DISABLE_ALLOWED (STD_OFF)
148#define WdgConf_WdgGeneral_WdgIndex_0 (0U)
159#define DemConf_DemEventParameter_WDG_DEM_NO_EVENT (0xFFFFU)
160#define WDG_DEM_NO_EVENT DemConf_DemEventParameter_WDG_DEM_NO_EVENT
162#ifndef WDG_E_MODE_FAILED
164#define WDG_E_MODE_FAILED DemConf_DemEventParameter_WDG_E_MODE_FAILED
167#ifndef WDG_E_DISABLE_REJECTED
169#define WDG_E_DISABLE_REJECTED DemConf_DemEventParameter_WDG_E_DISABLE_REJECTED
172#define WDG_NUM_INSTANCE (12U)
187extern CONST(uint32, WDG_CONST)
const struct Wdg_ConfigType_s WdgSettingsConfig
WDG Configuration struct declaration.
const uint32 RTIHwUnit_BaseAddr[WDG_NUM_INSTANCE]
Base Address of the watchdog instances.
const struct Wdg_ConfigType_PC_s WdgSettingsConfig_PC
WDG Configuration pre compile struct declaration.
#define WDG_NUM_INSTANCE
Definition Wdg_Cfg.h:172