4.4. CDD DMA Module

4.4.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

BSW

Basic Software

DET

Default Error Tracer

CDD

Complex Device Driver

DMA

Direct Memory Access

ISR

Interrupt Service Routine

INT

Interrupt

HW

Hardware

SW

Software

MCU

Micro Controller Unit

OS

Operating System

API

Application Programming Interface

4.4.2. Introduction

This document describes the functionality and configuration of the Cdd_Dma module.

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile

Vendor ID

DMA_VENDOR_ID (44)

Module ID

DMA_MODULE_ID (255)

Supported Platform

AM263x

The Cdd_Dma module initiates memory transfer without the intervention of the CPU and used in data transfer within peripheral, based on DMA channel configured.

4.4.3. Functional Overview

Cdd_Dma Driver using HW IP “EDMA”(Enhanced DMA). EDMA performs high-performance data transfer between two target endpoints, memories and peripheral devices without microcontroller support during transfer. EDMA transfer is programmed through a logical EDMA channel which allows the transfer to be optimally tailored to the requirements of the application.

The EDMA controller is based on two major principal blocks:

• EDMA third-party channel controller (EDMA_TPCC)

• EDMA third-party transfer controller (EDMA_TPTC)

Basic Working Principle

Fig. 4.25 Basic Working Principle

The TPCC is a high flexible channel controller that serves as both a user interface and an event interface for the EDMA controller. The EDMA_TPCC serves to prioritize incoming software requests or events from peripherals, and submits transfer requests (TRs) to the transfer controller.

The TPTC performs read and write transfers by EDMA ports to the target peripherals, as programmed in the Active and Pending set of the registers. The transfer controllers are responsible for data movement, and issue read/write commands to the source and destination addresses programmed for a given transfer in the EDMA_TPCC.

The Cdd_Dma module has 64 EDMA channels, which serves the purpose of driving transferring of data.

4.4.3.1. Initialization

Cdd_Dma_Init() has to be called to initialize the Cdd_Dma driver.

4.4.3.2. States

None

4.4.3.3. Assumptions

Driver assumes that cache initialization is done in application only and not done by the driver.

4.4.3.4. Limitations

Below are the IP’s that needed software workaround with EDMA because of the HW Limitations -

  1. UART : A dummy PaRAM needs to be linked to the actual TX PaRAM. This is because UART generates TX empty event after the last character is transferred and it results in an event miss error being set in EDMA (since the TX PaRAM has already been used up for the transfer). A dummy PaRAM set is linked to the actual TX PaRAM to service the extra event generated.

  2. McSpi : Above scenario also applies to McSPI. A dummy PaRAM set is linked to solve the issue.

NOTE: Both of these above limitations are taken care internally by UART and McSpi driver respectively.

4.4.3.5. Design overview

Please refer SITARA MCU MCAL Architecture Document and MCAL: CDD DMA Detailed Design Document provided as part of CSP.

4.4.4. Hardware Features

4.4.4.1. IP Supported Features

  • EDMA channels are supported.

  • Both memory transfer and transfer within peripheral is supported.

  • Both interrupt mode and polling mode are supported.

  • Linking of multiple params are supported.

  • Chaining of multiple channels are supported.

4.4.4.2. Not supported Features

  • QDMA is not supported.

4.4.4.3. Non compliance

4.4.4.3.1. Deviations to requirements (Requirement Traceability)

4.4.4.3.1.1. Deviation of requirements against AUTOSAR specification requirements

None

4.4.5. Source files

Static source C Files are defined below

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Dma
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Cdd_Dma.h : Contains the API’s of the Cdd_Dma driver to be used by upper layers.
┃ ┃ ┃ ┣ 📜Cdd_Dma_cslr_tpcc.h : Contains Internal functions definition and initialization of Cdd_Dma driver.
┃ ┃ ┃ ┣ 📜Cdd_Dma_cslr_tptc.h : Contains Internal functions definition and initialization of Cdd_Dma driver.
┃ ┃ ┃ ┣ 📜Cdd_Dma_edma.h : Contains Internal functions definition and initialization of Cdd_Dma driver.
┃ ┃ ┃ ┣ 📜Cdd_Dma_Irq.h : Contains ISR function declaration.
┃ ┃ ┃ ┗ 📜Cdd_Dma_Priv.h : Contains Internal functions definition and initialization of Cdd_Dma driver.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Cdd_Dma.c : Contains the implementation of the API’s for Cdd_Dma driver.
┃ ┃ ┃ ┣ 📜Cdd_Dma_Irq.c : Contains ISR function definitions.
┃ ┃ ┃ ┗ 📜Cdd_Dma_Priv.c : Contains Internal functions definition and initialization of Cdd_Dma driver.
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┗ 📜Cdd_Dma_dmaxbar.h : Contains DMA cross bar interrupt information.
┃ ┃ ┃ ┣ 📜Cdd_Dma_soc.c : Contains device specific a function definition, data types and definitions.
┃ ┃ ┃ ┗ 📜Cdd_Dma_trig_xbar.h : Contains DMA cross bar interrupt information.
┃ ┃ ┃ ┣ 📜Cdd_Dma_xbar.h : Contains DMA cross bar interrupt information.
┃ ┃ ┗ 📜Makefile
┃ 📂mcal_config
┃ 📂mcal_docs
┃ 📜README.txt

Plugin files are defined below in the table.

Plugin Files

Description

CDD_Dma_Cfg.h

Contains the Precompile switches, Symbolic names of the handles and xbar, HW units

CDD_Dma_Cfg.c

contains the configuration parameters

4.4.6. Module requirements

Please refer Software Product Specification document provided as part of CSP.

4.4.6.1. Memory Mapping

Memory Mapping Sections

CDD_DMA_CODE

CDD_DMA_CODE_ISR

CDD_DMA_VAR_NO_INIT

CDD_DMA_VAR

CDD_DMA_CFG

CDD_DMA_START_SEC_VAR_INIT_8 (.bss)

x

CDD_DMA_STOP_SEC_VAR_INIT_8

x

CDD_DMA_START_SEC_CONFIG_DATA (.const)

x

CDD_DMA_STOP_SEC_CONFIG_DATA

x

CDD_DMA_START_SEC_CODE (.text)

x

CDD_DMA_STOP_SEC_CODE

x

CDD_DMA_START_SEC_VAR_INIT_32 (.bss)

x

CDD_DMA_STOP_SEC_VAR_INIT_32

x

CDD_DMA_START_SEC_VAR_NO_INIT_UNSPECIFIED (.data)

x

CDD_DMA_STOP_SEC_VAR_NO_INIT_UNSPECIFIED

x

CDD_DMA_START_SEC_ISR_CODE

x

CDD_DMA_STOP_SEC_ISR_CODE

x

4.4.6.2. Scheduling

There are no scheduled functions within the CDD DMA driver

4.4.6.3. Error handling

4.4.6.3.1. Development Error Reporting (DET)

In development mode, the Cdd_Dma module reports development error through the Det_ReportError function of module DET. The errors reported to DET are described in the following table

Type of Error

Related Error code

Value (Hex)

API service called without module initialization.

CDD_DMA_E_UNINIT

0x01

API service for initialization is called when already initialized.

CDD_DMA_E_ALREADY_INITIALIZED

0x02

API parameter checking: invalid value.

CDD_DMA_E_PARAM_VALUE

0x03

API parameter checking: invalid pointer.

CDD_DMA_E_PARAM_POINTER

0x04

API service for indicating callback is already registered

CDD_DMA_E_ALREADY_REGISTERED

0x05

API service for indicating DMA handle already in use

CDD_DMA_E_ALREADY_IN_PROGRESS

0x06

4.4.6.3.2. Runtime Errors

None

4.4.7. Used resources

4.4.7.1. Interrupt Handling

Cdd_Dma driver provides ISR for transfer completion detection. The interrupt category must be configured in Cdd_Dma Driver and OS modules.

Respective ISR for each Cdd_Dma Instance in AM263x are as follows:

Cdd_Dma Instances

ISR Routines

CDD_DMA_MSS_A

CDD_EDMA_lld_transferCompletionMasterIsrFxn()

CDD_DMA_MSS_A instance of Cdd_Dma has interrupt number as “72” in AM263x.

4.4.8. Integration description

4.4.8.1. Dependent modules

4.4.8.1.1. MCU

The module MCU powers up the microcontroller’s peripherals at startup time and initializes the PLL as well as the internal clock domains which is connected to the Cdd_Dma unit.

The Cdd_Dma module will not take care of settings which configure the clock and PLL for channels in its init function. This must be done by the MCU module.

4.4.8.1.2. PORT

The Port driver configures the port pins used for the Cdd_Dma driver as input or output. Hence, the Port driver has to be initialized prior to the use of Cdd_Dma functions. Otherwise, Cdd_Dma driver functions will exhibit undefined behavior.

4.4.8.1.3. OS

An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table.The Cdd_Dma module may use AUTOSAR OS to suspend and restore global interrupts.

4.4.8.1.4. DET

The module PWM depends on the DET (by default) in order to report development errors.

4.4.8.1.5. DEM

None

4.4.8.1.6. Callback Functions

None

4.4.8.1.7. Callback Notification

None

4.4.8.1.8. SchM (Optional)

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that DMA module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator. For DMA Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

DMA Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

DMA_EXCLUSIVE_AREA_0

Cdd_Edma_lld_intrRegister

To protect against multiple access for shared resources

ALL_INTERRUPT_BLOCKING : All interrupts should be blocked as this API’s can be called in the interrupts

4.4.8.2. Multi-core support

Not supported

4.4.9. Configuration

4.4.9.1. CddDmaDriverHandler

This container contains the configuration parameters and sub containers of the AUTOSAR Complex device driver (CDD) module.

4.4.9.1.1. CddDmaTransferType

Item

Name

CddDmaTransferType

Description

This parameter selects the desired Transfer Type.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_DMA_TRANSFER_TYPE_MEMORY_TRANSFER

Range

CDD_DMA_TRANSFER_TYPE_UART_TX
CDD_DMA_TRANSFER_TYPE_UART_RX
CDD_DMA_TRANSFER_TYPE_ADC
CDD_DMA_TRANSFER_TYPE_MCSPI
CDD_DMA_TRANSFER_TYPE_MEMORY_TRANSFER
CDD_DMA_TRANSFER_TYPE_FLS

4.4.9.1.2. CddDmaInstance

Item

Name

CddDmaInstance

Description

This parameter selects the desired instance for DMA.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_DMA_MSS_A

Range

CDD_DMA_MSS_A

4.4.9.1.3. CddDmaRegionID

Item

Name

CddDmaRegionID

Description

This parameter specifies the Region ID for EDMA.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

7

Min-value

0

4.4.9.1.4. CddDmaTccNumber

Item

Name

CddDmaTccNumber

Description

This parameter specifies the TCC number for EDMA.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

63

Min-value

0

4.4.9.1.5. CddDmaQueueNumber

Item

Name

CddDmaQueueNumber

Description

This parameter specifies the Default Queue Number for EDMA.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

1

Min-value

0

4.4.9.1.6. CddDmaEnableInterrupt

Item

Name

CddDmaEnableInterrupt

Description

This determines whether interrupt needs to be registered.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.4.9.1.7. CddDmaTransferModeSelect

Item

Name

CddDmaTransferModeSelect

Description

This parameter selects the desired Transfer Modeselect either normal or linking or chaining.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_DMA_TRANSFER_MODE_NORMAL

Range

CDD_DMA_TRANSFER_MODE_NORMAL
CDD_DMA_TRANSFER_MODE_LINKING
CDD_DMA_TRANSFER_MODE_CHAINING

4.4.9.1.8. CddDmaChannelGroup

This container contains the DMA Channel Group.

4.4.9.1.8.1. CddDmaChannel

Item

Name

CddDmaChannel

Description

This parameter select the channel number to be used.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

63

Min-value

0

4.4.9.1.9. CddDmaParamSets

This container contains the DMA params.

4.4.9.1.9.1. CddDmaPramNumber

Item

Name

CddDmaPramNumber

Description

This parameter select the param number to be used.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

4.4.9.1.10. CddDmaChannelTriggerConfiguration

This container contains the DMA Channel Trigger reasource.

4.4.9.1.10.1. CddDmaDmaChannelModule

Item

Name

CddDmaDmaChannelModule

Description

The DMA channel selected for module.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_DMA_TRIG_XBAR_EDMA_MODULE_0

Range

CDD_DMA_TRIG_XBAR_EDMA_MODULE_0
CDD_DMA_TRIG_XBAR_EDMA_MODULE_1
CDD_DMA_TRIG_XBAR_EDMA_MODULE_2
CDD_DMA_TRIG_XBAR_EDMA_MODULE_3
CDD_DMA_TRIG_XBAR_EDMA_MODULE_4
CDD_DMA_TRIG_XBAR_EDMA_MODULE_5
CDD_DMA_TRIG_XBAR_EDMA_MODULE_6
CDD_DMA_TRIG_XBAR_EDMA_MODULE_7
CDD_DMA_TRIG_XBAR_EDMA_MODULE_8
CDD_DMA_TRIG_XBAR_EDMA_MODULE_9
CDD_DMA_TRIG_XBAR_EDMA_MODULE_10
CDD_DMA_TRIG_XBAR_EDMA_MODULE_11
CDD_DMA_TRIG_XBAR_EDMA_MODULE_12
CDD_DMA_TRIG_XBAR_EDMA_MODULE_13
CDD_DMA_TRIG_XBAR_EDMA_MODULE_14
CDD_DMA_TRIG_XBAR_EDMA_MODULE_15
CDD_DMA_TRIG_XBAR_EDMA_MODULE_16
CDD_DMA_TRIG_XBAR_EDMA_MODULE_17
CDD_DMA_TRIG_XBAR_EDMA_MODULE_18
CDD_DMA_TRIG_XBAR_EDMA_MODULE_19
CDD_DMA_TRIG_XBAR_EDMA_MODULE_20
CDD_DMA_TRIG_XBAR_EDMA_MODULE_21
CDD_DMA_TRIG_XBAR_EDMA_MODULE_22
CDD_DMA_TRIG_XBAR_EDMA_MODULE_23
CDD_DMA_TRIG_XBAR_EDMA_MODULE_24
CDD_DMA_TRIG_XBAR_EDMA_MODULE_25
CDD_DMA_TRIG_XBAR_EDMA_MODULE_26
CDD_DMA_TRIG_XBAR_EDMA_MODULE_27
CDD_DMA_TRIG_XBAR_EDMA_MODULE_28
CDD_DMA_TRIG_XBAR_EDMA_MODULE_29
CDD_DMA_TRIG_XBAR_EDMA_MODULE_30
CDD_DMA_TRIG_XBAR_EDMA_MODULE_31
CDD_DMA_TRIG_XBAR_EDMA_MODULE_32
CDD_DMA_TRIG_XBAR_EDMA_MODULE_33
CDD_DMA_TRIG_XBAR_EDMA_MODULE_34
CDD_DMA_TRIG_XBAR_EDMA_MODULE_35
CDD_DMA_TRIG_XBAR_EDMA_MODULE_36
CDD_DMA_TRIG_XBAR_EDMA_MODULE_37
CDD_DMA_TRIG_XBAR_EDMA_MODULE_38
CDD_DMA_TRIG_XBAR_EDMA_MODULE_39
CDD_DMA_TRIG_XBAR_EDMA_MODULE_40
CDD_DMA_TRIG_XBAR_EDMA_MODULE_41
CDD_DMA_TRIG_XBAR_EDMA_MODULE_42
CDD_DMA_TRIG_XBAR_EDMA_MODULE_43
CDD_DMA_TRIG_XBAR_EDMA_MODULE_44
CDD_DMA_TRIG_XBAR_EDMA_MODULE_45
CDD_DMA_TRIG_XBAR_EDMA_MODULE_46
CDD_DMA_TRIG_XBAR_EDMA_MODULE_47
CDD_DMA_TRIG_XBAR_EDMA_MODULE_48
CDD_DMA_TRIG_XBAR_EDMA_MODULE_49
CDD_DMA_TRIG_XBAR_EDMA_MODULE_50
CDD_DMA_TRIG_XBAR_EDMA_MODULE_51
CDD_DMA_TRIG_XBAR_EDMA_MODULE_52
CDD_DMA_TRIG_XBAR_EDMA_MODULE_53
CDD_DMA_TRIG_XBAR_EDMA_MODULE_54
CDD_DMA_TRIG_XBAR_EDMA_MODULE_55
CDD_DMA_TRIG_XBAR_EDMA_MODULE_56
CDD_DMA_TRIG_XBAR_EDMA_MODULE_57
CDD_DMA_TRIG_XBAR_EDMA_MODULE_58
CDD_DMA_TRIG_XBAR_EDMA_MODULE_59
CDD_DMA_TRIG_XBAR_EDMA_MODULE_60
CDD_DMA_TRIG_XBAR_EDMA_MODULE_61
CDD_DMA_TRIG_XBAR_EDMA_MODULE_62
CDD_DMA_TRIG_XBAR_EDMA_MODULE_63

4.4.9.1.10.2. CddDmaChannelTriggerSource

Item

Name

CddDmaChannelTriggerSource

Description

Source to Trigger DMA Channel.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_0

Range

CDD_DMA_TRIG_XBAR_LIN0_RXDMA
CDD_DMA_TRIG_XBAR_LIN0_TXDMA
CDD_DMA_TRIG_XBAR_LIN1_RXDMA
CDD_DMA_TRIG_XBAR_LIN1_TXDMA
CDD_DMA_TRIG_XBAR_LIN2_RXDMA
CDD_DMA_TRIG_XBAR_LIN2_TXDMA
CDD_DMA_TRIG_XBAR_LIN3_RXDMA
CDD_DMA_TRIG_XBAR_LIN3_TXDMA
CDD_DMA_TRIG_XBAR_LIN4_RXDMA
CDD_DMA_TRIG_XBAR_LIN4_TXDMA
CDD_DMA_TRIG_XBAR_I2C0_TX
CDD_DMA_TRIG_XBAR_I2C0_RX
CDD_DMA_TRIG_XBAR_I2C1_TX
CDD_DMA_TRIG_XBAR_I2C1_RX
CDD_DMA_TRIG_XBAR_I2C2_TX
CDD_DMA_TRIG_XBAR_I2C2_RX
CDD_DMA_TRIG_XBAR_I2C3_TX
CDD_DMA_TRIG_XBAR_I2C3_RX
CDD_DMA_TRIG_XBAR_SPI0_DMA_READ_REQ0
CDD_DMA_TRIG_XBAR_SPI0_DMA_READ_REQ1
CDD_DMA_TRIG_XBAR_SPI0_DMA_READ_REQ2
CDD_DMA_TRIG_XBAR_SPI0_DMA_READ_REQ3
CDD_DMA_TRIG_XBAR_SPI0_DMA_WRITE_REQ0
CDD_DMA_TRIG_XBAR_SPI0_DMA_WRITE_REQ1
CDD_DMA_TRIG_XBAR_SPI0_DMA_WRITE_REQ2
CDD_DMA_TRIG_XBAR_SPI0_DMA_WRITE_REQ3
CDD_DMA_TRIG_XBAR_SPI1_DMA_READ_REQ0
CDD_DMA_TRIG_XBAR_SPI1_DMA_READ_REQ1
CDD_DMA_TRIG_XBAR_SPI1_DMA_READ_REQ2
CDD_DMA_TRIG_XBAR_SPI1_DMA_READ_REQ3
CDD_DMA_TRIG_XBAR_SPI1_DMA_WRITE_REQ0
CDD_DMA_TRIG_XBAR_SPI1_DMA_WRITE_REQ1
CDD_DMA_TRIG_XBAR_SPI1_DMA_WRITE_REQ2
CDD_DMA_TRIG_XBAR_SPI1_DMA_WRITE_REQ3
CDD_DMA_TRIG_XBAR_SPI2_DMA_READ_REQ0
CDD_DMA_TRIG_XBAR_SPI2_DMA_READ_REQ1
CDD_DMA_TRIG_XBAR_SPI2_DMA_READ_REQ2
CDD_DMA_TRIG_XBAR_SPI2_DMA_READ_REQ3
CDD_DMA_TRIG_XBAR_SPI2_DMA_WRITE_REQ0
CDD_DMA_TRIG_XBAR_SPI2_DMA_WRITE_REQ1
CDD_DMA_TRIG_XBAR_SPI2_DMA_WRITE_REQ2
CDD_DMA_TRIG_XBAR_SPI2_DMA_WRITE_REQ3
CDD_DMA_TRIG_XBAR_SPI3_DMA_READ_REQ0
CDD_DMA_TRIG_XBAR_SPI3_DMA_READ_REQ1
CDD_DMA_TRIG_XBAR_SPI3_DMA_READ_REQ2
CDD_DMA_TRIG_XBAR_SPI3_DMA_READ_REQ3
CDD_DMA_TRIG_XBAR_SPI3_DMA_WRITE_REQ0
CDD_DMA_TRIG_XBAR_SPI3_DMA_WRITE_REQ1
CDD_DMA_TRIG_XBAR_SPI3_DMA_WRITE_REQ2
CDD_DMA_TRIG_XBAR_SPI3_DMA_WRITE_REQ3
CDD_DMA_TRIG_XBAR_SPI4_DMA_READ_REQ0
CDD_DMA_TRIG_XBAR_SPI4_DMA_READ_REQ1
CDD_DMA_TRIG_XBAR_SPI4_DMA_READ_REQ2
CDD_DMA_TRIG_XBAR_SPI4_DMA_READ_REQ3
CDD_DMA_TRIG_XBAR_SPI4_DMA_WRITE_REQ0
CDD_DMA_TRIG_XBAR_SPI4_DMA_WRITE_REQ1
CDD_DMA_TRIG_XBAR_SPI4_DMA_WRITE_REQ2
CDD_DMA_TRIG_XBAR_SPI4_DMA_WRITE_REQ3
CDD_DMA_TRIG_XBAR_RTI0_DMA_0
CDD_DMA_TRIG_XBAR_RTI0_DMA_1
CDD_DMA_TRIG_XBAR_RTI0_DMA_2
CDD_DMA_TRIG_XBAR_RTI0_DMA_3
CDD_DMA_TRIG_XBAR_RTI1_DMA_0
CDD_DMA_TRIG_XBAR_RTI1_DMA_1
CDD_DMA_TRIG_XBAR_RTI1_DMA_2
CDD_DMA_TRIG_XBAR_RTI1_DMA_3
CDD_DMA_TRIG_XBAR_RTI2_DMA_0
CDD_DMA_TRIG_XBAR_RTI2_DMA_1
CDD_DMA_TRIG_XBAR_RTI2_DMA_2
CDD_DMA_TRIG_XBAR_RTI2_DMA_3
CDD_DMA_TRIG_XBAR_RTI3_DMA_0
CDD_DMA_TRIG_XBAR_RTI3_DMA_1
CDD_DMA_TRIG_XBAR_RTI3_DMA_2
CDD_DMA_TRIG_XBAR_RTI3_DMA_3
CDD_DMA_TRIG_XBAR_MCANSS0_TX_DMA_0
CDD_DMA_TRIG_XBAR_MCANSS0_TX_DMA_1
CDD_DMA_TRIG_XBAR_MCANSS0_TX_DMA_2
CDD_DMA_TRIG_XBAR_MCANSS0_TX_DMA_3
CDD_DMA_TRIG_XBAR_MCANSS1_TX_DMA_0
CDD_DMA_TRIG_XBAR_MCANSS1_TX_DMA_1
CDD_DMA_TRIG_XBAR_MCANSS1_TX_DMA_2
CDD_DMA_TRIG_XBAR_MCANSS1_TX_DMA_3
CDD_DMA_TRIG_XBAR_MCANSS2_TX_DMA_0
CDD_DMA_TRIG_XBAR_MCANSS2_TX_DMA_1
CDD_DMA_TRIG_XBAR_MCANSS2_TX_DMA_2
CDD_DMA_TRIG_XBAR_MCANSS2_TX_DMA_3
CDD_DMA_TRIG_XBAR_MCANSS3_TX_DMA_0
CDD_DMA_TRIG_XBAR_MCANSS3_TX_DMA_1
CDD_DMA_TRIG_XBAR_MCANSS3_TX_DMA_2
CDD_DMA_TRIG_XBAR_MCANSS3_TX_DMA_3
CDD_DMA_TRIG_XBAR_USART0_DMA_0
CDD_DMA_TRIG_XBAR_USART0_DMA_1
CDD_DMA_TRIG_XBAR_USART1_DMA_0
CDD_DMA_TRIG_XBAR_USART1_DMA_1
CDD_DMA_TRIG_XBAR_USART2_DMA_0
CDD_DMA_TRIG_XBAR_USART2_DMA_1
CDD_DMA_TRIG_XBAR_USART3_DMA_0
CDD_DMA_TRIG_XBAR_USART3_DMA_1
CDD_DMA_TRIG_XBAR_USART4_DMA_0
CDD_DMA_TRIG_XBAR_USART4_DMA_1
CDD_DMA_TRIG_XBAR_USART5_DMA_0
CDD_DMA_TRIG_XBAR_USART5_DMA_1
CDD_DMA_TRIG_XBAR_MCRC_DMA_EVENT_0
CDD_DMA_TRIG_XBAR_MCRC_DMA_EVENT_1
CDD_DMA_TRIG_XBAR_MCRC_DMA_EVENT_2
CDD_DMA_TRIG_XBAR_MCRC_DMA_EVENT_3
CDD_DMA_TRIG_XBAR_QSPI_INTR
CDD_DMA_TRIG_XBAR_GPIO_INT_XBAR_OUT_0
CDD_DMA_TRIG_XBAR_GPIO_INT_XBAR_OUT_1
CDD_DMA_TRIG_XBAR_GPIO_INT_XBAR_OUT_2
CDD_DMA_TRIG_XBAR_GPIO_INT_XBAR_OUT_3
CDD_DMA_TRIG_XBAR_SOC_TIMESYNC_XBAR1_OUT_0
CDD_DMA_TRIG_XBAR_SOC_TIMESYNC_XBAR1_OUT_1
CDD_DMA_TRIG_XBAR_SOC_TIMESYNC_XBAR0_OUT_0
CDD_DMA_TRIG_XBAR_SOC_TIMESYNC_XBAR0_OUT_1
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_0
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_1
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_2
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_3
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_4
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_5
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_6
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_7
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_8
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_9
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_10
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_11
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_12
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_13
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_14
CDD_DMA_TRIG_XBAR_DMA_XBAR_OUT_15
CDD_DMA_TRIG_XBAR_MMC_DMA_RD
CDD_DMA_TRIG_XBAR_MMC_DMA_WR
CDD_DMA_TRIG_XBAR_DTHE_SHA_DMA_REQ0
CDD_DMA_TRIG_XBAR_DTHE_SHA_DMA_REQ1
CDD_DMA_TRIG_XBAR_DTHE_SHA_DMA_REQ2
CDD_DMA_TRIG_XBAR_DTHE_SHA_DMA_REQ3
CDD_DMA_TRIG_XBAR_DTHE_SHA_DMA_REQ4
CDD_DMA_TRIG_XBAR_DTHE_SHA_DMA_REQ5
CDD_DMA_TRIG_XBAR_DTHE_AES_DMA_REQ0
CDD_DMA_TRIG_XBAR_DTHE_AES_DMA_REQ1
CDD_DMA_TRIG_XBAR_DTHE_AES_DMA_REQ2
CDD_DMA_TRIG_XBAR_DTHE_AES_DMA_REQ3
CDD_DMA_TRIG_XBAR_DTHE_AES_DMA_REQ4
CDD_DMA_TRIG_XBAR_DTHE_AES_DMA_REQ5
CDD_DMA_TRIG_XBAR_DTHE_AES_DMA_REQ6
CDD_DMA_TRIG_XBAR_DTHE_AES_DMA_REQ7
CDD_DMA_TRIG_XBAR_MCANSS0_FE_0
CDD_DMA_TRIG_XBAR_MCANSS0_FE_1
CDD_DMA_TRIG_XBAR_MCANSS0_FE_2
CDD_DMA_TRIG_XBAR_MCANSS0_FE_3
CDD_DMA_TRIG_XBAR_MCANSS0_FE_4
CDD_DMA_TRIG_XBAR_MCANSS0_FE_5
CDD_DMA_TRIG_XBAR_MCANSS0_FE_6
CDD_DMA_TRIG_XBAR_MCANSS1_FE_0
CDD_DMA_TRIG_XBAR_MCANSS1_FE_1
CDD_DMA_TRIG_XBAR_MCANSS1_FE_2
CDD_DMA_TRIG_XBAR_MCANSS1_FE_3
CDD_DMA_TRIG_XBAR_MCANSS1_FE_4
CDD_DMA_TRIG_XBAR_MCANSS1_FE_5
CDD_DMA_TRIG_XBAR_MCANSS1_FE_6
CDD_DMA_TRIG_XBAR_MCANSS2_FE_0
CDD_DMA_TRIG_XBAR_MCANSS2_FE_1
CDD_DMA_TRIG_XBAR_MCANSS2_FE_2
CDD_DMA_TRIG_XBAR_MCANSS2_FE_3
CDD_DMA_TRIG_XBAR_MCANSS2_FE_4
CDD_DMA_TRIG_XBAR_MCANSS2_FE_5
CDD_DMA_TRIG_XBAR_MCANSS2_FE_6
CDD_DMA_TRIG_XBAR_MCANSS3_FE_0
CDD_DMA_TRIG_XBAR_MCANSS3_FE_1
CDD_DMA_TRIG_XBAR_MCANSS3_FE_2
CDD_DMA_TRIG_XBAR_MCANSS3_FE_3
CDD_DMA_TRIG_XBAR_MCANSS3_FE_4
CDD_DMA_TRIG_XBAR_MCANSS3_FE_5
CDD_DMA_TRIG_XBAR_MCANSS3_FE_6
CDD_DMA_TRIG_XBAR_GPMC_SDMAREQ

4.4.9.1.10.3. CddDmaDmaChannelXbar

Item

Name

CddDmaDmaChannelXbar

Description

DMA Channel Cross bar source.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_DMA_XBAR_DMA_TRIG_XBAR_0

Range

CDD_DMA_XBAR_DMA_TRIG_XBAR_0
CDD_DMA_XBAR_DMA_TRIG_XBAR_1
CDD_DMA_XBAR_DMA_TRIG_XBAR_2
CDD_DMA_XBAR_DMA_TRIG_XBAR_3
CDD_DMA_XBAR_DMA_TRIG_XBAR_4
CDD_DMA_XBAR_DMA_TRIG_XBAR_5
CDD_DMA_XBAR_DMA_TRIG_XBAR_6
CDD_DMA_XBAR_DMA_TRIG_XBAR_7
CDD_DMA_XBAR_DMA_TRIG_XBAR_8
CDD_DMA_XBAR_DMA_TRIG_XBAR_9
CDD_DMA_XBAR_DMA_TRIG_XBAR_10
CDD_DMA_XBAR_DMA_TRIG_XBAR_11
CDD_DMA_XBAR_DMA_TRIG_XBAR_12
CDD_DMA_XBAR_DMA_TRIG_XBAR_13
CDD_DMA_XBAR_DMA_TRIG_XBAR_14
CDD_DMA_XBAR_DMA_TRIG_XBAR_15

4.4.9.1.10.4. CddDmaDmaChannelXbarMap

Item

Name

CddDmaDmaChannelXbarMap

Description

DMA Channel Cross bar source.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CDD_DMA_XBAR_ADC0_INT1

Range

CDD_DMA_XBAR_EPWM0_SOCA
CDD_DMA_XBAR_EPWM1_SOCA
CDD_DMA_XBAR_EPWM2_SOCA
CDD_DMA_XBAR_EPWM3_SOCA
CDD_DMA_XBAR_EPWM4_SOCA
CDD_DMA_XBAR_EPWM5_SOCA
CDD_DMA_XBAR_EPWM6_SOCA
CDD_DMA_XBAR_EPWM7_SOCA
CDD_DMA_XBAR_EPWM8_SOCA
CDD_DMA_XBAR_EPWM9_SOCA
CDD_DMA_XBAR_EPWM10_SOCA
CDD_DMA_XBAR_EPWM11_SOCA
CDD_DMA_XBAR_EPWM12_SOCA
CDD_DMA_XBAR_EPWM13_SOCA
CDD_DMA_XBAR_EPWM14_SOCA
CDD_DMA_XBAR_EPWM15_SOCA
CDD_DMA_XBAR_EPWM16_SOCA
CDD_DMA_XBAR_EPWM17_SOCA
CDD_DMA_XBAR_EPWM18_SOCA
CDD_DMA_XBAR_EPWM19_SOCA
CDD_DMA_XBAR_EPWM20_SOCA
CDD_DMA_XBAR_EPWM21_SOCA
CDD_DMA_XBAR_EPWM22_SOCA
CDD_DMA_XBAR_EPWM23_SOCA
CDD_DMA_XBAR_EPWM24_SOCA
CDD_DMA_XBAR_EPWM25_SOCA
CDD_DMA_XBAR_EPWM26_SOCA
CDD_DMA_XBAR_EPWM27_SOCA
CDD_DMA_XBAR_EPWM28_SOCA
CDD_DMA_XBAR_EPWM29_SOCA
CDD_DMA_XBAR_EPWM30_SOCA
CDD_DMA_XBAR_EPWM31_SOCA
CDD_DMA_XBAR_EPWM0_SOCB
CDD_DMA_XBAR_EPWM1_SOCB
CDD_DMA_XBAR_EPWM2_SOCB
CDD_DMA_XBAR_EPWM3_SOCB
CDD_DMA_XBAR_EPWM4_SOCB
CDD_DMA_XBAR_EPWM5_SOCB
CDD_DMA_XBAR_EPWM6_SOCB
CDD_DMA_XBAR_EPWM7_SOCB
CDD_DMA_XBAR_EPWM8_SOCB
CDD_DMA_XBAR_EPWM9_SOCB
CDD_DMA_XBAR_EPWM10_SOCB
CDD_DMA_XBAR_EPWM11_SOCB
CDD_DMA_XBAR_EPWM12_SOCB
CDD_DMA_XBAR_EPWM13_SOCB
CDD_DMA_XBAR_EPWM14_SOCB
CDD_DMA_XBAR_EPWM15_SOCB
CDD_DMA_XBAR_EPWM16_SOCB
CDD_DMA_XBAR_EPWM17_SOCB
CDD_DMA_XBAR_EPWM18_SOCB
CDD_DMA_XBAR_EPWM19_SOCB
CDD_DMA_XBAR_EPWM20_SOCB
CDD_DMA_XBAR_EPWM21_SOCB
CDD_DMA_XBAR_EPWM22_SOCB
CDD_DMA_XBAR_EPWM23_SOCB
CDD_DMA_XBAR_EPWM24_SOCB
CDD_DMA_XBAR_EPWM25_SOCB
CDD_DMA_XBAR_EPWM26_SOCB
CDD_DMA_XBAR_EPWM27_SOCB
CDD_DMA_XBAR_EPWM28_SOCB
CDD_DMA_XBAR_EPWM29_SOCB
CDD_DMA_XBAR_EPWM30_SOCB
CDD_DMA_XBAR_EPWM31_SOCB
CDD_DMA_XBAR_ADC0_INT1
CDD_DMA_XBAR_ADC0_INT2
CDD_DMA_XBAR_ADC0_INT3
CDD_DMA_XBAR_ADC0_INT4
CDD_DMA_XBAR_ADC0_EVTINT
CDD_DMA_XBAR_ADC1_INT1
CDD_DMA_XBAR_ADC1_INT2
CDD_DMA_XBAR_ADC1_INT3
CDD_DMA_XBAR_ADC1_INT4
CDD_DMA_XBAR_ADC1_EVTINT
CDD_DMA_XBAR_ADC2_INT1
CDD_DMA_XBAR_ADC2_INT2
CDD_DMA_XBAR_ADC2_INT3
CDD_DMA_XBAR_ADC2_INT4
CDD_DMA_XBAR_ADC2_EVTINT
CDD_DMA_XBAR_ADC3_INT1
CDD_DMA_XBAR_ADC3_INT2
CDD_DMA_XBAR_ADC3_INT3
CDD_DMA_XBAR_ADC3_INT4
CDD_DMA_XBAR_ADC3_EVTINT
CDD_DMA_XBAR_ADC4_INT1
CDD_DMA_XBAR_ADC4_INT2
CDD_DMA_XBAR_ADC4_INT3
CDD_DMA_XBAR_ADC4_INT4
CDD_DMA_XBAR_ADC4_EVTINT
CDD_DMA_XBAR_FSI0_RX_DMA_EVT
CDD_DMA_XBAR_FSI0_DMA_TRIG1
CDD_DMA_XBAR_FSI0_DMA_TRIG2
CDD_DMA_XBAR_FSI1_RX_DMA_EVT
CDD_DMA_XBAR_FSI1_DMA_TRIG1
CDD_DMA_XBAR_FSI1_DMA_TRIG2
CDD_DMA_XBAR_FSI2_RX_DMA_EVT
CDD_DMA_XBAR_FSI2_DMA_TRIG1
CDD_DMA_XBAR_FSI2_DMA_TRIG2
CDD_DMA_XBAR_FSI3_RX_DMA_EVT
CDD_DMA_XBAR_FSI3_DMA_TRIG1
CDD_DMA_XBAR_FSI3_DMA_TRIG2
CDD_DMA_XBAR_FSI0_TX_DMA_EVT
CDD_DMA_XBAR_FSI1_TX_DMA_EVT
CDD_DMA_XBAR_FSI2_TX_DMA_EVT
CDD_DMA_XBAR_FSI3_TX_DMA_EVT
CDD_DMA_XBAR_SD0_FILT0_DRINT
CDD_DMA_XBAR_SD0_FILT1_DRINT
CDD_DMA_XBAR_SD0_FILT2_DRINT
CDD_DMA_XBAR_SD0_FILT3_DRINT
CDD_DMA_XBAR_SD1_FILT0_DRINT
CDD_DMA_XBAR_SD1_FILT1_DRINT
CDD_DMA_XBAR_SD1_FILT2_DRINT
CDD_DMA_XBAR_SD1_FILT3_DRINT
CDD_DMA_XBAR_ECAP0_DMA_INT
CDD_DMA_XBAR_ECAP1_DMA_INT
CDD_DMA_XBAR_ECAP2_DMA_INT
CDD_DMA_XBAR_ECAP3_DMA_INT
CDD_DMA_XBAR_ECAP4_DMA_INT
CDD_DMA_XBAR_ECAP5_DMA_INT
CDD_DMA_XBAR_ECAP6_DMA_INT
CDD_DMA_XBAR_ECAP7_DMA_INT
CDD_DMA_XBAR_ECAP8_DMA_INT
CDD_DMA_XBAR_ECAP9_DMA_INT

4.4.9.2. CddDmaGeneral

General configuration settings for the Complex Device Driver

4.4.9.2.1. CddDmaVersionInfoApi

Item

Name

CddDmaVersionInfoApi

Description

Switches the Cdd_Dma_GetVersionInfo function ON or OFF.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.4.9.2.2. CddDmaDeinitApi

Item

Name

CddDmaDeinitApi

Description

Switches the Cdd_Dma_DeInit function ON or OFF.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.4.9.2.3. CddDmaDevErrorDetect

Item

Name

CddDmaDevErrorDetect

Description

Switches the Development Error Detection and Notification ON or OFF.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.4.9.2.4. CddDmaRegisterReadBackApi

Item

Name

CddDmaRegisterReadBackApi

Description

Switches the Cdd_Dma_RegisterReadback function ON or OFF.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

4.4.10. Examples

4.4.10.1. Overview

Below 4 modes shall be verified using the examples

  • Chaining Mode

  • Interrupt Mode

  • Linking Mode

  • Polling Mode

  1. Initialize the Timer using AppUtils_TimerInit()

  2. Initialize the MCU for Clock configuration using Mcu_Init() and port using Port_Init()

  3. Initialize the interrupt using Cdd_Dma_InterruptConfig() (Not applicable for Polling mode)

  4. Start the timer using API start_timer()

  5. Get the DMA version using Cdd_Dma_GetVersionInfo()

  6. Initialize the DMA using Cdd_Dma_Init()

  7. Set the DMA parameters using Cdd_Dma_ParamSet()

  8. For Chaining Mode example,

    • Configure the Chaining Option

    • Link multiple DMA channels using Cdd_Dma_ChainChannel()

  9. For Linking Mode example, link the DMA channels using Cdd_Dma_LinkChannel()

  10. Register the callback function to be called once the transfer completed using Cdd_Dma_CbkRegister() (Not applicable for Polling Mode)

  11. Enable the transfer region of the DMA transfer using API Cdd_Dma_EnableTransferRegion()

  12. For Polling Mode example, status of the transfer is polled using API Cdd_Dma_GetStatus()

  13. Verify the transfer status

4.4.10.2. Hardware Software Setup and Tools

None

4.4.10.3. Steps to build and run example

  1. Cdd_Dma example applications demonstrates the MCAL CDD_DMA driver features, which is referred from folder <MCAL_ROOT>/examples/Dma.

  2. There are 4 example applications provided to verify all the features of the module.

  3. These applications can be built from the build folder by giving :

    “gmake –s dma_pollingmode_app PLATFORM=am263” for polling mode example

    “gmake –s dma_interruptmode_app PLATFORM=am263” for interrupt mode example

    “gmake –s dma_linkingmode_app PLATFORM=am263” for linking mode example

    “gmake –s dma_chainingmode_app PLATFORM=am263” for chaining mode example

    • In case of linking mode example multiple params are configured within the channel and once the execution gets completed with first paramSet then automatically second paramSet data will be loaded.

    • In case of chaining mode example multiple channels are chained together so in this case once the trigger for first channel happen for transmission it will internally trigger for second channel as well.So in this way with less number of trigger transmission happens.

  4. Once the build is completed we get a binary file,which is loaded in our controller and executed.

4.4.10.4. Example Logs


=================================
DmaInterruptModeApp: Sample Application - STARTS !!!
  
DMA_CHAININGMODE_APP: DMA MCAL Version Info
---------------------
DMA_CHAININGMODE_APP: Vendor ID: 44
DMA_CHAININGMODE_APP: Module ID: 255
DMA_CHAININGMODE_APP: SW Major Version: 10
DMA_CHAININGMODE_APP: SW Minor Version: 0
DMA_CHAININGMODE_APP: SW Patch Version: 0
 
DMA_CHAININGMODE_APP: Variant - Pre Compile being used !!!
                                                           
DMA_CHAININGMODE_APP: All tests have passed

===============================================
DmaInterruptModeApp: Sample Application - STARTS !!!
  
DMA_INTERRUPTMODE_APP: DMA MCAL Version Info
---------------------
DMA_INTERRUPTMODE_APP: Vendor ID: 44
DMA_INTERRUPTMODE_APP: Module ID: 255
DMA_INTERRUPTMODE_APP: SW Major Version: 10
DMA_INTERRUPTMODE_APP: SW Minor Version: 0
DMA_INTERRUPTMODE_APP: SW Patch Version: 0
 
DMA_INTERRUPTMODE_APP: Variant - Pre Compile being used !!!
                                                            
DMA_INTERRUPTMODE_APP: All tests have passed

========================================
DmaInterruptModeApp: Sample Application - STARTS !!!
  
DMA_LINKINGMODE_APP: DMA MCAL Version Info
---------------------
DMA_LINKINGMODE_APP: Vendor ID: 44
DMA_LINKINGMODE_APP: Module ID: 255
DMA_LINKINGMODE_APP: SW Major Version: 10
DMA_LINKINGMODE_APP: SW Minor Version: 0
DMA_LINKINGMODE_APP: SW Patch Version: 0
 
DMA_LINKINGMODE_APP: Variant - Pre Compile being used !!!
                                                          
DMA_LINKINGMODE_APP: All tests have passed

==============================================
DmaPollingModeApp: Sample Application - STARTS !!!
  
DMA_POLLINGMODE_APP: DMA MCAL Version Info
---------------------
DMA_POLLINGMODE_APP: Vendor ID: 44
DMA_POLLINGMODE_APP: Module ID: 255
DMA_POLLINGMODE_APP: SW Major Version: 10
DMA_POLLINGMODE_APP: SW Minor Version: 0
DMA_POLLINGMODE_APP: SW Patch Version: 0
 
DMA_POLLINGMODE_APP: Variant - Pre Compile being used !!!
                                                          
DMA_POLLINGMODE_APP: All tests have passed

=================================================

4.4.10.5. File Structure

📦AM263x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Dma
┃ ┃ ┃ ┣ 📂Dma_ChainingMode
┃ ┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📜DmaChainingModeApp.c : Contains DMA test example.
┃ ┃ ┃ ┃ ┣ 📜DmaChainingModeApp.h : Contains DMA test example header.
┃ ┃ ┃ ┃ ┣ 📜Makefile
┃ ┃ ┃ ┣ 📂Dma_InterruptMode
┃ ┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📜DmaInterruptModeApp.c : Contains DMA test example.
┃ ┃ ┃ ┃ ┣ 📜DmaInterruptModeApp.h : Contains DMA test example header.
┃ ┃ ┃ ┃ ┣ 📜Makefile
┃ ┃ ┃ ┣ 📂Dma_LinkingMode
┃ ┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📜DmaLinkingModeApp.c : Contains DMA test example.
┃ ┃ ┃ ┃ ┣ 📜DmaLinkingModeApp.h : Contains DMA test example header.
┃ ┃ ┃ ┃ ┣ 📜Makefile
┃ ┃ ┃ ┣ 📂Dma_PollingMode
┃ ┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📜DmaPollingModeApp.c : Contains DMA test example.
┃ ┃ ┃ ┃ ┣ 📜DmaPollingModeApp.h : Contains DMA test example header.
┃ ┃ ┃ ┃ ┣ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Dma_Demo_Cfg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am263
┃ ┃ ┃ ┃ ┃ ┣ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Dma_Cfg.h : Contains the Precompile switches, Symbolic names.
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Dma_Cfg.c : Contains all Pre-Compile Configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┣ 📜README.txt

4.4.11. FAQ’s

None

4.4.12. References

Technical Reference Manual