Features Supported
- APIs to log strings to the selected console
- APIs to assert if a expression evaluates to 0
- Before asserting, it will log the file and line number to console
- Ability to disable assert's and logging via a pre-processor define
- The following console options are supported
- Log to CCS IDE console via JTAG
- Log to UART terminal
- Log to shared memory, can be viewed via the CPU on which log reader is enabled
- Log to CPU local memory, can be viewed via ROV in CCS or when Linux is enabled via Linux kernel debugfs
- Ability to read logs from shared memory and output to selected console.
- SysCfg support for below,
- SysCfg can be used to select the log console
- When UART log is selected, SysCfg allows to select the UART instance and its properties (baud rate etc) to use.
- SysCfg option to enable shared memory reader task
- APIs to read line as string and/or format input in scanf style from UART console.
Features NOT Supported
- Log APIs should not be called from ISR context. When called in ISR the APIs have no effect.
Important Usage Guidelines
Shared memory logging
- The core on which the shared memory reader is enabled, the option to use shared memory writer is ignored.
- When shared memory writer/reader is enabled, a shared memory section is used to write and read the strings for all the cores,
- When SysCfg is used, the array representing this shared memory is generated in the file
ti_dpl_config.c
.
- Place the section attributed to this array in the linker command file for each core such that all cores point to the same memory address for this section.
- And this memory section should be marked as non-cache in the MPU/MMU entry for each core.
- It is recommended to enable UART logging and shared memory reader on one "main" core and other core's should enable the shared memory writer.
- The memory used for logging is limited per core. If the writer is faster than reader, then the writer drops the characters to be printed.
- To change the size of the log buffer, change the value of DebugP_SHM_LOG_SIZE in
source/kernel/dpl/DebugP.h
. - Note
- When shared memory reader is enabled for a nortos application user needs to invoke DebugP_shmLogRead API to read logs from shared memory. DebugP_shmLogRead will read the log once and exit thus application needs to call this API periodically in-order to gather continous logs.
UART logging
- Make sure the selected UART driver is opened for the logs to be output to UART.
- When enabled via SysCfg, calling the function
Drivers_open
opens and initializes the UART for logging.
Other guidelines
- Log and assert APIs should not be called from ISR context.
- The assert and logging APIs are task or thread safe, i.e they can be called from multiple tasks without the output getting mixed.
- The cores on which CCS or UART or shared memory writer is enabled can use either NORTOS or FreeRTOS.
Example Usage
Include the below file to access the APIs,
Example usage for assert,
Example usage for logs,
char *
str =
"Hello, world !!!";
Example usage for scanf,
uint32_t value32;
value32 = 0;
Example snippet to show linker command file placement of the shared memory log section generated via SysCfg,
SECTIONS
{
/* this is used when Debug log's to shared memory are enabled, else this is not used */
.bss.log_shared_mem (NOLOAD) : {} > LOG_SHM_MEM
}
MEMORY
{
/* shared memories that are used by all cores */
/* On M4F,
* - By default MSMC RAM is not accessible to M4F, a RAT entry is needed to make it
* accessible on M4F
* - So make sure there is a RAT entry which has a 1:1 mapping from 0x70000000 to 0x70200000
*/
/* On R5F,
* - make sure there is a MPU entry which maps below regions as non-cache
*/
LOG_SHM_MEM : ORIGIN = 0x701D4000, LENGTH = 0x00004000
}
API
APIs for Debug log's and assert's