Result of get SSC request.
| hdr | TISCI header |
| modfreq_hz | The current modulation frequency in Hz. |
| mod_depth | The current modulation depth in "permyriad". |
| spread_type | The current spread type. |
| enable | The current enable state. |
Data Fields | |
| struct tisci_header | hdr |
| uint32_t | modfreq_hz |
| uint32_t | mod_depth |
| uint8_t | spread_type |
| uint8_t | enable |
| struct tisci_header tisci_msg_get_clock_ssc_resp::hdr |
| uint32_t tisci_msg_get_clock_ssc_resp::modfreq_hz |
| uint32_t tisci_msg_get_clock_ssc_resp::mod_depth |
| uint8_t tisci_msg_get_clock_ssc_resp::spread_type |
| uint8_t tisci_msg_get_clock_ssc_resp::enable |