AM64x MCU+ SDK  12.01.00
PRU-ICSSG for Ethernet Networking

Mode of Operation

ICSSG can be configured to operate in two modes, Dual-MAC and Switch.

It is important to differentiate between these two modes. Dual-MAC mode implements two independent Ethernet MACs using ICSSG Slice 0/1, they have two different MAC, IP addresses and two different instances of the TCP/IP stack, while a Switch presents a single IP and MAC address for any external entity.

ICSSG Switch and Dual-MAC architecture

The ICSSG architecture consists of two logical slices to implement the switch functionalities. PRU0 (RX PRU0), TX_PRU0 and RTU_PRU0 is considered as Slice0 and the other cores PRU1 (RX PRU1), TX_PRU1 and RTU_PRU1 form the Slice1.
In Switch mode, each slice handles cross-port transmission: receiving on one port and transmitting on the opposite port. In contrast, in Dual-MAC mode, each slice operates independently, handling both receiving and transmitting on the same port.
This has been achieved by accordingly configuring the TX_MUX_SELn field of MII_RT_TXCFGn memory-mapped register (n= 0,1). For more details, refer TRM section 6.4.14.11 PRU_MII_RT_MII_RT Registers.

Bit-field Switch Dual-MAC
TX_MUX_SEL0 1h 0h
TX_MUX_SEL1 0h 1h

Figure1: ICSSG Architecture in Switch Mode

Figure2: ICSSG Architecture in Dual-MAC Mode

ICSSG Packet flow paths

There are 3 basic packet flow paths:

  • Host Egress: Packets are received from Port1/2 by RX_PRU and sent to the Host.
  • Forwarding: Packets are forwarded or switched from Port1 to Port2 using Slice0 (RX_PRU0 and TX_PRU0). Packets are forwarded from Port2 to Port1 using Slice1 (RX_PRU1 and TX_PRU1).
  • Local Injection: Packets are sent from Host to Ports 1/2 via the RTU_PRU and TX_PRU.

Figure3: ICSSG packet flow paths

Memory usage by ICSSG Queues

The ICSSG Queues used for packet content buffering are elaborated here

File : {Any of ENET ICSSG examples} CCS Project > Generated Source > SysConfig > ti_enet_soc.c

Switch mode

Buffer are allocated for each of the packet flow paths

Memory Pool Purpose Default size of each Queue in Pool Number of Queues Default Total pool size
gEnetSoc_icssg1PortPoolMem_0 Forwarding path buffer used for the purpose of Forwarding of Frames from Port 1 to Port 2 6KB Default: 8
(Max: 8 to support 8 QoS)
48KB
gEnetSoc_icssg1PortPoolMem_1 Forwarding path buffer used for the purpose of Forwarding of Frames from Port 2 to Port 1 6KB Default: 8
(Max: 8 to support 8 QoS)
48KB
gEnetSoc_icssg1HostPoolMem_0 Local Injection path buffer used for the purpose of transmitting frames from the host to Port A or/and Port B via ICSSG Slice 0. 6KB when Gigabit support is enabled
3KB when Gigabit support is disabled
Calculated as: n = 2 * QoS Level
(Factor 2 accounts for the Own-port Host pool and Opposite-port Host pool)

Default Configuration: QoS level is 3 by default in SysCfg, hence there are 2 * 3 = 6 queues
36KB when Gigabit support is enabled
18KB when Gigabit support is disabled
gEnetSoc_icssg1HostPoolMem_1 Local Injection path buffer used for the purpose of transmitting frames from the host to Port A or/and Port B via ICSSG Slice 1. 6KB when Gigabit support is enabled
3KB when Gigabit support is disabled
Calculated as: n = 2 * QoS Level
(Factor 2 accounts for the Own-port Host pool and Opposite-port Host pool)

Default Configuration: QoS level is 3 by default in SysCfg, hence there are 2 * 3 = 6 queues
36KB when Gigabit support is enabled
18KB when Gigabit support is disabled
gEnetSoc_icssg1HostQueueMem_0 Host Egress path buffer used for the purpose of reception of frames from the Port A to the host. 8KB when Gigabit support is enabled
5KB when Gigabit support is disabled
Default: 2 16KB when Gigabit support is enabled
10KB when Gigabit support is disabled
gEnetSoc_icssg1HostQueueMem_1 Host Egress path buffer used for the purpose of reception of frames from the Port B to the host. 8KB when Gigabit support is enabled
5KB when Gigabit support is disabled
Default: 2 16KB when Gigabit support is enabled
10KB when Gigabit support is disabled

Dual-MAC mode

Buffers are allocated for the Host egress and Local injection paths. However, no buffers are allocated for forwarding path since Dual-MAC mode by definition does not have the feature of forwarding.

Memory Pool Purpose Default size of each Queue in Pool Number of Queues Default Total pool size
gEnetSoc_icssg1PortPoolMem_0 Forwarding path buffer used for the purpose of Forwarding of Frames from Port 1 to Port 2 0KB 0 0KB
gEnetSoc_icssg1PortPoolMem_1 Forwarding path buffer used for the purpose of Forwarding of Frames from Port 2 to Port 1 0KB 0 0KB
gEnetSoc_icssg1HostPoolMem_0 Local Injection path buffer used for the purpose of transmitting frames from the host to Port A or/and Port B via ICSSG Slice 0. 8KB when Gigabit support is enabled
4KB when Gigabit support is disabled
n = QoS Level
Default: QoS level is 3 by default in SysCfg
24KB when Gigabit support is enabled
12KB when Gigabit support is disabled
gEnetSoc_icssg1HostPoolMem_1 Local Injection path buffer used for the purpose of transmitting frames from the host to Port A or/and Port B via ICSSG Slice 1. 8KB when Gigabit support is enabled
4KB when Gigabit support is disabled
n = QoS Level
Default: QoS level is 3 by default in SysCfg
24KB when Gigabit support is enabled
12KB when Gigabit support is disabled
gEnetSoc_icssg1HostQueueMem_0 Host Egress path buffer used for the purpose of reception of frames from the Port A to the host. 8KB when Gigabit support is enabled
5KB when Gigabit support is disabled
Default: 2 16KB when Gigabit support is enabled
10KB when Gigabit support is disabled
gEnetSoc_icssg1HostQueueMem_1 Host Egress path buffer used for the purpose of reception of frames from the Port B to the host. 8KB when Gigabit support is enabled
5KB when Gigabit support is disabled
Default: 2 16KB when Gigabit support is enabled
10KB when Gigabit support is disabled

Modify Port Pool memory usage

Port pool memory usage can be modified by varying the:

A. Size per queue and/or

  • Go to file: {MCU_SDK_install_path}\source\networking\enet\core\sysconfig\networking\.meta\enet_icss\templates\enet_soc_cfg_am64x_am243x.c.xdt
  • Modify the define ICSSG_SWITCH_PORT_POOL_SIZE to configure the required queue size.
  • Save the file.
  • Build the application.
  • Now, you can see the sizes getting reflected in the generated file: ti_enet_soc.c (memory allocated can also be verified in the .map file under the .icss_mem output section)

B. Number of Queues initialized

  • ICSSG_SWITCH_PORT_BUFFER_POOL_NUM: The number of ICSSG Port buffer pools is by default defined as 8 (max) to provide a unique Pool for upto 8 QoS levels.
  • This number can be reduced as per the requirement of the user application, for example 'n' (n = 1 to 8).
  • However, care must be taken to ensure all priorities (PCPs) are mapped to only those 0 to n-1 Queues.
  • This can be done by using the IOCTL ENET_MACPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP

Steps:

  • Go to file: {MCU_SDK_install_path}\source\networking\enet\core\include\per\icssg.h
    • Change the ICSSG_SWITCH_PORT_BUFFER_POOL_NUM to any value from 1 to 8.
    • Save the file.
  • Rebuild the library.
    • Run this command: gmake -s -j8 -f makefile.am243x enet-icssg_r5f.ti-arm-clang here {MCU_SDK_install_path}
  • With respect to the the Enet ICSSG Layer 2 example {MCU_SDK_install_path}\source\networking\enet\core\examples\enet_layer2_icssg\
    • EnetMp_rxTask() → Modify the prioMap[] array which is passed as argument to set_priority_queue_mapping()

Example

  • If setting ICSSG_SWITCH_PORT_BUFFER_POOL_NUM = 3, Then the available pools will only be 0 ,1, 2.
  • Hence, all the traffic must be directed to only these queues 0 to 2 by using the above IOCTL. Type of mapping is left to the user.

The Input Argument of the IOCTL ENET_MACPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP can be set based on below: uint32_t EnetPort_PriorityMap::priorityMap[ENET_PRI_NUM] : The array index corresponds to the PCP and the value holds the mapped Q value

PCP(Index) Queue Number = priorityMap[pcp]
0 0
1 0
2 0
3 1
4 1
5 2
6 2
7 2

Sample IOCTL usage: ENET_MACPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP

/* Mapping the PCP to Queue*/
EnetMacPort_SetEgressPriorityMapInArgs SetEgressPriorityMapInArgs;
EnetPort_PriorityMap PriorityMap;
PriorityMap.priorityMap[0] = 0;
PriorityMap.priorityMap[1] = 0;
PriorityMap.priorityMap[2] = 0;
PriorityMap.priorityMap[3] = 1;
PriorityMap.priorityMap[4] = 1;
PriorityMap.priorityMap[5] = 2;
PriorityMap.priorityMap[6] = 2;
PriorityMap.priorityMap[7] = 2;
SetEgressPriorityMapInArgs.macPort = macPortList[i];
SetEgressPriorityMapInArgs.priorityMap = PriorityMap;
ENET_IOCTL_SET_IN_ARGS(&prms, &SetEgressPriorityMapInArgs);
if (status != ENET_SOK)
{
EnetAppUtils_print("EnetApp_enablePorts() failed to set PCP to Q map: %d\r\n", status);
}

Modify Host Pool memory usage

Host pool memory usage can be modified by varying the:

A. Size per Queue (and/or)

  • Go to file: {MCU_SDK_install_path}\source\networking\enet\core\sysconfig\networking\.meta\enet_icss\templates\enet_soc_cfg_am64x_am243x.c.xdt
  • Modify the define ICSSG_SWITCH_HOST_POOL_SIZE to configure the required queue size.
  • Save the file.
  • Build the application.
  • Now you can see the sizes getting reflected in the generated file: ti_enet_soc.c.
  • Memory allocated can also be verified in the .map file under the .icss_mem output section.

B. Number of Queues initialized

  • ICSSG_SWITCH_HOST_BUFFER_POOL_NUM_CFG: The number of ICSSG Host buffer pools is by default defined as (2 * QoS Level). By default, QoS Level=3 hence number of queue in the pool is 6.

To modify the number of pools:

  • Go to file: {MCU_SDK_install_path}\source\networking\enet\core\sysconfig\networking\.meta\enet_icss\enet_icss.syscfg
  • Modify the QoS Level parameter to your desired value.
  • Build the application.
  • Now, you can see the sizes getting reflected in the generated file: ti_enet_soc.c. (Memory allocated can also be verified in the .map file under the .icss_mem output section)

Locally inject different Traffic classes

According to IEEE 802.1D, there can be different traffic types like best effort, excellent effort generated by different user application. Some of these traffic might be latency sensitive for ex: PTP network control traffic. Traffic-class to transmit queue mapping feature determines the transmit queue for transmitting data streams based on traffic class configured by the user application. Port queues supports maximum of 8 queues (per port) to treat the traffic at QoS level. For ex: best effort data can be segregated from all the time-critical traffic. Port queues are serviced from highest (7) to lowest priority (0), so highest txPktTc variable number (between 0-7) shall be serviced first. There are a total of 8 QoS Levels and each QoS Level has a dedicated Queue. Also, multiple traffic types can be combined to single queue. Refer IEEE 802.1D for more details.

  • When the user wants to send out packets from the Host to either ports via the ICSSG, it can be sent via different one of the 8 Host Pool queues (gEnetSoc_icssg1HostPoolMem_0/1).
    • This can be achieved by using the txPktInfo->txPktTc parameter.
    • Refer to enet_layer2_icssg.c.
    • txPktTc can range from 0 to 7 corresponding to the 8 levels of QoS.
Note
txPktTc passed should be less than the "QoS Level" set in SysCfg by the user. If not, the packets will be sent to a queue which has not been initialized itself, resulting in stall due to no buffer.
EnetPort_PriorityMap
Priority map.
Definition: enet_mod_port.h:132
EnetMacPort_SetEgressPriorityMapInArgs::priorityMap
EnetPort_PriorityMap priorityMap
Definition: enet_mod_macport.h:521
EnetPort_PriorityMap::priorityMap
uint32_t priorityMap[ENET_PRI_NUM]
Definition: enet_mod_port.h:135
ENET_IOCTL_SET_IN_ARGS
#define ENET_IOCTL_SET_IN_ARGS(prms, in)
Set the input args for an IOCTL command.
Definition: enet_ioctl.h:122
ENET_MACPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP
@ ENET_MACPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP
Set QoS egress priority map.
Definition: enet_mod_macport.h:155
ENET_IOCTL
#define ENET_IOCTL(hEnet, coreId, ioctlCmd, prms, status)
Helper macro used to first register IOCTL handler and then invoke the IOCTL.
Definition: enet_ioctl.h:188
EnetMacPort_SetEgressPriorityMapInArgs::macPort
Enet_MacPort macPort
Definition: enet_mod_macport.h:518
ENET_SOK
#define ENET_SOK
Success.
Definition: enet_types.h:76
EnetMacPort_SetEgressPriorityMapInArgs
Input args for ENET_MACPORT_IOCTL_SET_EGRESS_QOS_PRI_MAP command.
Definition: enet_mod_macport.h:516