AM64x MCU+ SDK  12.01.00
SDL MCU ESM

Introduction

This example demonstrates High and Low priority events received from the MCU_ESM through the application-registered callback. It also shows routing and clearing of events to the MCU_SAFETY_ERRORn pin.

This example displays setting up ESM to

* Enable/Disable input events to the ESM module for each ESM instance
* Registration of application callback for ESM error events for each ESM instance
* Designating input events as high priority or low priority for each ESM instance
* Designating direct pin routing to MCU_SAFETY_ERRORn pin for external monitor communication

Use Cases

Use Case Description
UC-0 Configuration of High Priority ESM
UC-1 Configuration of Config Priority ESM
UC-2 Configuration of Low Priority ESM

Supported Combinations

Parameter Value
CPU + OS m4fss0-0 nortos
r5ss0-0 nortos
Toolchain ti-arm-clang
Board am64x-evm
Example folder examples/sdl/mcu_esm0/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

ESM Example Application
TIMER_ESM_init: Init MCU ESM complete
ESM example init complete
Any clear of MCU_SAFETY_ERRORn pin will first wait 10 usecs
Minimum Time Interval is 2000 usecs
ESM timer initialization complete
Starting Test Case 0
Use Case 0 completed: Input Event Trigger = Step completed successfully,
Event Handler Complete = Step completed successfully,
MCU_SAFETY_ERRORn Pin Clear = Step completed successfully
Starting Test Case 1
Use Case 1 completed: Input Event Trigger = Step completed successfully,
Event Handler Complete = Step completed successfully,
MCU_SAFETY_ERRORn Pin Clear = Step completed successfully
Starting Test Case 2
Use Case 2 completed: Input Event Trigger = Step completed successfully,
Event Handler Complete = Step completed successfully,
MCU_SAFETY_ERRORn Pin Clear = Step completed successfully
ESM Example Application summary
-------------------------------
Completed 3 Test Cases
Received 1 High Priority Interrupts
Received 1 Low Priority Interrupts
Received 1 Config Priority Interrupts
Test Case Event Log
------------------
Test Case 0: ESM Call back function called : grpChannel 0x2, index 0x1, intSrc 0x41
ESM instance #1, ESM interrupt type = High Priority ESM event
Test Case 1: ESM Call back function called : grpChannel 0x1, index 0x0, intSrc 0x0
ESM instance #1, ESM interrupt type = Config ESM event
Test Case 2: ESM Call back function called : grpChannel 0x1, index 0x3, intSrc 0x23
ESM instance #1, ESM interrupt type = Low Priority ESM event
ESM Example Application: Complete
All tests have passed!!