AM64x MCU+ SDK  12.01.00
SDL ECC SEC

Introduction

This example takes an aggregator index as input from the user and performs single bit error test for the corresponding aggregator. It involves the following steps:

  • Setup of an ESM application callback to receive Single Error Correction (SEC) and setup of ECC Aggregators in general
  • Triggering of ECC events for all the RAM IDs, including Interconnect type and Wrapper type
  • Printing out error information within the ECC callback upon reception of ECC events

Aggregators Supported

The following aggregators can be tested using this example.

Aggregator Index ECC Aggregator
0 SDL_PSRAMECC0_PSRAM256X32E_ECC_AGGR
1 SDL_MMCSD1_EMMCSD4SS_ECC_AGGR_RXMEM
2 SDL_ADC0_ADC12_CORE_FIFO_RAM_ECC_AGGR
3 SDL_ECC_AGGR1
4 SDL_ECC_AGGR0
5 SDL_SA2_UL0_SA2_UL_SA2_UL_ECC_AGGR
6 SDL_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR
7 SDL_DMASS0_DMSS_AM64_ECCAGGR
8 SDL_MMCSD1_EMMCSD4SS_ECC_AGGR_TXMEM
9 SDL_MCAN1_MCANSS_MSGMEM_WRAP_ECC_AGGR
10 SDL_PRU_ICSSG1_ICSS_G_16FF_CORE_BORG_ECC_AGGR
11 SDL_PRU_ICSSG0_ICSS_G_16FF_CORE_BORG_ECC_AGGR
12 SDL_MSRAM_256K2_MSRAM32KX64E_ECC_AGGR
13 SDL_FSS0_FSS_UL_OSPI0_OSPI_WRAP_ECC_AGGR
14 SDL_CPSW0_CPSW_3GUSS_CORE_ECC_CPSW_ECC_AGGR
15 SDL_GICSS0_GIC500SS_1_2_ECC_AGGR
16 SDL_PCIE0_PCIE_G2X1_64_CORE_AXI_ECC_AGGR
17 SDL_PCIE0_PCIE_G2X1_64_CORE_CORE_ECC_AGGR
18 SDL_USB0_USB3P0SS64_16FFC_USB3P0SS64_CORE_A__ECC_AGGR
19 SDL_PDMA1_PDMA_AM64_MAIN1_ECCAGGR
20 SDL_DMSC0_DMSC_LITE
21 SDL_MSRAM_256K1_MSRAM32KX64E_ECC_AGGR
22 SDL_MSRAM_256K0_MSRAM32KX64E_ECC_AGGR
23 SDL_MSRAM_256K3_MSRAM32KX64E_ECC_AGGR
24 SDL_MSRAM_256K5_MSRAM32KX64E_ECC_AGGR
25 SDL_MSRAM_256K4_MSRAM32KX64E_ECC_AGGR
26 SDL_MSRAM_256K7_MSRAM32KX64E_ECC_AGGR
27 SDL_MSRAM_256K6_MSRAM32KX64E_ECC_AGGR
28 SDL_MCU_M4FSS0_BLAZAR_ECC
29 SDL_PDMA0_PDMA_AM64_MAIN0_ECCAGGR
30 SDL_MMCSD0_EMMC8SS_16FFC_ECC_AGGR_RXMEM
31 SDL_MMCSD0_EMMC8SS_16FFC_ECC_AGGR_TXMEM
32 SDL_VTM0_K3VTM_N16FFC_ECCAGGR
33 SDL_R5FSS1_PULSAR_LITE_CPU0_ECC_AGGR
34 SDL_R5FSS1_PULSAR_LITE_CPU1_ECC_AGGR
35 SDL_R5FSS0_PULSAR_LITE_CPU0_ECC_AGGR
36 SDL_R5FSS0_PULSAR_LITE_CPU1_ECC_AGGR
37 SDL_COMPUTE_CLUSTER0_SAM64_A53_256KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE0
38 SDL_COMPUTE_CLUSTER0_SAM64_A53_256KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_COREPAC
39 SDL_COMPUTE_CLUSTER0_SAM64_A53_256KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE1

Supported Combinations

Parameter Value
CPU + OS m4fss0-0 nortos
r5fss0-0 nortos
Toolchain ti-arm-clang
Board am64x-evm
Example folder examples/sdl/ecc_sec/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run for a couple of aggregators,

[MAIN_Cortex_R5_0_0]
ECC_Test_init: Exception init complete
ECC_Test_init: Init MCU ESM complete
ECC_Test_init: Init MAIN ESM complete
ECC_Test_init: ECC Callback Init complete for MCU ESM
ECC_Test_init: ECC Callback Init complete for Main ESM
ECC SDL API tests: starting
Refer the User Guide for the aggregator information
Select the memory to test...2
...selected 2
PSC Domain STATE Result = 1PSC MOdule STATE Result = 3
ecc_aggrtest: [2] single bit error self test: SDL_ADC0_ADC12_CORE_FIFO_RAM_ECC_AGGR starting
ECC_Memory_init: [2] SDL_ADC0_ADC12_CORE_FIFO_RAM_ECC_AGGR ECC Init complete
self test started not accessable RamId 0 starting
Got it
self test started not accessable RamId 1 starting
Got it
Select the memory to test...6
...selected 6
PSC Domain STATE Result = 1PSC MOdule STATE Result = 3
ecc_aggrtest: [6] single bit error self test: SDL_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR starting
ECC_Memory_init: [6] SDL_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR ECC Init complete
self test started accessable RamId 0 starting
self test started RamId 1 starting
Select the memory to test...