AM64x MCU+ SDK  09.02.00
UDMA Memcpy Polling

Introduction

This example performs UDMA block copy transfer using Type 15 Transfer Record (TR15) using Transfer Record Packet Descriptor (TRPD) in polling mode.

The application opens and configures a BCDMA channel using SysConfig. Then the application prepares a TRPD for a 1D transfer from source to destination buffer, submits the request to DMA, waits for the DMA to complete by polling the channels's completion ring accelerator (RA).

Once the transfer it completes, it does cache operation for data coherency and compares the source and destination buffers for any data mismatch.

Supported Combinations

Attention
A53 NORTOS, A53 FREERTOS and A53 FREERTOS SMP support is experimental and is NOT supported by TI.
Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
a53ss0-0 nortos
a53ss0-0 freertos
a53ss0-0 freertos-smp
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am64x-evm, am64x-sk
Example folder examples/drivers/udma/udma_memcpy_polling

Steps to Run the Example

See Also

UDMA

Sample Output

Shown below is a sample output when the application is run,

[UDMA] Memcpy application started ...
All tests have passed!!