AM64x MCU+ SDK  11.02.00
MMCSD RAW IO

Introduction

This example demonstrates basic read write to the eMMC/SD Card. The MMC instance and the media connected to it are selectable via Sysconfig.

The example writes known data to a particular offset in the media and then reads it back. The read back data is then compared with the written known data.

When both the comparisons match, test result is passed otherwise failed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
a53ss0-0 freertos
r5fss0-0 freertos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am64x-evm, am64x-sk
Example folder examples/drivers/mmcsd/mmcsd_raw_io

Steps to Run the Example

See Also

MMCSD

Sample Output

[MMCSD RAW IO] Starting...
All tests have passed!!