AM64x MCU+ SDK  12.01.00
Enet CLI

Introduction

The Enet CLI library provides a command line interpreter for networking applications.

Features

  • APIs to easily enable CLI in any networking application.
  • Built-in commands which can aid in debugging.
  • API to create custom commands in application.
  • Portable to any command interpreter library. (Currently uses FreeRTOS_Plus_CLI.)

List of Built-In Commands

Module Command Description
enet_cfg enet_cfg mqprio <port_num> [{-i❘-e} <map0> ... <map7>] Modifies priority remap registers on the CPSW. Use -i tag to modify VLAN priority regeneration map. Use -e to modify QoS egress priority map. Specifying only the port will show the current remap register values of the port.
enet_cfg tracelvl [<lvl>] Sets the trace level for enet processes to lvl. Refer to this for more information on trace levels. Prints current trace level if lvl is not specified
enet_cfg classifier [-r] [-c <rx_chn>] [-e <ether_type>] [-p <mac_port>] [-sm <src_mac_addr>] [-dm <dest_mac_addr>] [-sip <src_ipv4_addr>] [-dip <dest_ipv4_addr>] [-iv <inner_vid>] [-ov <outer_vid>] [-pcp <priority>] Configures a classifier with the specified rules. Use the -r tag to remove the classifer with the specified rules. Specifying rx_chn along with -r tag will remove all classifiers associated to the specified Rx channel.
enet_cfg help Prints a list of all commands available in the enet_cfg module.
enet_dbg enet_dbg cpswstats <port_num> [-r] Prints the CPSW statistics data of the specified port. Use the -r tag to reset the data after its printed.
enet_dbg dumpale Prints the ALE table. (Works only in debug mode.)
enet_dbg dumppolicer Prints the policer table.
enet_dbg help Prints a list of all commands available in the enet_dbg module.
phy phy_scan Prints a list of available PHYs.
phy status [<mac_port>] Prints the link status of the PHY at the specified MAC port. Prints the link status of all PHYs, if mac_port is not specified.
phy dump <mac_port> Prints the data of PHY registers at the specified MAC port.
phy write <mac_port> <addr> <data> Writes the data to the PHY register with address addr attached to the specified MAC port.
phy read <mac_port> <addr> Prints the data stored in the PHY register with address addr attached to the specified MAC port.
phy help Prints a list of all commands available in the phy module.
utils utils cpuload Prints current CPU usage.
utils readmem <start_addr> [<num_of_words>] Prints value stored in memory starting from start_addr. Prints only one word if num_of_words is not specified.
utils writemem <start_addr> <word1> ... Writes to memory starting from start_addr.
utils help Prints a list of all commands available in the utils module.

Demo and Examples

Enet CLI Example

Usage Guide

  • To use the built-in commands, the enet_cli library uses certain data (like enet handle, core ID, and so on) that needs to be initialized first using EnetCli_init().
  • Enable the built-in commands using the EnetCli_registerBuiltInCommands() function.
  • To process a command, use the EnetCli_processCommand() function. A command can return more than one line of output and the function might be required to run several times to get the full output. A sample code snippet to handle this case:
    ...
    bool moreDataToFollow;
    ...
    /* Continuously take commands from the user */
    while (1)
    {
    DebugP_scanf(rxBuffer, MAX_READ_BUFFER_LEN);
    /* Repeatedly call the process function until function returns false.
    The function will return false once no more output data is remaining.*/
    do
    {
    moreDataToFollow = EnetCli_processCommand(rxBuffer, txBuffer,
    MAX_WRITE_BUFFER_LEN);
    DebugP_log(txBuffer);
    memset(txBuffer, 0x00, MAX_WRITE_BUFFER_LEN);
    } while (moreDataToFollow);
    memset(rxBuffer, 0x00, MAX_READ_BUFFER_LEN);
    }
    ...

Adding Custom Commands

Depending on the command interpreter used, the procedure to add custom commands will vary.

FreeRTOS_Plus_CLI

  • Define the functions that will be executed when the custom commands are used. Refer to the FreeRTOS+CLI documentation for more information.
  • Define an array of commands. The array should be of the type CLI_Command_Definition_t. For more information on defining commands refer to the FreeRTOS+CLI documentation.
  • Use the EnetCli_registerCustomCommands() function to register the commands to the command interpreter.
  • The custom commands will automatically be processed when using the EnetCli_processCommand() function.