AM64x MCU+ SDK  11.00.00
Datasheet

Introduction

This datasheet provides the performance numbers of various device drivers in MCU PLUS SDK for AM64X

Generic Setup details

SOC Details Values
Core R5F
Core Operating Speed 800 MHz
Cache Status Enabled
Optimization Details Values
Build Profile Release
R5F Compiler flags -mcpu=cortex-r5 -mfloat-abi=hard -mfpu=vfpv3-d16 -Wall -Werror -g -mthumb -Wno-gnu-variable-sized-type-not-at-end -Wno-unused-function
R5F Linker flags -Wl,–diag_suppress=10063 -Wl,–ram_model -Wl,–reread_libs
Code Placement MSRAM
Data Placement MSRAM

Performance Numbers

SBL OSPI performance

AM64X-EVM

  • Software/Application used : sbl_ospi and ipc_notify_echo
  • Size of sbl_ospi appimage : 325 KB
  • Size of ipc_notify_echo appimage : 185 KB
  • Cores present in the appimage : m4f0-0, r5f0-0, r5f0-1, r5f1-0, r5f1-1, a530-0
  • Boot Media Clock : 166.667 MHz (Octal DDR mode)
Boot time breakdown Time (ms)
ROM : init + SBL load from flash 12.00
SBL : SYSFW Load 11.11
SBL : System Init 14.65
SBL : Drivers_open 1.638
SBL : Board_driversOpen 126.34
SBL : Sciclient Get Version 9.84
SBL : CPU Load 34.25
SBL : Total time taken 194.186
  • The time taken for Board_driversOpen (around 20 ms) is mostly for the PHY tuning of OSPI. If this needs to be further reduced, one can pre-train the PHY, note down delay values and set it directly instead of the tuning procedure.
  • Most of the time taken for the CPU load is in loading the M4F. Other CPUs take ~1.5ms each. This needs more investigation. Possible reason is the M4F IRAM and DRAM initialization time.
  • Here the CPU load or section copy takes place from the OSPI memory to the respective memory directly, this would be slower that mem to mem copy.
  • The time taken for Sciclient Get Version can be avoided if the version check is disabled

SBL SD performance

  • Software/Application used : sbl_sd and adc_singleshot
  • Size of sbl_sd appimage : 339 KB
  • Size of adc_singleshot appimage : 54 KB
  • Cores present in the appimage : r5f0-0
  • SD card read speed : 12.5 MBps mode
Boot time breakdown Time (ms)
ROM : init + SBL load from flash 12.00
SBL : SYSFW Load 11.10
SBL : System Init 14.234
SBL : Drivers_open 76.724
SBL : Board_driversOpen 0.00
SBL : Sciclient Get Version 9.844
SBL : File read from SD Card 5.580
SBL : CPU Load 12.857
-------------------------------------— -----------—
SBL : Total time taken 130.351
  • The MMCSD driver and SD card initialization is done as part of Drivers_open, so Board_driversOpen happens instantaneously.
  • Most of the time taken for the CPU load is in loading the M4F. Other CPUs take ~1.5ms each. This needs more investigation. Possible reason is the M4F IRAM and DRAM initialization time.
  • The CPU load is faster in this case because SD bootloader is at its core a memory bootloader. Appimage file from SD card is read into the memory (this takes 15 ms in this case). The CPU load now is mostly memcpy in the OCRAM. This would be quite fast. The only caveat here is that the buffer size to receive appimage is allocated in OCRAM, so it's limited. This is not the case in OSPI.
  • The time taken for Sciclient Get Version can be avoided if the version check is disabled

XIP Benchmark

  • Software/Application used : xip_benchmark
  • FIR operation
Caching status Cycles taken
Code/Data fully cached 26741
Code/Data not cached 159419
Code/Data not cached 1 of 10 iterations 40258
  • MEMCPY operation
Caching status Cycles taken
Code/Data fully cached 1565
Code/Data not cached 17916
Code/Data not cached 1 of 10 iterations 3204

MCAN performance

  • Internal loopback mode of operation
  • Memory Mode : TX Buffer Mode, RX FIFO Mode
  • MCAN CLK : 80MHz
  • CPU : R5F
Frame Type Arbitration BitRate(Mbps) Data BitRate(Mbps) Arb Phase bits Data Phase bits Throughput (Msg/Sec)
CAN FD STANDARD FORMAT 1 5 27 538 6666
CAN FD EXTENDED FORMAT 1 5 46 538 5780

MCSPI performance

MCSPI driver performance in different modes

  • measurement is provided for Master mode in Loopback configuration with TX and RX.
  • Transfer time captured with driver API in different operation mode.
  • Throughput comparison is added for transfer of 400 Bytes with different word width and corresponding number of words.
  • Time
  • CPU : R5F
  • Transfer Length : 400 Bytes
  • SPI Clock speed : 50MHz
Number of Words Word Width (Bits) Polled mode Throughput / Transfer time Interrupt mode (Mbps) Throughput / Transfer time Dma mode (Mbps) Throughput / Transfer time
400 08 12.91 Mbps / 254.15 us 23.74 Mbps / 134.79 us 0.91 Mbps / 3500.68 us
200 16 25.54 Mbps / 125.30 us 31.49 Mbps / 101.63 us 0.95 Mbps / 3356.74 us
100 32 38.84 Mbps / 82.38 us 37.58 Mbps / 85.14 us 0.97 Mbps / 3284.85 us
  • Theoretically for 400 Bytes at 50MHz time required for clocks is 64us.
  • Additionally hardware adds 160ns + 1bit time delay between each word transfer as measured in the scope

CPSW Performance

For CPSW performance refer Ethernet Performance

ICSSG Performance

TCP Test

  • Software/Application used : enet_lwip_icssg
  • iperf test type : TCP iperf
  • iperf command used : iperf -c 192.168.0.158 -i 10 -t 100 -r
  • Packet allocation : 32 buffers per each Rx flow, 16 buffers for Tx channel

TCP Performance(am64x/243x emvs):

TCP direction B/W (Mb/s) CPU load(%)
TCP RX 93.2 52.1
TCP TX 92.9 87.57
TCP Biderectional TX = 66.4 + RX = 66.5 99.24

TCP Performance(am243x-lp):

TCP direction B/W (Mb/s) CPU load(%)
TCP RX 93.20 36.82
TCP TX 93.30 52.54
TCP Biderectional TX = 88.8 + RX = 88.9 85.58

UDP Test

  • Software/Application used : enet_lwip_icssg
  • iperf test type : UDP iperf
  • iperf command used : iperf -c 192.168.0.158 -u -b 60M -l 256 -i 10 -t 100 -r
  • Packet allocation : 32 buffers per each Rx flow, 16 buffers for Tx channel

UDP TX Performance(am64x/243x emvs):

  • For Packet Size: 1500 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 100 0 -
50 Mbps 100 0.03 -
100 Mbps 100 0.07 -
Max(220 Mbps) 100 0.07 -

UDP TX Performance(am243x-lp):

  • For Packet Size: 1500 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 100 0 -
50 Mbps 100 0 -
100 Mbps 100 0 -

UDP RX Performance(am64x/243x emvs):

  • For Packet Size: 256 B
Rx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 44.35 0.11 -
50 Mbps 60.34 41 -
100 Mbps - - -
  • For Packet Size: 512 B
Rx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 21.83 0 -
50 Mbps 56.74 0.09 -
100 Mbps 65.61 41 -
  • For Packet Size: 1500 B
Rx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 16.84 0 -
50 Mbps 28.93 0 -
100 Mbps 53.16 0.06 -
Max(180 Mbps) 73.83 0.29 -

UDP RX Performance(am243x-lp):

  • For Packet Size: 256 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 37.35 0.12 -
50 Mbps 48 36 -
100 Mbps - - -
  • For Packet Size: 512 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 21.83 0 -
50 Mbps 40 0.12 -
100 Mbps 50 36 -
  • For Packet Size: 1500 B
Tx Side BW/Packet Size CPU load(%) Packet loss(%) Latency
25 Mbps 15 0 -
50 Mbps 26.5 0.08 -
100 Mbps 38 0.1 -

IPC performance

IPC NOTIFY

  • 10000 messages are sent and average one way message latency is measured
Local Core Remote Core Average Message Latency (us)
r5f0-0 m4f0-0 1.76
r5f0-0 r5f0-1 0.77
r5f0-0 r5f1-0 0.82
r5f0-0 r5f1-1 0.90
r5f0-0 a530-0 1.03
r5f0-0 a530-1 0.00

IPC RPMSG

  • 10000 messages are sent and average one way message latency is measured
Local Core Remote Core Message Size Average Message Latency (us)
r5f0-0 r5f0-1 32 7.870
r5f0-0 r5f0-1 64 10.425
r5f0-0 r5f0-1 112 14.284
r5f0-0 m4f0-0 32 17.425
r5f0-0 m4f0-0 64 23.454
r5f0-0 m4f0-0 112 32.487
r5f0-0 a530-0 32 7.249
r5f0-0 a530-0 64 8.551
r5f0-0 a530-0 112 10.754

MATHLIB

MATHLIB BENCHMARK

  • Calculated for the 500 samples taken between 0 and 2 * Pi
  • Trignometric function timings compared between the optimized Mathlib mcusdk implementation and the compiler mathlib version
  • The max error for each operation between the optimized Mathlib mcusdk functions and the compiler mathlib version is printed
    Function Err Max Cycles Mathlib (mcusdk) avg cycles Mathlib (mcusdk) max cycles mathlib (clang) avg cycles mathlib (clang)
    sin 0.0000007150 52 52.228001 701 278.614014
    cos 0.0000002870 750 66.578003 617 279.187988
    sincos sin 0.0000001790 79 78.895996 469 274.947998
    sincos cos 0.0000001900
    asin 0.0000003430 74 74.071999 616 430.029999
    acos 0.0000004770 76 76.000000 1066 385.256012
    atan 0.0000005360 80 80.084000 674 371.962006
    atan2 0.0000007150 117 104.776001 650 479.980011

SA2UL

PKA RSA SIGN VERIFY

  • Software/Application used : test_sa2ul_pka
  • Supported keys : 4K and 2K
  • CPU with operating speed : R5F with 800MHZ
  • OS used : nortos
    ECDSA Sign/sec Verify/sec Sign and verify/sec
    2048 631 8771 589
    4096 97 2770 94

SHA

  • Software/Application used : test_sa2ul_sha
  • Code Placement : OCMC
  • Data Placement : OCMC
  • Input Data sizes : 512B, 1KB, 2KB, 4KB, 8KB, 16KB and 32KB
  • CPU with operating speed : R5F with 800MHZ
    SHA Size Performance (Mbps)
    512 32.00 KB 2042.216379
    512 16.00 KB 1816.943044
    512 8.00 KB 1420.565204
    512 4.00 KB 948.937557
    512 2.00 KB 593.784543
    512 1024.00 B 340.376026
    512 512.00 B 180.749076
    256 32.00 KB 1592.430996
    256 16.00 KB 1417.569285
    256 8.00 KB 1153.295205
    256 4.00 KB 838.136650
    256 2.00 KB 544.929946
    256 1024.00 B 324.580259
    256 512.00 B 176.551724

PKA ECDSA

  • Software/Application used : test_sa2ul_pka
  • Supported Curves : p-256 and p-384
  • CPU with operating speed : R5F with 800MHZ
  • OS used : nortos
    ECDSA Sign/sec Verify/sec Sign and verify/sec
    256 1136 693 430
    384 586 349 218

AES

  • Software/Application used : test_sa2ul_aes
  • Code Placement : OCMC
  • Data Placement : OCMC
  • Input Data sizes : 512B, 1KB, 2KB, 4KB, 8KB, 16KB and 32KB
  • CPU with operating speed : R5F with 800MHZ
    Key Length operation Size Performance (Mbps)
    128 Encryption 32.00 KB 1417.914323
    128 Decryption 32.00 KB 1834.987356
    128 Encryption 16.00 KB 1259.550751
    128 Decryption 16.00 KB 1650.806845
    128 Encryption 8.00 KB 1084.875949
    128 Decryption 8.00 KB 1371.548161
    128 Encryption 4.00 KB 862.287425
    128 Decryption 4.00 KB 1023.440306
    128 Encryption 2.00 KB 602.740734
    128 Decryption 2.00 KB 695.711253
    128 Encryption 1024.00 B 392.831026
    128 Decryption 1024.00 B 425.089187
    128 Encryption 512.00 B 228.332520
    128 Decryption 512.00 B 234.341701
    256 Encryption 32.00 KB 1330.308797
    256 Decryption 32.00 KB 1520.049867
    256 Encryption 16.00 KB 1219.671521
    256 Decryption 16.00 KB 1358.399834
    256 Encryption 8.00 KB 1058.675767
    256 Decryption 8.00 KB 1157.828718
    256 Encryption 4.00 KB 831.569598
    256 Decryption 4.00 KB 906.163365
    256 Encryption 2.00 KB 605.917160
    256 Decryption 2.00 KB 653.106782
    256 Encryption 1024.00 B 389.515602
    256 Decryption 1024.00 B 399.975587
    256 Encryption 512.00 B 227.713690
    256 Decryption 512.00 B 226.705410

RSA ENCRYPT DECRYPT

  • Software/Application used : test_sa2ul_rsa
  • Code Placement : OCMC
  • Supported keys : 4K and 2K
  • CPU with operating speed : R5F with 800MHZ
  • Software/Application used : test_sa2ul_rsa
    Key Length operation Size Performance(Mbps)
    2048 Encryption 256.00 B 0.263871
    2048 Decryption 256.00 B 1.294870
    4096 Encryption 512.00 B 0.512152
    4096 Decryption 512.00 B 0.400639

USB

NET Driver ( RNDIS )

  • Measures TCP only TX bandwidth at every 1 sec interval using standard lwip-perf application.
  • Software/Applicaiton used : rndis_nortos
  • Input media : USB 2.0
  • Linux Host application used : iperf
  • CPU with operating speed : R5F with 800MHz
  • lwip-webserver ip address : 192.168.7.1
  • RNDIS Host ip address : 192.168.7.2
  • TCP window size : 85.0 KByte
ID Interval Transfer Bandwidth
0 0.0- 1.0 sec 4.25 MBytes 35.7 Mbits/sec
1 1.0- 2.0 sec 4.12 MBytes 34.6 Mbits/sec
2 2.0- 3.0 sec 4.12 MBytes 34.6 Mbits/sec
3 3.0- 4.0 sec 4.12 MBytes 34.6 Mbits/sec
4 4.0- 5.0 sec 4.12 MBytes 34.6 Mbits/sec
5 5.0- 6.0 sec 4.12 MBytes 34.6 Mbits/sec
6 6.0- 7.0 sec 4.12 MBytes 34.6 Mbits/sec
7 7.0- 8.0 sec 4.12 MBytes 34.6 Mbits/sec
8 8.0- 9.0 sec 4.25 MBytes 35.7 Mbits/sec
9 9.0-10.0 sec 4.12 MBytes 34.6 Mbits/sec
10 0.0-10.0 sec 41.5 MBytes 34.8 Mbits/sec