Change-1 : ENET(CPSW) and ENET(ICSS) pinmux configuration Change-2 : Support to configure link parameters in Sysconfig GUI tool.
In MCU+ SDK version of 10.00, ENET(CPSW) and ENET(ICSS) component in Sysconfig GUI has been updated with fixes to correct MII/RMII mode for ICSSG and CPSW Resp.. Additonally support added to release unused pins based on number of ports were enabled in CPSW.
The above described change makes any older 'example.syscfg' generated using SDK version of 09.00 or earlier not compatible with SDK version 10.00 or later. This incompatibility is seen only when either ENET(CPSW) or ENET(ICSS) is added in your application/example.If neither of the components are added, you may ignore this change and there is no impact. User will see the error in sysconfig gui tool when the old example.syscfg file is opened in updated version of mcu plus sdk.
If is possible to create a example.syscfg as per user configurations, please generate a new example.syscfg from any SDK example and change the configration as per your need. This is the safest option.
Sometimes, it is not easy to get a new example.syscfg that matches the older example.syscfg. In those case, please follow the below steps
Save the modifications. Then open sysconfig GUI tool with the modifications, save and close the tool.
In MCU+ SDK version of 10.00, parameters that configures link capabilities for auto negotiation such as speed and duplexity is added into syscfg GUI.
'EnetApp_initLinkArgs' function that is defined in the user applicaiton code is no longer called. Instead, a new function EnetApp_initLinkArgs is defined.