![Logo](ti_logo.svg) |
AM64x MCU+ SDK
09.02.01
|
|
Go to the documentation of this file.
41 #ifndef SDL_LBIST_PRIV_H_
42 #define SDL_LBIST_PRIV_H_
45 #if defined (IP_VERSION_LBIST_V0)
52 #define LBIST_NOT_DONE (0x0U)
53 #define LBIST_DONE (0x1U)
Definition: sdlr_lbist.h:52
SDL_lbistInstInfo * SDL_LBIST_getInstInfo(uint32_t instance)
uint32_t * pLBISTSig
Definition: sdl_lbist_priv.h:60
Definition: sdl_lbist_priv.h:56
void SDL_LBIST_eventHandler(void *arg)
This file contains the SDL DPL API's.
volatile uint32_t doneFlag
Definition: sdl_lbist_priv.h:66
uint32_t interruptNumber
Definition: sdl_lbist_priv.h:64
SDL_LBIST_config_t LBISTConfig
Definition: sdl_lbist_priv.h:68
SDL_lbistRegs * pLBISTRegs
Definition: sdl_lbist_priv.h:58
uint32_t expectedMISR
Definition: sdl_lbist_priv.h:62
This structure contains the different configuration used for LBIST Note that the LBIST configuration ...
Definition: sdl_ip_lbist.h:66