![Logo](ti_logo.svg) |
AM64x MCU+ SDK
09.02.01
|
|
Go to the documentation of this file.
33 #ifndef MCSPI_DMA_UDMA_H_
34 #define MCSPI_DMA_UDMA_H_
43 #define MCSPI_UDMA_CHANNEL_ENABLE (1U)
45 typedef struct McspiDma_UdmaArgs_s
51 typedef struct MCSPI_DmaChConfig_s
void * txChHandle
Definition: mcspi_dma_udma.h:53
void * rxChHandle
Definition: mcspi_dma_udma.h:55
void * cqRxEvtHandle
Definition: mcspi_dma_udma.h:59
void * txRingMem
Definition: mcspi_dma_udma.h:67
uint32_t ringMemSize
Definition: mcspi_dma_udma.h:71
Definition: mcspi_dma_udma.h:46
void * cqTxEvtHandle
Definition: mcspi_dma_udma.h:57
void * txHpdMem
Definition: mcspi_dma_udma.h:61
Definition: mcspi_dma_udma.h:52
void * rxHpdMem
Definition: mcspi_dma_udma.h:63
uint32_t isOpen
Definition: mcspi_dma_udma.h:79
uint32_t hpdMemSize
Definition: mcspi_dma_udma.h:65
void * rxRingMem
Definition: mcspi_dma_udma.h:69
uint32_t txEvtNum
Definition: mcspi_dma_udma.h:77
uint32_t rxEvtNum
Definition: mcspi_dma_udma.h:75
uint32_t isChEnabled
Definition: mcspi_dma_udma.h:81
uint32_t ringElemCnt
Definition: mcspi_dma_udma.h:73
void * drvHandle
Definition: mcspi_dma_udma.h:47