![Logo](ti_logo.svg) |
AM64x MCU+ SDK
09.02.01
|
|
Go to the documentation of this file.
69 #include <drivers/i2c/v0/cslr_i2c.h>
75 #define I2C_MAX_NUM_OWN_TARGET_ADDR (4U)
84 #define I2C_STS_SUCCESS ((int32_t) 0)
87 #define I2C_STS_ERR ((int32_t)-1)
90 #define I2C_STS_ERR_TIMEOUT ((int32_t)-2)
92 #define I2C_STS_ERR_INVALID_PARAM ((int32_t)-3)
94 #define I2C_STS_ERR_BUS_BUSY ((int32_t)-4)
97 #define I2C_STS_ERR_NO_ACK ((int32_t)-5)
100 #define I2C_STS_ERR_ARBITRATION_LOST ((int32_t)-6)
102 #define I2C_STS_ERR_ACCESS_ERROR ((int32_t)-7)
104 #define I2C_STS_RESTART ((int32_t)-8)
116 #define I2C_NO_WAIT ((uint32_t)0)
119 #define I2C_WAIT_FOREVER ((uint32_t)-1)
129 #define I2C_STATE_RESET ((uint8_t) 0U)
132 #define I2C_STATE_IDLE ((uint8_t) 1U)
135 #define I2C_STATE_BUSY ((uint8_t) 2U)
138 #define I2C_STATE_ERROR ((uint8_t) 3U)
150 #define I2C_100KHZ ((uint8_t) 0U)
152 #define I2C_400KHZ ((uint8_t) 1U)
154 #define I2C_1P0MHZ ((uint8_t) 2U)
156 #define I2C_3P4MHZ ((uint8_t) 3U)
167 #define I2C_MEM_ADDR_SIZE_8_BITS ((uint8_t) 1U)
169 #define I2C_MEM_ADDR_SIZE_16_BITS ((uint8_t) 2U)
180 #define I2C_WRITE_STATE ((uint8_t) 10U)
182 #define I2C_READ_STATE ((uint8_t) 11U)
184 #define I2C_TARGET_XFER_STATE ((uint8_t) 12U)
186 #define I2C_TARGET_RESTART_STATE ((uint8_t) 13U)
360 int32_t transferStatus);
372 int32_t transferStatus);
I2C_Clock_getTicks Clock_getTicks
Definition: i2c_lld.h:398
#define I2C_MAX_NUM_OWN_TARGET_ADDR
Definition: i2c_lld.h:75
uint32_t startTicks
Definition: i2c_lld.h:434
I2CLLD_Transaction * txn
Definition: i2c_lld.h:229
uint32_t readCount
Definition: i2c_lld.h:213
int32_t I2C_lld_Transaction_init(I2CLLD_Transaction *transaction)
API to set default values of I2CLLD_Transaction in transaction.
I2CLLD_targetTransaction * currentTargetTransaction
Definition: i2c_lld.h:424
uint32_t writeCountIdx
Definition: i2c_lld.h:428
uint8_t * writeBuf
Definition: i2c_lld.h:302
uint8_t * writeBufIdx
Definition: i2c_lld.h:426
uint32_t writeCount
Definition: i2c_lld.h:304
int32_t I2C_lld_Message_init(I2CLLD_Message *msg)
API to set default values of I2CLLD_Message in msg.
uint32_t readCount
Definition: i2c_lld.h:308
uint32_t targetAddress
Definition: i2c_lld.h:236
void(* I2C_lld_targetTransferCompleteCallback)(void *args, const I2CLLD_targetTransaction *targetTxn, int32_t transferStatus)
The definition of a transfer completion callback function used by the I2C driver when used in Target ...
Definition: i2c_lld.h:370
int32_t I2C_lld_write(I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
API to initiate the write transaction in polled mode.
uint32_t funcClk
Definition: i2c_lld.h:394
I2C Message.
Definition: i2c_lld.h:226
I2C_Clock_uSleep Clock_uSleep
Definition: i2c_lld.h:402
uint32_t memAddr
Definition: i2c_lld.h:275
void * arg
Definition: i2c_lld.h:238
uint8_t * readBuf
Definition: i2c_lld.h:306
int32_t I2C_lld_read(I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams, uint32_t timeout)
API to initiate the read transaction in polled mode.
uint8_t * writeBuf
Definition: i2c_lld.h:207
void(* I2C_lld_transferCompleteCallback)(void *args, const I2CLLD_Message *msg, int32_t transferStatus)
The definition of a transfer completion callback function used by the I2C driver when used in Control...
Definition: i2c_lld.h:358
uint8_t * readBuf
Definition: i2c_lld.h:211
uint32_t timeout
Definition: i2c_lld.h:240
I2CLLD_Transaction i2ctxn
Definition: i2c_lld.h:440
bool expandSA
Definition: i2c_lld.h:245
int32_t I2C_lld_readIntr(I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
API to initiate the read transaction in Interrupt mode.
int32_t I2C_lld_recoverBus(I2CLLD_Handle handle, uint32_t i2cDelay)
Function to recover the bus in case of lockup.
bool expandSA
Definition: i2c_lld.h:261
I2CLLD_Message * currentMsg
Definition: i2c_lld.h:422
I2C Transaction.
Definition: i2c_lld.h:204
uint8_t * buffer
Definition: i2c_lld.h:257
int32_t I2C_lld_mem_read(I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams, uint32_t timeout)
Function to initiate a transfer from I2C in interrupt mode.
int32_t I2C_lld_mem_write(I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams, uint32_t timeout)
Function to initiate a transfer from I2C in interrupt mode.
uint32_t timeout
Definition: i2c_lld.h:310
uint8_t * dataArray
Definition: i2c_lld.h:442
uint32_t intrNum
Definition: i2c_lld.h:390
uint32_t baseAddr
Definition: i2c_lld.h:388
int32_t I2C_lld_transferIntr(I2CLLD_Handle handle, I2CLLD_Message *msg)
Function to initiate a transfer from I2C in interrupt mode.
bool expandSA
Definition: i2c_lld.h:313
void I2C_lld_targetIsr(void *args)
This is the I2C Target ISR and can be used as IRQ handler in Target mode.
uint32_t txnCount
Definition: i2c_lld.h:231
int32_t I2C_lld_transferPoll(I2CLLD_Handle handle, I2CLLD_Message *msg)
Function to initiate a transfer from I2C in polled mode.
uint32_t readCountIdx
Definition: i2c_lld.h:432
int32_t I2C_lld_init(I2CLLD_Handle handle)
This API Initializes the I2C instance.
I2C_lld_transferCompleteCallback transferCompleteCallback
Definition: i2c_lld.h:404
I2C_ExtendedParams extendedParams
Definition: i2c_lld.h:273
uint32_t writeCount
Definition: i2c_lld.h:209
uint32_t(* I2C_Clock_getTicks)(void)
The definition of a get System Tick function used by the I2C driver to keep track of time.
Definition: i2c_lld.h:328
bool memTxnActive
Definition: i2c_lld.h:449
uint8_t memAddrSize
Definition: i2c_lld.h:446
bool controllerMode
Definition: i2c_lld.h:242
uint32_t(* I2C_Clock_usecToTicks)(uint64_t usecs)
The definition of a micro seconds to ticks function used by the I2C driver to get ticks from microsec...
Definition: i2c_lld.h:339
Data structure used with I2C_lld_mem_write(), I2C_lld_mem_writeIntr(), I2C_lld_mem_read(),...
Definition: i2c_lld.h:271
uint32_t deviceAddress
Definition: i2c_lld.h:255
int32_t I2C_lld_writeIntr(I2CLLD_Handle handle, I2C_ExtendedParams *extendedParams)
API to initiate the write transaction in Interrupt mode.
void(* I2C_Clock_uSleep)(uint32_t usec)
The definition of a sleep function used by the I2C driver for delay.
Definition: i2c_lld.h:348
uint32_t intStatusErr
Definition: i2c_lld.h:415
Data structure used with I2C_lld_write(), I2C_lld_writeIntr(), I2C_lld_read(), I2C_lld_readIntr()
Definition: i2c_lld.h:253
int32_t I2C_lld_mem_readIntr(I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams)
Function to initiate a transfer from I2C in interrupt mode.
uint8_t * readBufIdx
Definition: i2c_lld.h:430
uint8_t bitRate
Definition: i2c_lld.h:392
int32_t I2C_lld_probe(I2CLLD_Handle handle, uint32_t targetAddr)
Function to probe I2C.
int32_t I2C_lld_setBusFrequency(I2CLLD_Handle handle, uint32_t busFrequency)
Function to set the bus frequency.
int32_t I2C_lld_mem_writeIntr(I2CLLD_Handle handle, I2C_Memory_ExtendedParams *mem_extendedParams)
Function to initiate a transfer from I2C in interrupt mode.
void I2C_lld_controllerIsr(void *args)
This is the I2C Controller ISR and can be used as IRQ handler in Controller mode.
I2C_lld_targetTransferCompleteCallback targetTransferCompleteCallback
Definition: i2c_lld.h:406
int32_t I2C_lld_deInit(I2CLLD_Handle handle)
This API De-Initializes the I2C instance.
uint8_t state
Definition: i2c_lld.h:413
uint32_t size
Definition: i2c_lld.h:259
I2CLLD_targetTransaction i2cTargetTransaction
Definition: i2c_lld.h:451
I2C Driver Object.
Definition: i2c_lld.h:381
I2C_Clock_usecToTicks Clock_usecToTicks
Definition: i2c_lld.h:400
I2CLLD_Message i2cMsg
Definition: i2c_lld.h:438
I2C Target Transaction.
Definition: i2c_lld.h:299
void * args
Definition: i2c_lld.h:453
struct I2CLLD_Object * I2CLLD_Handle
int32_t I2C_lld_targetTransferIntr(I2CLLD_Handle handle, I2CLLD_targetTransaction *txn)
Function to initiate a transfer from I2C in target mode.
uint8_t memAddrSize
Definition: i2c_lld.h:277
uint32_t currentTxnCount
Definition: i2c_lld.h:436