|
AM64x MCU+ SDK
09.02.01
|
|
Go to the documentation of this file.
43 #include <drivers/hw_include/soc_config.h>
44 #include <board/flash/flash_config.h>
46 #define FLASH_INVALID_VALUE (0xFFFFFFFFU)
99 typedef struct Flash_DevConfig_s {
186 uint8_t *buf, uint32_t len) ;
202 uint8_t *buf, uint32_t len) ;
270 typedef struct Flash_Params_s {
280 typedef struct Flash_Fxns_s
295 typedef struct Flash_Attrs_s {
316 typedef struct Flash_Config_s
327 #if defined (DRV_VERSION_FLASH_V0)
328 #include <board/flash/ospi/flash_nor_ospi.h>
331 #if defined (DRV_VERSION_FLASH_V1)
332 #include <board/flash/qspi/flash_nor_qspi.h>
335 #if defined (DRV_VERSION_FLASH_V2)
336 #include <board/flash/ospi/flash_nor_ospi.h>
337 #include <board/flash/ospi/flash_nand_ospi.h>
340 #if defined (DRV_VERSION_GPMC_V0)
341 #include <board/flash/gpmc/flash_nand_gpmc.h>
uint8_t cmdPageLoadCyc1
Definition: flash.h:111
uint32_t flashType
Definition: flash.h:297
uint8_t cmdPageProgCyc1
Definition: flash.h:116
void Flash_close(Flash_Handle handle)
Close flash driver.
uint8_t cmdReadStatus
Definition: flash.h:120
Flash_Attrs * attrs
Definition: flash.h:318
uint32_t flashSize
Definition: flash.h:302
uint8_t srEraseStatus
Definition: flash.h:92
Flash_OpenFxn openFxn
Definition: flash.h:282
FlashCfg_EraseConfig eraseCfg
Definition: flash.h:134
uint32_t srWipReg
Definition: flash.h:85
uint32_t blockCount
Definition: flash.h:303
FlashCfg_ProtoEnConfig protocolCfg
Definition: flash.h:136
uint8_t cmdExtType
Definition: flash.h:101
void(* Flash_CloseFxn)(Flash_Config *config)
Driver implementation to close a specific flash driver.
Definition: flash.h:170
uint8_t cmdWren
Definition: flash.h:107
Flash_DevConfig * devConfig
Definition: flash.h:320
uint32_t driverInstance
Definition: flash.h:301
Flash driver configuration, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:317
int32_t Flash_offsetToBlkPage(Flash_Handle handle, uint32_t offset, uint32_t *block, uint32_t *page)
Utility API to convert offset in bytes to (Block Num, Page Num)
int32_t Flash_SectorPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t sector, uint32_t page)
Utility API to convert (Sector Num, Page Num) to offset in bytes.
uint8_t deviceBusyType
Definition: flash.h:126
uint8_t cmdRdsr
Definition: flash.h:108
uint32_t xspiWipReg
Definition: flash.h:129
uint8_t cmdPageProgCyc2
Definition: flash.h:117
Flash_EraseSectorFxn eraseSectorFxn
Definition: flash.h:287
uint32_t progStatusReg
Definition: flash.h:87
uint32_t flashBusyTimeout
Definition: flash.h:132
uint32_t sectorSize
Definition: flash.h:308
Flash_Fxns * fxns
Definition: flash.h:319
uint8_t srWriteProtectMask
Definition: flash.h:94
uint32_t pageSize
Definition: flash.h:306
uint8_t addrByteSupport
Definition: flash.h:104
int32_t(* Flash_ReadFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to read from flash using a specific flash driver.
Definition: flash.h:185
int32_t Flash_blkPageToOffset(Flash_Handle handle, uint32_t *offset, uint32_t block, uint32_t page)
Utility API to convert (Block Num, Page Num) to offset in bytes.
Flash device attributes, these are filled by SysCfg based on the flash device that is selected.
Definition: flash.h:295
char * flashName
Definition: flash.h:298
uint8_t cmdRandomReadCyc2
Definition: flash.h:114
uint32_t xspiWipBit
Definition: flash.h:130
Flash_EraseFxn eraseFxn
Definition: flash.h:286
Flash_Handle Flash_getHandle(uint32_t instanceId)
Get handle to flash driver.
Driver implementation callbacks.
Definition: flash.h:281
int32_t(* Flash_EraseFxn)(Flash_Config *config, uint32_t blockNum)
Driver implementation to erase a block using a specific flash driver.
Definition: flash.h:215
uint8_t cmdWrsr
Definition: flash.h:82
uint32_t xspiEraseStatusReg
Definition: flash.h:90
uint32_t Flash_getPhyTuningOffset(Flash_Handle handle)
Return flash offset to write PHY tuning data.
uint8_t cmdPageLoad
Definition: flash.h:83
Flash_NandConfig * nandCfg
Definition: flash.h:137
uint8_t fourByteAddrEnSeq
Definition: flash.h:106
uint8_t srProgStatus
Definition: flash.h:91
uint8_t srWip
Definition: flash.h:109
uint8_t srWel
Definition: flash.h:124
struct Flash_Config_s Flash_Config
Forward declaration of Flash_Config.
Definition: flash.h:67
uint8_t resetType
Definition: flash.h:125
int32_t(* Flash_WriteFxn)(Flash_Config *config, uint32_t offset, uint8_t *buf, uint32_t len)
Driver implementation to write to flash using specific flash driver.
Definition: flash.h:201
Flash_CloseFxn closeFxn
Definition: flash.h:283
uint8_t cmdPageLoadCyc2
Definition: flash.h:112
uint32_t flashWriteTimeout
Definition: flash.h:131
void Flash_Params_init(Flash_Params *params)
Set default parameters in the Flash_Params structure.
int32_t(* Flash_ResetFxn)(Flash_Config *config)
Driver implementation to soft reset the flash.
Definition: flash.h:241
uint8_t srWriteProtectReg
Definition: flash.h:93
uint32_t pageCount
Definition: flash.h:305
struct Flash_Params_s Flash_Params
Forward declaration of Flash_Params.
Definition: flash.h:72
uint32_t spareAreaSize
Definition: flash.h:309
uint8_t pageRowAddrCyc
Definition: flash.h:119
int32_t(* Flash_custProtocolFxn)(Flash_Config *config)
User implementation of a custom function to configure flash to operate in a specific protocol.
Definition: flash.h:262
uint32_t skipHwInit
Definition: flash.h:322
Flash_Attrs * Flash_getAttrs(uint32_t instanceId)
Return flash attributes.
uint8_t xspiWipRdCmd
Definition: flash.h:127
Flash device config. This will be part of the flash config, so has to be filled by sysconfig or other...
Definition: flash.h:80
uint32_t blockSize
Definition: flash.h:304
FlashCfg_ReadIDConfig idCfg
Definition: flash.h:135
uint32_t eraseStatusReg
Definition: flash.h:89
int32_t Flash_offsetToSectorPage(Flash_Handle handle, uint32_t offset, uint32_t *sector, uint32_t *page)
Utility API to convert offset in bytes to (Sector Num, Page Num)
int32_t Flash_eraseSector(Flash_Handle handle, uint32_t sectorNum)
Erase a sector from flash.
uint32_t deviceId
Definition: flash.h:299
Flash_ReadFxn readFxn
Definition: flash.h:284
uint8_t enable4BAddr
Definition: flash.h:103
int32_t Flash_reset(Flash_Handle handle)
Do a soft reset of the flash.
int32_t(* Flash_EraseSectorFxn)(Flash_Config *config, uint32_t sectorNum)
Driver implementation to erase a sector using a specific flash driver.
Definition: flash.h:228
Flash_WriteFxn writeFxn
Definition: flash.h:285
int32_t(* Flash_OpenFxn)(Flash_Config *config, Flash_Params *params)
Driver implementation to open a specific flash driver.
Definition: flash.h:158
uint8_t cmdReset
Definition: flash.h:121
Flash_Handle Flash_open(uint32_t instanceId, Flash_Params *params)
Open flash driver.
uint8_t cmdRandomInput
Definition: flash.h:115
uint8_t cmdRandomReadCyc1
Definition: flash.h:113
uint32_t xspiRdsrDummy
Definition: flash.h:86
uint8_t byteOrder
Definition: flash.h:102
uint32_t manufacturerId
Definition: flash.h:300
Flash_ResetFxn resetFxn
Definition: flash.h:288
uint8_t pageColAddrCyc
Definition: flash.h:118
int32_t Flash_eraseBlk(Flash_Handle handle, uint32_t blockNum)
Erase a block from flash.
int32_t Flash_write(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Write to flash.
uint8_t cmdPageProg
Definition: flash.h:84
int32_t(* Flash_quirksFxn)(Flash_Config *config)
User implementation of a custom function to handle vendor specific quirks.
Definition: flash.h:253
uint32_t sectorCount
Definition: flash.h:307
Parameters passed during Flash_open()
Definition: flash.h:270
void * Flash_Handle
Handle to the FLash driver returned by Flash_opem()
Definition: flash.h:62
Flash_quirksFxn quirksFxn
Definition: flash.h:272
Flash_custProtocolFxn custProtoFxn
Definition: flash.h:273
int32_t Flash_read(Flash_Handle handle, uint32_t offset, uint8_t *buf, uint32_t len)
Read data from flash.
uint32_t xspiProgStatusReg
Definition: flash.h:88
void * object
Definition: flash.h:321