AM64x MCU+ SDK  09.02.01
USB DFU Example

Introduction

  • This examples demonstrates the use of TinyUSB DFU DEV Class driver. Its implements all the necessary callbacks that are required by TinyUSB DFU DEV class driver.
  • When user issues DFU download command then the application receives the data in a static buffer via USB DFU. Once the manifest state is completed the application sends the received data back to UART0.
  • When user issues DFU Upload command it sends the **"Hello world from AM64x-AM243x DFU! - Partition 0"** string back to the HOST PC.
  • refer USB2.0 DFU specs to konw more about USB 2.0 DFU class.
Note
The max buffer size is 4KB thus, as far as this example is concerned user can send at max 4KB of data.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0_nortos
Toolchain ti-arm-clang
Board am64x-evm
Example folder examples/usb/device/dfu

Steps to Run the Example

Build the example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

HW Setup

  • To test the application, one can use a Windows/Linux PC as a USB host
  • Connect the J24 on AM64x/AM243x EVM to the USB host

USB 2.0 Host/Device Connector

Run the example

  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • When the application is running. Observer DFU device detected on HOST PC.
  • Open cmd in windows and terminal in case of Linux. Run Following command to detect whether the DFU device has been enumerated or not.

    Windows

    dfu-util -l 
    

    Linux

    sudo dfu-util -l 
    
  • If the enumeration is successful the following should be displayed on console.

AM64x-AM243x DFU Device detected.

DFU Download

  • Open COM port in windows and /dev/ttyUSBx in linux which opens console for UART0.
  • Once the DFU device is enumerated run the following command.

    Windows

    dfu-util -a 0 -i 0 -D test_data.txt
    

    Linux

    sudo dfu-util -a 0 -i 0 -D test_data.txt
    
  • The test_data.txt file contains a string data that is to be transfered.
  • Once the DFU transfer is completed following will be displayed on the terminal.

DFU Download command successful
  • Open UART0 serial port to observe the content of test_data.txt file displayed on same serial port.

Content of received file displayed on serial port.

DFU Upload

  • Run the following command to read the data from DFU device.

    Windows

    dfu-util -a 0 -i 0 -U upload_data.txt 
    

    Linux

    sudo dfu-util -a 0 -i 0 -U upload_data.txt
    
  • Once the DFU Upload transaction is successful , open upload_data.txt file to see the contents

Data sent by DFU device to DFU host.

See Also

USB