AM64x MCU+ SDK  09.02.01
SA2UL Random Number Generator Test

Introduction

This example demonstrates the Random number generation using SA2UL module.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am64x-evm
Example folder examples/security/crypto/sa2ul_rng/sa2ul_rng.c

Steps to Run the Example

See Also

SA2UL

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

All tests have passed!!
[SA2UL] Sa2ul Rng example started ...
[SA2UL] Sa2ul Rng output word 1 -- 0x3704DD0A
[SA2UL] Sa2ul Rng output word 2 -- 0x68719DEA
[SA2UL] Sa2ul Rng output word 3 -- 0x3A2733EE
[SA2UL] Sa2ul Rng output word 4 -- 0x943F007E
[SA2UL] Sa2ul Rng output word 1 -- 0xCE83C20D
[SA2UL] Sa2ul Rng output word 2 -- 0xAEB445B0
[SA2UL] Sa2ul Rng output word 3 -- 0xE052FEC9
[SA2UL] Sa2ul Rng output word 4 -- 0x713231C3
[SA2UL] Sa2ul Rng output word 1 -- 0xD5CF553B
[SA2UL] Sa2ul Rng output word 2 -- 0x1AB11E5F
[SA2UL] Sa2ul Rng output word 3 -- 0x25163494
[SA2UL] Sa2ul Rng output word 4 -- 0x5CD0432F
[SA2UL] Sa2ul Rng output word 1 -- 0x8372B743
[SA2UL] Sa2ul Rng output word 2 -- 0x75AA97AC
[SA2UL] Sa2ul Rng output word 3 -- 0x59F277C7
[SA2UL] Sa2ul Rng output word 4 -- 0x8DFC768C
[SA2UL] Sa2ul Rng output word 1 -- 0xAF3B154C
[SA2UL] Sa2ul Rng output word 2 -- 0x3A93F540
[SA2UL] Sa2ul Rng output word 3 -- 0xC3174A84
[SA2UL] Sa2ul Rng output word 4 -- 0xA361D316
[SA2UL] Sa2ul Rng example completed!!
All tests have passed!!