AM64x MCU+ SDK  09.02.01
I2C Memory Read

Introduction

This example demonstrates writing 10 Bytes of data to I2C based EEPROM devices present in the board and then reading back the same data from the EEPROM.

Supported Combinations

Attention
A53 NORTOS support is experimental and is NOT supported by TI.
Parameter Value
CPU + OS r5fss0-0 nortos
a53ss0-0 nortos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am64x-evm, am64x-sk
Example folder examples/drivers/i2c/i2c_memory_read

Steps to Run the Example

See Also

I2C

Sample Output

Shown below is a sample output when the application is run,