AM64x MCU+ SDK  09.02.01
I2C Led Read Write LLD

Introduction

This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. The application will blink all the I2C controlled LED in the EVM.

Application blinks leds for 3 loops in interrupt mode and 3 loops in polling mode. Application exits after 6 iterations.

Supported Combinations

Attention
A53 NORTOS, A53 FREERTOS and A53 FREERTOS SMP support is experimental and is NOT supported by TI.
Parameter Value
CPU + OS r5fss0-0 nortos
a53ss0-0 nortos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am64x-evm, am64x-sk
Example folder examples/drivers/i2c/i2c_led_blink_polling_lld

Steps to Run the Example

See Also

I2C Low Level Driver

Sample Output

Shown below is a sample output when the application is run,

[I2C] LED Read Write Test Started ...
LED will Blink for 3 loop in polling Mode ...
LED will Blink for 3 loop in interrupt Mode ...
All tests have passed!!