AM64x MCU+ SDK  09.02.01
GPIO LED Blink

Introduction

This example configures a GPIO pin connected to an LED on the EVM in output mode. The application toggles the LED on/off for 10 seconds and exits.

Supported Combinations

Attention
A53 NORTOS, A53 FREERTOS and A53 FREERTOS SMP support is experimental and is NOT supported by TI.
Parameter Value
CPU + OS r5fss0-0 nortos
m4fss0-0 nortos
a53ss0-0 nortos
a53ss0-0 freertos
a53ss0-0 freertos-smp
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am64x-evm, am64x-sk
Example folder examples/drivers/gpio/gpio_led_blink/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Watch out for LED LD26 on the EVM to blink which is controlled by MCU_GPIO0_5.

See Also

GPIO

Sample Output

Shown below is a sample output when the application is run,

GPIO LED Blink Test Started ...
LED will Blink for 10 seconds ...
GPIO LED Blink Test Passed!!
All tests have passed!!