AM64x MCU+ SDK  09.02.01
SOC

The SOC driver provides API to configure SOC specific features like clocks.

Features Supported

  • API to enable/disable a module clock
  • API to set clock frequency for module
  • Generic utility API like get CPU clock, get core name string, control module MMR lock/unlock API
  • Address Translation APIs for all the R5F cores
  • SOC Software Warm Reset/POR Reset APIs

SysConfig Features

  • SOC driver is integrated with each of the drivers. User need not perform any explicit configuration for this driver

Features NOT Supported

NA

Important Usage Guidelines

  • Most of these APIs are already integrated with SysConfig tool and the generated code does the required call to enable a module, set the required clock and so on. User need to use these APIs in their application only for exceptional scenarios.
Note
The SOC_controlModuleLockMMR API will be ineffective in the case of AM64x SOC, since AM64x is mostly used in conjunction with Linux, and the linux kernel assumes MMRs to be unlocked. This is protected with a #if statement in the SOC driver. Please remove this condition if the SDK is used without linux.
  • All MCU domain resets act as a main reset to the whole device. (MAIN and MCU domains)
  • MAIN domain resets will only reset the MAIN domain.
  • Please refer "Reset" chapter in techical reference manual for more details.

Example Usage

Include the below file to access the APIs

#include <drivers/soc.h>

Get Core Name String

const char *coreName;
DebugP_log("Core name is: %s\r\n", coreName);

Get CPU Clock Frequency

uint64_t cpuClockRate;
cpuClockRate = SOC_getSelfCpuClk();
DebugP_log("CPU Clock Frequency: %u\r\n", cpuClockRate);

Set CPU Clock Frequency

#include <drivers/sciclient.h> /* For the device and clock macros */
uint32_t moduleId = TISCI_DEV_PRU_ICSSG0;
uint64_t clkRate = 300000000U;
SOC_moduleSetClockFrequency(moduleId, clkId, clkRate);

Set CPU Clock Frequency with a specific parent clock

#include <drivers/sciclient.h> /* For the device and clock macros */
uint32_t moduleId = TISCI_DEV_PRU_ICSSG0;
uint64_t clkRate = 300000000U;
SOC_moduleSetClockFrequencyWithParent(moduleId, clkId, clkParentId, clkRate);

API

APIs for SOC Specific Functions

sciclient.h
This file contains prototypes for APIs contained as a part of SCICLIENT as well as the structures of ...
SOC_moduleSetClockFrequency
int32_t SOC_moduleSetClockFrequency(uint32_t moduleId, uint32_t clkId, uint64_t clkRate)
Set module clock to specified frequency.
SOC_moduleSetClockFrequencyWithParent
int32_t SOC_moduleSetClockFrequencyWithParent(uint32_t moduleId, uint32_t clkId, uint32_t clkParent, uint64_t clkRate)
Set module clock to specified frequency and with a specific parent.
CSL_CORE_ID_R5FSS0_0
#define CSL_CORE_ID_R5FSS0_0
Definition: cslr_soc_defines.h:71
TISCI_DEV_PRU_ICSSG0_CORE_CLK
#define TISCI_DEV_PRU_ICSSG0_CORE_CLK
Definition: tisci_clocks.h:627
DebugP_log
#define DebugP_log(format,...)
Function to log a string to the enabled console.
Definition: DebugP.h:225
SOC_getSelfCpuClk
uint64_t SOC_getSelfCpuClk(void)
Get the clock frequency in Hz of the CPU on which the driver is running.
TISCI_DEV_PRU_ICSSG0_CORE_CLK_PARENT_HSDIV4_16FFT_MAIN_2_HSDIVOUT0_CLK
#define TISCI_DEV_PRU_ICSSG0_CORE_CLK_PARENT_HSDIV4_16FFT_MAIN_2_HSDIVOUT0_CLK
Definition: tisci_clocks.h:628
TISCI_DEV_PRU_ICSSG0
#define TISCI_DEV_PRU_ICSSG0
Definition: tisci_devices.h:133
SOC_getCoreName
const char * SOC_getCoreName(uint16_t coreId)
Convert a core ID to a user readable name.