The Octal Serial Peripheral Interface (OSPI) module is a kind of Serial Peripheral Interface (SPI) module which allows single, dual, quad or octal read and write access to external flash devices. The OSPI module is used to transfer data, either in a memory mapped direct mode (for example a processor wishing to execute code directly from external flash memory), or in an indirect mode where the module is set-up to silently perform some requested operation, signaling its completion via interrupts or status registers.
Features Supported
- Support for single, dual, quad (QSPI mode) or octal I/O instructions.
- Supports dual Quad-SPI mode for fast boot applications.
- Memory mapped ‘direct’ mode of operation for performing flash data transfers and executing code from flash memory.
- Programmable delays between transactions.
- Legacy mode allowing software direct access to low level transmit and receive FIFOs, bypassing the higher layer processes.
- An independent reference clock to decouple bus clock from SPI clock – allows slow system clocks.
- Programmable baud rate generator to generate OSPI clocks.
- Supports BOOT mode.
- Handling ECC errors for flash devices with embedded correction engine.
SysConfig Features
- Note
- It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
- OSPI instance name
- Input clock frequency to be used for OSPI module
- Input clock divider which decides the baud-rate at which the flash will be read
- Chip Select
- Enabling of various features like DMA, PHY mode(not supported yet), XIP(not supported yet)
- In advanced config, you can choose various parameters like frame format, decoder chip select, read dummy cycles etc.
- Pinmux configurations for the OSPI instance
Features not Supported
- Interrupt mode is not supported yet.
Example Usage
Include the below file to access the APIs
Instance Open Example
Instance Close Example
API
APIs for OSPI