AM64x MCU+ SDK  09.02.00
sdl_rom_checksum.h
Go to the documentation of this file.
1 /* Copyright (C) 2023 Texas Instruments Incorporated.
2  *
3  * Redistribution and use in source and binary forms, with or without
4  * modification, are permitted provided that the following conditions
5  * are met:
6  *
7  * Redistributions of source code must retain the above copyright
8  * notice, this list of conditions and the following disclaimer.
9  *
10  * Redistributions in binary form must reproduce the above copyright
11  * notice, this list of conditions and the following disclaimer in the
12  * documentation and/or other materials provided with the
13  * distribution.
14  *
15  * Neither the name of Texas Instruments Incorporated nor the names of
16  * its contributors may be used to endorse or promote products derived
17  * from this software without specific prior written permission.
18  *
19  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
20  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
21  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
22  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
23  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
24  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
25  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
26  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
27  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
28  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
29  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
30  *
31  */
44 #ifndef SDL_ROM_CHECKSUM_H_
45 #define SDL_ROM_CHECKSUM_H_
46 
47 #ifdef __cplusplus
48 extern "C" {
49 #endif
50 #include <sdl/include/soc_config.h>
51 #if defined (IP_VERSION_ROMCHECKSUM_V0)
53 #endif
54 
75 #define SDL_LENGTH_OF_DATA_TO_BE_HASHED ((uint32_t)196544)
76 
81 #define SDL_LENGTH_OF_GOLDEN_DATA ((uint64_t)8)
82 
87 #define SDL_GOLDEN_DATA_POINTER (uint64_t *)(0x004182FFC0)
88 
93 #define SDL_DATA_TO_BE_HASHED_POINTER (uint8_t *)(0x0041800000)
94 
114 
116 #ifdef __cplusplus
117 }
118 #endif
119 
120 #endif /* SDL_ROM_CHECKSUM_H_ */
sdl_ip_rom_checksum.h
This file contains the SDL-FL API's for ROM Checksum.
SDL_ROM_Checksum_compute
int32_t SDL_ROM_Checksum_compute(void)
This function will compute Checksum of ROM.