AM64x MCU+ SDK  09.02.00
DDR ECC Test MAIN ESM

Note
This example demostrates handling the ESM error in the Main domain R5. The error can also be routed to MCU ESM and error handled in the safety domain (M4 core)

Introduction

This example simulates a 1b and 2b ECC error for DDR and waits for interrupt via the MAIN ESM instance. If the interrupt is not received the test fails.

Supported Combinations

AM64X

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am64x-evm am64x-sk
Example folder examples/drivers/ddr/ddr_ecc_test_main_esm/

Steps to Run the Example

See Also

DDR

Sample Output

Shown below is a sample output when the application is run,

Waiting on Single bit Error Correction Interrupt...
1b ECC error detected and corrected
Waiting on Dual bit error detection Interrupt...
2b ECC error detected
All tests have passed!!