![Logo](ti_logo.svg) |
AM64x MCU+ SDK
09.00.00
|
|
Go to the documentation of this file.
96 #ifndef MAX_LOGMSG_CATEGORIES
98 #define MAX_LOGMSG_CATEGORIES 16
104 #define DBGMSG_LEVEL_MARK {"NON", "FTL", "ERR", "WRN", "INF", "IFV", "DBG", "DBV"}
110 #define UBL_TS_BIT_FIELDS 3 // bit0 and bit1
116 #define UBL_OVERRIDE_ISTR(x,y) ub_log_initstr_override(x,UBB_GETENV(y))
118 #ifdef PRINT_FORMAT_NO_WARNING
120 #define PRINT_FORMAT_ATTRIBUTE1
121 #define PRINT_FORMAT_ATTRIBUTE4
124 #define PRINT_FORMAT_ATTRIBUTE1 __attribute__((format (printf, 1, 2)))
125 #define PRINT_FORMAT_ATTRIBUTE4 __attribute__((format (printf, 4, 5)))
@ UBL_WARN
Definition: ub_logging.h:88
@ UBL_NONE
Definition: ub_logging.h:85
int ub_log_return(int cat_index)
return console log level and console log level to the previous status
const char * ub_log_initstr_override(const char *ns, const char *os)
override 'istr' of ub_log_inig
@ UBL_INFO
Definition: ub_logging.h:89
int ub_log_add_category(const char *catstr)
add a category of logging at the bottom of the index
int ub_log_print(int cat_index, int flags, ub_dbgmsg_level_t level, const char *astr)
print log message
@ UBL_ERROR
Definition: ub_logging.h:87
void ub_log_flush(void)
flush out messages on the both of cosole log and debug log
@ UBL_DEBUGV
Definition: ub_logging.h:92
bool ub_clog_on(int cat_index, ub_dbgmsg_level_t level)
check if console log is enabled or not for the indicated cat_index and level
@ UBL_INFOV
Definition: ub_logging.h:90
@ UBL_DEBUG
Definition: ub_logging.h:91
ub_dbgmsg_level_t
This defines different logging levels.
Definition: ub_logging.h:84
void ub_log_init(const char *istr)
initialize logging by a string
uint32_t flags
Definition: csl_udmap_tr.h:0
int ub_log_change(int cat_index, ub_dbgmsg_level_t clevel, ub_dbgmsg_level_t dlevel)
change console log level to clevel, and debug log level to delevl
bool ub_dlog_on(int cat_index, ub_dbgmsg_level_t level)
check if debug log is enabled or not for the indicated cat_index and level
@ UBL_FATAL
Definition: ub_logging.h:86
void ub_console_debug_select_print(bool console, bool debug, const char *astr)
output to console out and debug out by selection