![Logo](ti_logo.svg) |
AM64x MCU+ SDK
09.00.00
|
|
Go to the documentation of this file.
34 #ifndef SDL_SOC_RTI_H_
35 #define SDL_SOC_RTI_H_
37 #include <sdl/include/am64x_am243x/sdlr_soc_baseaddress.h>
58 #define SDL_RTI_MAX_INSTANCE (0x07U)
59 #define INSTANCE_INVALID (0x0U)
93 SDL_RTI1_CFG_BASE, SDL_RTI8_CFG_BASE, SDL_RTI9_CFG_BASE, \
94 SDL_RTI10_CFG_BASE, SDL_RTI11_CFG_BASE, \
@ SDL_INSTANCE_RTI9_CFG
Definition: sdl_soc_rti.h:79
@ SDL_INSTANCE_RTI10_CFG
Definition: sdl_soc_rti.h:81
@ SDL_INSTANCE_MCU_RTI0_CFG
Definition: sdl_soc_rti.h:73
@ SDL_INSTANCE_RTI8_CFG
Definition: sdl_soc_rti.h:78
@ SDL_INSTANCE_INVALID
Definition: sdl_soc_rti.h:83
@ SDL_INSTANCE_RTI11_CFG
Definition: sdl_soc_rti.h:82
int32_t SDL_RTI_getBaseaddr(SDL_RTI_InstanceType instance, uint32_t *baseAddr)
#define SDL_RTI_MAX_INSTANCE
Definition: sdl_soc_rti.h:58
@ SDL_INSTANCE_RTI0_CFG
Definition: sdl_soc_rti.h:75
@ SDL_INSTANCE_RTI1_CFG
Definition: sdl_soc_rti.h:76
static uint32_t SDL_RTI_baseAddress[SDL_RTI_MAX_INSTANCE+1U]
Definition: sdl_soc_rti.h:92
SDL_RTI_InstanceType
Definition: sdl_soc_rti.h:71