AM64x MCU+ SDK  09.00.00
ECC

To increase functional and system reliability, the memories in many device modules and subsystems are protected by Error Correcting Code (ECC), which performs Single Error Correction (SEC) and Double Error Detection (DED). Detected errors are reported via ESM. Single bit errors are corrected, and double bit errors are detected. The ECC Aggregator is connected to these memory and interconnect components which have the ECC. The ECC aggregator provides access to control and monitor the ECC protected memories in a module or subsystem.

SDL provides support for ECC aggregator configuration. Each ECC aggregator instance can be independently configured through the same SDL API by passing a different instance. The safety manual also defines test-for-diagnostics for the various IPs with ECC/parity support. The SDL also provides the support for executing ECC aggregator self-tests, using the error injection feature of the ECC aggregator. The ECC aggregators should be configured at startup, after running BIST.

Features Supported

The SDL provides support for the ECC through:

  • ECC Configuration API
  • ECC self-test API
  • ECC error injection API
  • ECC static register readback API
  • ECC error status APIs

There are over 40 ECC aggregators on the device each supporting multiple memories and interconnects.

SysConfig Features

  • None

Features NOT Supported

  • None

Important Usage Guidelines

There are two types of ECC aggregator RAM IDs supported on the device (wrapper and interconnect). The wrapper types are used for memories where local computations are performed for particular processing cores in the device, and the interconnect types are utilized for interconnect bus signals between cores or to/from peripherals.

For wrapper RAM ID types, after injecting an error, the memory associated with that RAM ID needs to be accessed in order to trigger the error interrupt event. It is the application's responsibility to trigger the error event through memory access after injecting the error.

Example Usage

The following shows an example of SDL ECC API usage by the application to set up the ECC to monitor for errors, as well as how to perform ECC self-test. The ESM should be configured to notify of the desired ECC events for the IPs. Please refer to the TRM for a list of the ESM events.

The following function is required to be defined by the application. It is used by the ECC module to notify the application in case of certain ECC errors that are reported through the R5F exception handlers. If it is not defined, it will result in a linker error. An example implementation is given below.

uint32_t errorSrc,
uint32_t address,
uint32_t ramId,
uint64_t bitErrorOffset,
uint32_t bitErrorGroup)
{
DebugP_log("\r\n ECC Error Call back function called : eccMemType %d, errorSrc 0x%x, " \
"address 0x%x, ramId %d, bitErrorOffset 0x%04x%04x, bitErrorGroup %d\n",
eccMemType, errorSrc, address, ramId, (uint32_t)(bitErrorOffset >> 32),
(uint32_t)(bitErrorOffset & 0x00000000FFFFFFFF), bitErrorGroup);
DebugP_log("\r Take action \n");
/* Any additional customer specific actions can be added here */
}

Certain ECC events on CPU memory are reported as Exception events. In this case, the ECC SDL provdes a set of exception handlers that can be used to enable the SDL ECC self-test functionality and for notification of the ECC errors. The following example shows how to set up the exception handlers to use the SDL ECC implementations, and also provide application-specific handlers that will be called by the SDL handlers after the handler checks for ECC errors:

const SDL_R5ExptnHandlers ECC_Test_R5ExptnHandlers =
{
.swiExptnHandler = &SDL_EXCEPTION_swIntrExptnHandler,
.irqExptnHandler = &SDL_EXCEPTION_irqExptnHandler,
.fiqExptnHandler = &SDL_EXCEPTION_fiqExptnHandler,
.udefExptnHandlerArgs = ((void *)0u),
.swiExptnHandlerArgs = ((void *)0u),
.pabtExptnHandlerArgs = ((void *)0u),
.dabtExptnHandlerArgs = ((void *)0u),
.irqExptnHandlerArgs = ((void *)0u),
};
void ECC_Test_undefInstructionExptnCallback(void)
{
DebugP_log("\r\nUndefined Instruction exception\r\n");
}
void ECC_Test_swIntrExptnCallback(void)
{
DebugP_log("\r\nSoftware interrupt exception\r\n");
}
void ECC_Test_prefetchAbortExptnCallback(void)
{
DebugP_log("\r\nPrefetch Abort exception\r\n");
}
void ECC_Test_dataAbortExptnCallback(void)
{
DebugP_log("\r\nData Abort exception\r\n");
}
void ECC_Test_irqExptnCallback(void)
{
DebugP_log("\r\nIrq exception\r\n");
}
void ECC_Test_fiqExptnCallback(void)
{
DebugP_log("\r\nFiq exception\r\n");
}
void ECC_Test_exceptionInit(void)
{
SDL_EXCEPTION_CallbackFunctions_t exceptionCallbackFunctions =
{
.udefExptnCallback = ECC_Test_undefInstructionExptnCallback,
.swiExptnCallback = ECC_Test_swIntrExptnCallback,
.pabtExptnCallback = ECC_Test_prefetchAbortExptnCallback,
.dabtExptnCallback = ECC_Test_dataAbortExptnCallback,
.irqExptnCallback = ECC_Test_irqExptnCallback,
.fiqExptnCallback = ECC_Test_fiqExptnCallback,
};
/* Initialize SDL exception handler */
SDL_EXCEPTION_init(&exceptionCallbackFunctions);
/* Register SDL exception handler */
Intc_RegisterExptnHandlers(&ECC_Test_R5ExptnHandlers);
return;
}

To configure ECC for an instance and specified ram IDs:

static SDL_ECC_MemSubType ECC_Test_AGGR1_A0subMemTypeList[MAIN_AGGR1_AGGR1_MAX_MEM_SECTIONS] =
{
SDL_ECC_AGGR1_IAM64_MAIN_INFRA_CBASS_CBASS_MAIN_0_AM64_MAIN_INFRA_CBASS_CBASS_IK3VTM_N16FFC_MAIN_0_VBUSP_P2P_BRIDGE_IK3VTM_N16FFC_MAIN_0_VBUSP_BRIDGE_BUSECC_RAM_ID,
SDL_ECC_AGGR1_IAM64_MAIN_INFRA_CBASS_CBASS_MAIN_0_AM64_MAIN_INFRA_CBASS_CBASS_MAIN_SYSCLK0_4_CLK_EDC_CTRL_CBASS_INT_MAIN_SYSCLK0_4_BUSECC_RAM_ID,
};
static SDL_ECC_InitConfig_t ECC_Test_AGGR1A0ECCInitConfig =
{
.numRams = MAIN_AGGR1_AGGR1_MAX_MEM_SECTIONS,
.pMemSubTypeList = &(ECC_Test_AGGR1_A0subMemTypeList[0]),
};

Initialization of ECC

int32_t ECC_Example_init (void)
{
int32_t retValue=0;
void *ptr = (void *)&arg;
SDL_ErrType_t result;
#if defined (R5F_CORE)
/* Initialise exception handler */
ECC_Test_exceptionInit();
DebugP_log("\r\nECC_Test_init: Exception init complete \r\n");
if (retValue == 0) {
/* Initialize ECC Memory */
result = SDL_ECC_initMemory(SDL_ECC_AGGR1, SDL_ECC_AGGR1_IAM64_MAIN_INFRA_CBASS_CBASS_MAIN_0_AM64_MAIN_INFRA_CBASS_CBASS_IK3VTM_N16FFC_MAIN_0_VBUSP_P2P_BRIDGE_IK3VTM_N16FFC_MAIN_0_VBUSP_BRIDGE_BUSECC_RAM_ID);
if (result != SDL_PASS) {
/* print error and quit */
DebugP_log("\r\nECC_Test_init: Error initializing Memory of R5FSS0 CORE0 ECC: result = %d\r\n", result);
retValue = -1;
} else {
DebugP_log("\r\nECC_Test_init: Initialize of R5FSS0 CORE0 ECC Memory is complete \r\n");
}
}
#endif
if (retValue == SDL_APP_TEST_PASS) {
/* Initialize MAIN ESM module */
result = SDL_ESM_init(SDL_ESM_INST_MAIN_ESM0, &ECC_Test_esmInitConfig_MAIN, SDL_ESM_applicationCallbackFunction, ptr);
if (result != SDL_APP_TEST_PASS) {
/* print error and quit */
DebugP_log("ECC_Example_init: Error initializing MAIN ESM: result = %d\n\n", result);
retValue = SDL_APP_TEST_FAILED;
} else {
DebugP_log("ECC_Example_init: Init MAIN ESM complete \n\n");
}
}
if (retValue == SDL_APP_TEST_PASS) {
/* Initialize MCU ESM module */
result = SDL_ESM_init(SDL_ESM_INST_MCU_ESM0, &ECC_Test_esmInitConfig_MCU, SDL_ESM_applicationCallbackFunction, ptr);
if (result != SDL_APP_TEST_PASS) {
/* print error and quit */
DebugP_log("ECC_Example_init: Error initializing MCU ESM: result = %d\n\n", result);
retValue = SDL_APP_TEST_FAILED;
} else {
DebugP_log("ECC_Example_init: Init MCU ESM complete \n\n");
}
}
if (retValue == SDL_APP_TEST_PASS) {
/* Initialize ECC */
result = SDL_ECC_init(SDL_ECC_AGGR1, &ECC_Test_AGGR1A0ECCInitConfig);
if (result != SDL_APP_TEST_PASS) {
/* print error and quit */
DebugP_log("SDTF_init: Error initializing M4F core ECC: result = %d\n\n", result);
retValue = SDL_APP_TEST_FAILED;
} else {
DebugP_log("\n\nSDTF_init: AGGR1 ECC Init complete \n\n");
}
}
return retValue;
}

Once the ECC is configured, then error notifications will come to the ESM module, and will activate the ESM-registered application callback. The application callback may want to retrive the error information in order to take some action based on the error, like clearing the ECC interrupts, logging the error information, or some other action:

retVal = SDL_ECC_getESMErrorInfo(esmInst, intSrc, &eccmemtype, &eccIntrSrc);
retVal = SDL_ECC_getErrorInfo(eccmemtype, eccIntrSrc, &eccErrorInfo);
/* Any additional customer specific actions can be added here */

To clear and acknowledge the ECC interrupt:

if (eccErrorInfo.injectBitErrCnt != 0)
{
/* Clear interrupt for EDC Interconnect memory types */
SDL_ECC_clearNIntrPending(eccmemtype, eccErrorInfo.memSubType, eccIntrSrc, SDL_ECC_AGGR_ERROR_SUBTYPE_INJECT, eccErrorInfo.injectBitErrCnt);
}
else
{
/* Clear interrupt for Wrapper memory types */
SDL_ECC_clearNIntrPending(eccmemtype, eccErrorInfo.memSubType, eccIntrSrc, SDL_ECC_AGGR_ERROR_SUBTYPE_NORMAL, eccErrorInfo.bitErrCnt);
}
retVal = SDL_ECC_ackIntr(eccmemtype, eccIntrSrc);

Execute an ECC Self-Test for a specified ECC aggregator (memtype) and RAM Id (subtype):

Inject an error for a specified ECC aggregator (memtype) and RAM Id (subtype)

/* Run one shot test for AGGR1 2 bit error */
/* Note the address is relative to start of ram */
injectErrorConfig.pErrMem = (uint32_t *)(0u);
injectErrorConfig.flipBitMask = 0x5;
injectErrorConfig.chkGrp = 0x1;
subType = SDL_ECC_AGGR1_IAM64_MAIN_INFRA_CBASS_CBASS_MAIN_0_AM64_MAIN_INFRA_CBASS_CBASS_MAIN_SYSCLK0_4_CLK_EDC_CTRL_CBASS_INT_MAIN_SYSCLK0_4_BUSECC_RAM_ID;
result = SDL_ECC_injectError(SDL_ECC_AGGR1,
subType,
&injectErrorConfig);
if (result != SDL_EFAIL ) {
DebugP_log("\r\n Error inject at pErrMem 0x%p EFAIL test failed",
injectErrorConfig.pErrMem);
retVal = -1;
} else {
/* Access the memory where injection is expected */
testLocationValue = injectErrorConfig.pErrMem[0];
DebugP_log("\r\n Error inject at pErrMem 0x%p: EFAIL test complete",
injectErrorConfig.pErrMem);
}
return retVal;

Read the Static registers:

/* Read back the static registers */
result = SDL_ECC_getStaticRegisters(SDL_ECC_AGGR0_SAM62_SEC_ECC_AGGR, &staticRegs);
if (result != SDL_PASS) {
/* print error and quit */
DebugP_log("\r\nECC_Test_init: Error reading the static registers: result = %d\n\n");
retValue = -1;
} else {
DebugP_log("\r\nECC_Test_init: M4F Memtype Register Readback successful \n\n");
}

API

APIs for SDL ECC (ECC_AGGR)

SDL_ECC_InitConfig_t
Definition: sdl_ecc.h:312
SDL_ECC_AGGR_ERROR_SUBTYPE_NORMAL
#define SDL_ECC_AGGR_ERROR_SUBTYPE_NORMAL
Definition: V1/sdl_ip_ecc.h:160
SDL_ECC_initMemory
int32_t SDL_ECC_initMemory(SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType)
Initializes Memory to be ready for ECC error detection. Assumes ECC is already enabled.
SDL_ECC_InitConfig_t::numRams
uint32_t numRams
Definition: sdl_ecc.h:313
SDL_R5ExptnHandlers
Structure containing the Exception Handlers. If application does not want register an exception handl...
Definition: sdl_interrupt.h:111
SDL_INJECT_ECC_ERROR_FORCING_2BIT_ONCE
@ SDL_INJECT_ECC_ERROR_FORCING_2BIT_ONCE
Definition: sdl_ecc.h:253
SDL_ECC_injectError
int32_t SDL_ECC_injectError(SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_ECC_InjectErrorType errorType, const SDL_ECC_InjectErrorConfig_t *pECCErrorConfig)
Injects ECC error at specified location Assumes ECC is already enabled.
SDL_ECC_ackIntr
int32_t SDL_ECC_ackIntr(SDL_ECC_MemType eccMemType, SDL_Ecc_AggrIntrSrc intrSrc)
Acknowledge the ECC interrupt.
SDL_EXCEPTION_swIntrExptnHandler
void SDL_EXCEPTION_swIntrExptnHandler(void *param)
SW Interrupt Exception Handler.
SDL_ECC_getStaticRegisters
int32_t SDL_ECC_getStaticRegisters(SDL_ECC_MemType eccMemType, SDL_ECC_staticRegs *pStaticRegs)
Gets the static registers for the specified ECC instance.
SDL_EXCEPTION_undefInstructionExptnHandler
void SDL_EXCEPTION_undefInstructionExptnHandler(void *param)
Undefined Instruction Exception Handler.
SDL_ECC_AGGR_ERROR_SUBTYPE_INJECT
#define SDL_ECC_AGGR_ERROR_SUBTYPE_INJECT
Definition: V1/sdl_ip_ecc.h:162
SDL_EXCEPTION_prefetchAbortExptnHandler
void SDL_EXCEPTION_prefetchAbortExptnHandler(void *param)
Prefetch Abort Exception Handler.
Intc_RegisterExptnHandlers
void Intc_RegisterExptnHandlers(const SDL_R5ExptnHandlers *handlers)
This function registers handlers for various exceptions.
DebugP_log
#define DebugP_log(format,...)
Function to log a string to the enabled console.
Definition: DebugP.h:225
SDL_EXCEPTION_irqExptnHandler
void SDL_EXCEPTION_irqExptnHandler(void *param)
IRQ Exception Handler.
SDL_EXCEPTION_init
void SDL_EXCEPTION_init(const SDL_EXCEPTION_CallbackFunctions_t *callbackFunctions)
Initialise Exception module.
SDL_EXCEPTION_CallbackFunctions_t
Structure of call back functions for various exception events.
Definition: sdl_exception.h:74
SDL_ECC_getESMErrorInfo
int32_t SDL_ECC_getESMErrorInfo(SDL_ESM_Inst instance, uint32_t intSrc, SDL_ECC_MemType *eccMemType, SDL_Ecc_AggrIntrSrc *intrSrcType)
Retrieves the ECC error information for the specified ESM error. If it isn't an ECC error or the ECC ...
SDL_ESM_init
int32_t SDL_ESM_init(SDL_ESM_Inst instance, const SDL_ESM_config *pConfig, SDL_ESM_applicationCallback applicationCallback, void *appArg)
SDL ESM API to initialize an ESM instance. The API initializes the specified ESM instance with the pr...
SDL_R5ExptnHandlers::udefExptnHandler
exptnHandlerPtr udefExptnHandler
Definition: sdl_interrupt.h:112
SDL_ECC_MemSubType
uint32_t SDL_ECC_MemSubType
This enumerator indicate ECC memory Sub Type.
Definition: sdl_ecc.h:285
SDL_ECC_clearNIntrPending
int32_t SDL_ECC_clearNIntrPending(SDL_ECC_MemType eccMemType, SDL_ECC_MemSubType memSubType, SDL_Ecc_AggrIntrSrc intrSrc, SDL_Ecc_AggrEDCErrorSubType subType, uint32_t numEvents)
Clears N pending interrupts for the specified memtype, subtype and interrupt source.
SDL_ECC_getErrorInfo
int32_t SDL_ECC_getErrorInfo(SDL_ECC_MemType eccMemType, SDL_Ecc_AggrIntrSrc intrSrc, SDL_ECC_ErrorInfo_t *pErrorInfo)
Retrieves the ECC error information for the specified memtype and interrupt source.
SDL_EXCEPTION_fiqExptnHandler
void SDL_EXCEPTION_fiqExptnHandler(void *param)
FIQ Exception Handler.
SDL_ECC_applicationCallbackFunction
void SDL_ECC_applicationCallbackFunction(SDL_ECC_MemType eccMemType, uint32_t errorSrc, uint32_t address, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup)
Application provided external callback function for ECC handling Called inside the reference function...
SDL_EXCEPTION_dataAbortExptnHandler
void SDL_EXCEPTION_dataAbortExptnHandler(void *param)
Data Abort Exception Handler.
SDL_ECC_MemType
uint32_t SDL_ECC_MemType
This enumerator indicate ECC memory type.
Definition: sdl_ecc.h:292
SDL_ECC_init
int32_t SDL_ECC_init(SDL_ECC_MemType eccMemType, const SDL_ECC_InitConfig_t *pECCInitConfig)
Initializes ECC module for ECC detection.
SDL_EXCEPTION_CallbackFunctions_t::udefExptnCallback
SDL_EXCEPTION_Callback_t udefExptnCallback
Definition: sdl_exception.h:75