This example shows about how to implement a simple UDP IGMP-Server on LwIP networking stack using BSD-Socket API coupled with ethernet driver (ENET)
On AM64X, we can do ethernet based communication using CPSW as HW mechanism
The example does below
Parameter | Value |
---|---|
CPU + OS | r5fss0-0_freertos |
Toolchain | ti-arm-clang |
Board | am64x-evm |
Example folder | examples/networking/lwip/enet_cpsw_udp_igmp |
Note: To run the example on any core other than r5fss0-0, user needs to change the DMA channel resource ownership accordingly using the resource partioning tool in Modifying resource allocation and build the new SBL.
Feature | Section | Description | Remarks/Default Setting |
---|---|---|---|
Mdio Manual Mode Enable | TI Networking / Enet (CPSW) | Flag to enable MDIO manual mode in example. Driver support for Manual mode is enabled, so this parameter configures manual mode in the example. | Default is true. If your silicon is affected with errata i2329— MDIO interface corruption, then TI suggests to use MDIO_MANUAL_MODE as software workaround. |
Disable Mac Port1, Disable Mac Port2 | TI Networking / Enet (CPSW) | Select which port to disable. | Default is Port1 enabled. If both Port1 and Port 2 are enabled, any port can be used and if operating in switch mode, it enables traffic switching between the two ports. |
Enable Packet Pool Allocation | TI Networking / Enet (CPSW) | Flag to enable packet buffer memory allocation from enet utils library. It should be disabled to avoid utils memory wastage, in case application allots packet via other mechanism. | Default is true. If enabled size of pkt pool size depends on 'Large Pool Packet Size', 'Large Pool Packet Count', 'Medium Pool Packet Size', 'Medium Pool Packet Count', 'Small Pool Packet Size' and 'Small Pool Packet Count'. EnetMem_allocEthPkt API uses this memory to allocate the DMA Ethernet packet. |
Only Enable Packet Info Allocation | TI Networking / Enet (CPSW) | Flag to allocate only the DMA Packet Info structures, this does not include the buffer memory. This is useful when the buffer memory is internally allocated by the application. (Ex- Lwip pools) | Default is true. If enabled "PktInfoMem Only Count" determines the number of additional DMA Packet Info structures allocated. EnetMem_allocEthPktInfoMem uses this memory to allocate empty DMA Packet Info structures. |
Number of Tx Packet | TI Networking / Enet (CPSW) / DMA channel config | No of Tx packets required for DMA channel | Default is 16. For LwIP example, the Tx packet buffer memory is internally allocated in lwippools.h. Only the DMA Pkt Info structures are allocated via sysCfg, so this number should match the "PktInfoMem Only Count" described in the above item. To increase the Tx packet count, user needs to update the number correspondingly at "PktInfoMem Only Count" and lwippools.h and build the libs. |
Number of Rx Packet | TI Networking / Enet (CPSW) / DMA channel config | No of Rx packets required for DMA channel | Default is 32. It contributes to the size of Pkt Mem Pool, DMA ring buffer and accessories size. Rx packet buffer memory is completely mananged with application sysCfg, this is done by using Rx custom Pbuf in LwIP. |
Netif instance | TI Networking / Enet (CPSW) / LWIP Interface config | No of netifs allocated by the example | Only one netif should be set to default when more than one netif is allocated. |
Ncat is a general-purpose command-line tool for reading, writing, redirecting, and encrypting data across a network. It aims to be your network Swiss Army knife, handling a wide variety of security testing and administration tasks. Ncat is suitable for interactive use or as a network-connected back end for other tools.
Note: For UDP transmission on LwIP based application, application should perform cache coherency operation on payload before submitting the packet for transmission. This is because zero copy is enabled for UDP packet transmission and cache operation in driver are disabled for UDP payload portions. This example application does this using CacheP_wbInv.
Start UDP client using 'ncat' cmds as shown below. Below steps have been tried with a Linux Ubuntu 18.04 host PC running bash shell
Install 'ncat' if not installed by doing below
Invoke 'ncat' to connect to Multicast IP '224.0.1.129' on port 2638
00:00:00:00:00:00
, likely you are using a very early Si sample which does not have MAC address "fused" in, in this case do below stepssource/networking/.meta/enet_cpsw/templates/am64x_am243x/enet_soc_cfg.c.xdt
Enet IF UP Event.
message, if not check the ethernet cable