EtherNet/IP™ Adapter3.02.00
Setup

Software Installation

The EtherNet/IP Adapter software is installed as part of the MCU+ SDK for AM64X MCUs. It is recommended to consult the Getting Started guide for the SDK before you begin working with the EtherNet/IP Adapter software itself.

This software has been tested with CCS version 12.2.0.00009 (Windows).

Connect the Evaluation Board

  • Connect the evaluation board to your computer using the micro-USB cable. One cable is required for the JTAG interface, a second cable for the UART console.
  • Connect the boards to the power supplies according to the specifications in the AM64x/AM243x EVM User's Guide.