EtherCAT Slave1.12.02

◆ EC_API_SLV_cbRegisterMeasurement()

void EC_API_SLV_cbRegisterMeasurement ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
void *  pContext_p,
EC_API_SLV_CBMsrmt_t  cbFunc_p 
)

Initialize flash memory block.

Parameters
[in]pEcSlaveApi_pSlave API Handle Instance
[in]pContext_pInit flash block Callback context
[in]cbFunc_pInit flash block Callback
Example
#include <ecSlvApi.h>
// required variables
// the Call
EC_API_SLV_cbRegisterFlashInit(ecSlaveApi, cbFunc);
void(* EC_API_SLV_CBInitFlash_t)(void *pContext_p)
Init flash memory block to load and store eeprom content.
Definition: ecSlvApi.h:972
void EC_API_SLV_cbRegisterFlashInit(EC_API_SLV_SHandle_t *pEcSlaveApi_p, void *pContext_p, EC_API_SLV_CBInitFlash_t cbFunc_p)
Initialize flash memory block.
Definition: ecSlvApiStub.c:1697
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:157
Examples
ecSlvCiA402.c.