EtherCAT Slave1.12.02

◆ EC_API_SLV_CoE_getObjectEntryLength()

uint32_t EC_API_SLV_CoE_getObjectEntryLength ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
EC_API_SLV_SCoE_ObjEntry_t pObjEntry_p,
uint32_t *  length_p 
)

This function returns the object entry length.

Parameters
[in]pEcSlaveApi_pThe pointer to the EtherCAT API instance.
[in]pObjEntry_pPointer to the object entry instance.
[out]length_pObject entry length.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t length = 0;
i32uErr_l = EC_API_SLV_CoE_getObjectLength(ecSlaveApi, ptObject, &length);
uint32_t EC_API_SLV_CoE_getObjectLength(EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint32_t *length_p)
This function returns the object length.
Definition: ecSlvApi_CoEStub.c:278
See also
EC_API_SLV_CoE_getObject EC_API_SLV_CoE_getObjectLength