EtherCAT Slave1.12.02

◆ EC_API_SLV_CiA402_activateAxis()

void EC_API_SLV_CiA402_activateAxis ( EC_API_SLV_SHandle_t pEcSlaveApi_p,
uint8_t  axisNo_p,
bool  active_p 
)

Activate Axis. This function is required to inform the CiA402 state machine that the axis is switched on.

Parameters
[in]pEcSlaveApi_pEtherCAT DTK instance.
[in]axisNo_pAxis number.
[in]active_pAxis activated or not.
Example
#include <ecSlvApi.h>
// required variables
uint8_t AxisNo = 1;
bool active = true;
// the Call
retVal = EC_API_SLV_CiA402ActivateAxis(ecSlaveApi, axisNo, active);
struct EC_API_SLV_SHandle EC_API_SLV_SHandle_t
EC_API_SLV_SHandle_t describes the EtherCAT Slave API.
Definition: ecSlvApi.h:157
See also
EC_API_SLV_CiA402_setAxisNumber
Examples
ESL_cia402Demo.c.