![Logo](ti_logo.svg) |
AM64x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
52 #include <sdl/include/soc_config.h>
54 #if defined (IP_VERSION_VTM_V0)
VTM Static Registers for Voltage Domain.
Definition: sdl_vtm.h:126
SDL_VTM_Ctrlcfg tsCtrl_cfg
Definition: sdl_vtm.h:109
int32_t SDL_VTM_initTs(SDL_VTM_InstTs instance, const SDL_VTM_configTs *pConfig)
VTM Temperature sensor initialization.
uint16_t SDL_VTM_vdEvtSel_set
Definition: sdl_ip_vtm.h:172
uint8_t vid_opp_val
Definition: sdl_vtm.h:93
VTM Global Configuration Registers.
Definition: sdl_ip_vtm.h:464
SDL_VTM_tsThrVal thr_val
Definition: sdl_vtm.h:115
int32_t SDL_VTM_verifyConfigVd(SDL_VTM_InstVd instance, const SDL_VTM_configVd *pConfig)
VTM Voltage Domain configures verification.
SDL_VTM_InstVd
Definition: sdl_soc_vtm.h:108
int32_t SDL_VTM_getStaticRegistersVd(SDL_VTM_InstVd instance, SDL_VTM_staticRegsVd *pStaticRegs)
VTM Voltage Domain readback Static configuration registers.
VTM temperature sensor configuration.
Definition: sdl_vtm.h:105
SDL_VTM_InstTs
Definition: sdl_soc_vtm.h:76
SDL_VTM_vid_opp vid_opp
Definition: sdl_vtm.h:91
SDL_VTM_vdEvtSel_set vd_temp_evts
Definition: sdl_vtm.h:95
SDL_VTM_configTsCtrl configTsCtrl
Definition: sdl_vtm.h:107
SDL_VTM_tsGlobal_cfg tsGlobal_cfg
Definition: sdl_vtm.h:97
uint16_t SDL_VTM_intrCtrl
Definition: sdl_ip_vtm.h:148
uint32_t vtm_vd_evt_sel_ctrl
Definition: sdl_vtm.h:128
uint32_t vtm_ts_ctrl2
Definition: sdl_vtm.h:145
int32_t SDL_VTM_getSensorStatus(SDL_VTM_InstTs instance, const SDL_VTM_Stat_read_ctrl *pCtrl, SDL_VTM_Stat_val *pStat_val)
Read VTM Temperature sensor status.
int32_t SDL_VTM_initVd(SDL_VTM_InstVd instance, const SDL_VTM_configVd *pConfig)
VTM Voltage Domain initialization.
int32_t high_temp_in_milli_degree_celsius
Definition: sdl_vtm.h:111
VTM temperature sensor band gap control.
Definition: sdl_ip_vtm.h:502
int32_t SDL_VTM_getStaticRegistersTs(SDL_VTM_InstTs instance, SDL_VTM_staticRegsTs *pStaticRegs)
VTM Temperature sensor readback Static configuration registers.
int32_t SDL_VTM_verifyConfigTs(SDL_VTM_InstTs instance, const SDL_VTM_configTs *pConfig)
VTM Temperature sensor configures verification.
int32_t SDL_VTM_intrCntrl(SDL_VTM_InstVd instance, SDL_VTM_intrCtrl intrCtrl)
Set maximum Threshold values of VTM Temperature sensor.
VTM Static Registers for Temperature sensor.
Definition: sdl_vtm.h:143
int32_t low_temp_in_milli_degree_celsius
Definition: sdl_vtm.h:113
uint8_t SDL_VTM_Stat_read_ctrl
Definition: sdl_ip_vtm.h:416
uint32_t vtm_ts_th2
Definition: sdl_vtm.h:151
int32_t SDL_VTM_getTemp(SDL_VTM_InstTs instance, uint32_t *pTempVal)
Read VTM Temperature sensor values in degree celcius.
VTM temperature sensor threshold values.
Definition: sdl_ip_vtm.h:529
uint8_t SDL_VTM_configTsCtrl
Definition: sdl_ip_vtm.h:93
VTM Voltage Domain configuration.
Definition: sdl_vtm.h:87
uint8_t SDL_VTM_configVdCtrl
This enumerator define forVTM VD configuration valid map.
Definition: sdl_ip_vtm.h:80
uint32_t vtm_vd_opp_vid
Definition: sdl_vtm.h:130
SDL_VTM_tsGlobal_cfg vtm_global_cfg
Definition: sdl_vtm.h:132
VTM temperature sensor Stat values.
Definition: sdl_ip_vtm.h:552
uint32_t vtm_ts_ctrl
Definition: sdl_vtm.h:147
SDL_VTM_configVdCtrl configVdCtrl
Definition: sdl_vtm.h:89
uint8_t SDL_VTM_vid_opp
Definition: sdl_ip_vtm.h:108
uint32_t vtm_ts_th
Definition: sdl_vtm.h:149