![Logo](ti_logo.svg) |
AM64x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
68 #define DP83867_LED_NUM (4U)
77 typedef enum Dp83867_Gpio0Mode_e
110 typedef enum Dp83867_Gpio1Mode_e
143 typedef enum Dp83867_LedMode_e
191 typedef struct Dp83867_Cfg_s
@ DP83867_GPIO1_LED3
Definition: dp83867.h:128
uint32_t impedanceInMilliOhms
Definition: dp83867.h:213
uint32_t idleCntThresh
Definition: dp83867.h:209
@ DP83867_LED_LINKED_10BT
Definition: dp83867.h:167
@ DP83867_GPIO0_1588RXSFD
Definition: dp83867.h:86
@ DP83867_LED_FULLDUPLEX
Definition: dp83867.h:176
@ DP83867_GPIO0_1588TXSFD
Definition: dp83867.h:83
Dp83867_Gpio1Mode gpio1Mode
Definition: dp83867.h:219
Dp83867_LedMode
LED modes (sources).
Definition: dp83867.h:144
void Dp83867_initCfg(Dp83867_Cfg *cfg)
Initialize DP83867 PHY specific config params.
Dp83867_Gpio0Mode gpio0Mode
Definition: dp83867.h:216
@ DP83867_GPIO1_ENERGYDET
Definition: dp83867.h:125
@ DP83867_LED_RXERR
Definition: dp83867.h:185
@ DP83867_LED_LINKED
Definition: dp83867.h:146
@ DP83867_LED_LINKED_BLINKACT
Definition: dp83867.h:179
@ DP83867_GPIO1_WOL
Definition: dp83867.h:122
@ DP83867_GPIO0_PRBSERR
Definition: dp83867.h:98
@ DP83867_GPIO0_RXERR
Definition: dp83867.h:80
@ DP83867_GPIO0_LED3
Definition: dp83867.h:95
@ DP83867_LED_LINKED_1000BT
Definition: dp83867.h:161
@ DP83867_LED_RXACT
Definition: dp83867.h:155
@ DP83867_LED_COLLDET
Definition: dp83867.h:158
Dp83867_Gpio1Mode
GPIO_1 mux modes.
Definition: dp83867.h:111
@ DP83867_GPIO1_PRBSERR
Definition: dp83867.h:131
bool txClkShiftEn
Definition: dp83867.h:194
@ DP83867_GPIO0_ENERGYDET
Definition: dp83867.h:92
@ DP83867_LED_LINKED_100BTX
Definition: dp83867.h:164
uint8_t txFifoDepth
Definition: dp83867.h:206
@ DP83867_GPIO1_COL
Definition: dp83867.h:113
uint32_t rxDelayInPs
Definition: dp83867.h:203
Dp83867_Gpio0Mode
GPIO_0 mux modes.
Definition: dp83867.h:78
bool rxClkShiftEn
Definition: dp83867.h:197
@ DP83867_GPIO0_WOL
Definition: dp83867.h:89
@ DP83867_LED_RXTXACT
Definition: dp83867.h:149
@ DP83867_GPIO1_1588RXSFD
Definition: dp83867.h:119
@ DP83867_LED_RXTXERR
Definition: dp83867.h:182
@ DP83867_LED_LINKED_10100BT
Definition: dp83867.h:170
@ DP83867_GPIO1_CONSTANT0
Definition: dp83867.h:134
#define DP83867_LED_NUM
Number of LEDs available in the PHY.
Definition: dp83867.h:68
@ DP83867_GPIO1_CONSTANT1
Definition: dp83867.h:137
uint32_t txDelayInPs
Definition: dp83867.h:200
@ DP83867_GPIO0_CONSTANT1
Definition: dp83867.h:104
DP83867 PHY configuration parameters.
Definition: dp83867.h:192
@ DP83867_GPIO1_1588TXSFD
Definition: dp83867.h:116
@ DP83867_LED_TXACT
Definition: dp83867.h:152
@ DP83867_LED_LINKED_1001000BT
Definition: dp83867.h:173
@ DP83867_GPIO0_CONSTANT0
Definition: dp83867.h:101