EtherNet/IP™ Adapter3.02.00

◆ EI_API_CIP_CBCfgAssembly

typedef uint32_t(* EI_API_CIP_CBCfgAssembly) (EI_API_CIP_NODE_T *pCipNode_p, uint16_t o2t_p, uint16_t t2o_p, uint16_t cfg_inst_p, const uint8_t *const cfg_data, uint16_t cfg_data_size, uint16_t linkAddress_p)

Function prototype for CIP get configuration assembly data callback function.